<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Network driver panic on TWR-LS1021A - Qoriq SDK-v2.0 in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/Network-driver-panic-on-TWR-LS1021A-Qoriq-SDK-v2-0/m-p/471423#M699</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes this log was with the pre-built sdk uImage, dtb, rootfs. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But custom images with a slightly modified ls1021a_defconfig, yocto sdk2 branch lead to the same issue.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 23 Jun 2016 17:11:14 GMT</pubDate>
    <dc:creator>xkonni</dc:creator>
    <dc:date>2016-06-23T17:11:14Z</dc:date>
    <item>
      <title>Network driver panic on TWR-LS1021A - Qoriq SDK-v2.0</title>
      <link>https://community.nxp.com/t5/Layerscape/Network-driver-panic-on-TWR-LS1021A-Qoriq-SDK-v2-0/m-p/471416#M692</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello All,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have been trying to boot the LS1021A-TWR board with Qoriq SDK v2.0 and been seeing this network driver crash there after the NFS boot hangs:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------snip----------------&lt;/P&gt;&lt;P&gt;Key type dns_resolver registered&lt;/P&gt;&lt;P&gt;Registering SWP/SWPB emulation handler&lt;/P&gt;&lt;P&gt;sgtl5000 1-000a: Using internal LDO instead of VDDD&lt;/P&gt;&lt;P&gt;asoc-simple-card sound: sgtl5000 &amp;lt;-&amp;gt; 2b50000.sai mapping ok&lt;/P&gt;&lt;P&gt;hctosys: unable to open rtc device (rtc0)&lt;/P&gt;&lt;P&gt;IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready&lt;/P&gt;&lt;P&gt;random: nonblocking pool is initialized&lt;/P&gt;&lt;P&gt;IPv6: ADDRCONF(NETDEV_UP): eth1: link is not ready&lt;/P&gt;&lt;P&gt;IPv6: ADDRCONF(NETDEV_UP): eth2: link is not ready&lt;/P&gt;&lt;P&gt;fsl-gianfar soc:ethernet@2d50000 eth1: Link is Up - 1Gbps/Full - flow control rx/tx&lt;/P&gt;&lt;P&gt;IPv6: ADDRCONF(NETDEV_CHANGE): eth1: link becomes ready&lt;/P&gt;&lt;P&gt;Sending DHCP requests ..&lt;/P&gt;&lt;P&gt;------------[ cut here ]------------&lt;/P&gt;&lt;P&gt;WARNING: CPU: 1 PID: 0 at net/sched/sch_generic.c:321 dev_watchdog+0x1d8/0x260()&lt;/P&gt;&lt;P&gt;NETDEV WATCHDOG: eth1 (fsl-gianfar): transmit queue 0 timed out&lt;/P&gt;&lt;P&gt;Modules linked in:&lt;/P&gt;&lt;P&gt;CPU: 1 PID: 0 Comm: swapper/1 Not tainted 4.1.8-rt8+ls1+gbd51baf #2&lt;/P&gt;&lt;P&gt;Hardware name: Freescale LS1021A&lt;/P&gt;&lt;P&gt;[&amp;lt;80025508&amp;gt;] (unwind_backtrace) from [&amp;lt;800222c0&amp;gt;] (show_stack+0x10/0x14)&lt;/P&gt;&lt;P&gt;[&amp;lt;800222c0&amp;gt;] (show_stack) from [&amp;lt;8056e888&amp;gt;] (dump_stack+0x70/0x8c)&lt;/P&gt;&lt;P&gt;[&amp;lt;8056e888&amp;gt;] (dump_stack) from [&amp;lt;8003cbc8&amp;gt;] (warn_slowpath_common+0x80/0xac)&lt;/P&gt;&lt;P&gt;[&amp;lt;8003cbc8&amp;gt;] (warn_slowpath_common) from [&amp;lt;8003cc20&amp;gt;] (warn_slowpath_fmt+0x2c/0x3c)&lt;/P&gt;&lt;P&gt;[&amp;lt;8003cc20&amp;gt;] (warn_slowpath_fmt) from [&amp;lt;804806c4&amp;gt;] (dev_watchdog+0x1d8/0x260)&lt;/P&gt;&lt;P&gt;[&amp;lt;804806c4&amp;gt;] (dev_watchdog) from [&amp;lt;8007e69c&amp;gt;] (call_timer_fn+0x20/0x90)&lt;/P&gt;&lt;P&gt;[&amp;lt;8007e69c&amp;gt;] (call_timer_fn) from [&amp;lt;8007e9a8&amp;gt;] (run_timer_softirq+0x1d8/0x218)&lt;/P&gt;&lt;P&gt;[&amp;lt;8007e9a8&amp;gt;] (run_timer_softirq) from [&amp;lt;8003fe68&amp;gt;] (__do_softirq+0xd4/0x200)&lt;/P&gt;&lt;P&gt;[&amp;lt;8003fe68&amp;gt;] (__do_softirq) from [&amp;lt;80040558&amp;gt;] (irq_exit+0x84/0xf4)&lt;/P&gt;&lt;P&gt;[&amp;lt;80040558&amp;gt;] (irq_exit) from [&amp;lt;800712ac&amp;gt;] (__handle_domain_irq+0x90/0xb4)&lt;/P&gt;&lt;P&gt;[&amp;lt;800712ac&amp;gt;] (__handle_domain_irq) from [&amp;lt;80009444&amp;gt;] (gic_handle_irq+0x3c/0x5c)&lt;/P&gt;&lt;P&gt;[&amp;lt;80009444&amp;gt;] (gic_handle_irq) from [&amp;lt;80573000&amp;gt;] (__irq_svc+0x40/0x54)&lt;/P&gt;&lt;P&gt;Exception stack(0xbf07bf98 to 0xbf07bfe0)&lt;/P&gt;&lt;P&gt;bf80:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 00000001 00000000&lt;/P&gt;&lt;P&gt;bfa0: 00000000 8002e360 bf07a000 00000000 30c0387d 00000000 bf07bfe8 807ac418&lt;/P&gt;&lt;P&gt;bfc0: 00000001 00000000 01000000 bf07bfe0 8001fd74 8001fd78 60000113 ffffffff&lt;/P&gt;&lt;P&gt;[&amp;lt;80573000&amp;gt;] (__irq_svc) from [&amp;lt;8001fd78&amp;gt;] (arch_cpu_idle+0x2c/0x38)&lt;/P&gt;&lt;P&gt;[&amp;lt;8001fd78&amp;gt;] (arch_cpu_idle) from [&amp;lt;80069c30&amp;gt;] (cpu_startup_entry+0x22c/0x26c)&lt;/P&gt;&lt;P&gt;[&amp;lt;80069c30&amp;gt;] (cpu_startup_entry) from [&amp;lt;8000950c&amp;gt;] (__enable_mmu+0x0/0x14)&lt;/P&gt;&lt;P&gt;---[ end trace f274e2c156a0521b ]---&lt;/P&gt;&lt;P&gt;fsl-gianfar soc:ethernet@2d50000 eth1: Link is Up - 1Gbps/Full - flow control rx/tx&lt;/P&gt;&lt;P&gt;.&lt;/P&gt;&lt;P&gt;fsl-gianfar soc:ethernet@2d50000 eth1: Link is Up - 1Gbps/Full - flow control rx/tx&lt;/P&gt;&lt;P&gt;.&lt;/P&gt;&lt;P&gt;fsl-gianfar soc:ethernet@2d50000 eth1: Link is Up - 1Gbps/Full - flow control rx/tx&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;---------------8&amp;lt;-------------------&lt;/P&gt;&lt;P&gt;Could anyone confirm that network driver is working without any issues in Qoriq SDK v2.0 for Layerscape LS1021A board ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in Advance!&lt;/P&gt;&lt;P&gt;-skrishna&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 01 Jun 2016 16:57:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Network-driver-panic-on-TWR-LS1021A-Qoriq-SDK-v2-0/m-p/471416#M692</guid>
      <dc:creator>skrishnakar</dc:creator>
      <dc:date>2016-06-01T16:57:00Z</dc:date>
    </item>
    <item>
      <title>Re: Network driver panic on TWR-LS1021A - Qoriq SDK-v2.0</title>
      <link>https://community.nxp.com/t5/Layerscape/Network-driver-panic-on-TWR-LS1021A-Qoriq-SDK-v2-0/m-p/471417#M693</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please provide U-Boot log for the board.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 Jun 2016 01:45:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Network-driver-panic-on-TWR-LS1021A-Qoriq-SDK-v2-0/m-p/471417#M693</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2016-06-02T01:45:36Z</dc:date>
    </item>
    <item>
      <title>Re: Network driver panic on TWR-LS1021A - Qoriq SDK-v2.0</title>
      <link>https://community.nxp.com/t5/Layerscape/Network-driver-panic-on-TWR-LS1021A-Qoriq-SDK-v2-0/m-p/471418#M694</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;same happens for me.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;here's a (hopefully) complete bootlog: &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;=&amp;gt; run sdboot&lt;/P&gt;&lt;P&gt;reading uImage&lt;/P&gt;&lt;P&gt;3510824 bytes read in 166 ms (20.2 MiB/s)&lt;/P&gt;&lt;P&gt;reading ls1021a-twr.dtb&lt;/P&gt;&lt;P&gt;21610 bytes read in 18 ms (1.1 MiB/s)&lt;/P&gt;&lt;P&gt;reading rootfs&lt;/P&gt;&lt;P&gt;53187597 bytes read in 2257 ms (22.5 MiB/s)&lt;/P&gt;&lt;P&gt;## Booting kernel from Legacy Image at 81000000 ...&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Image Name:&amp;nbsp;&amp;nbsp; Linux-4.1.8-rt8+gbd51baf&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Image Type:&amp;nbsp;&amp;nbsp; ARM Linux Kernel Image (uncompressed)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Data Size:&amp;nbsp;&amp;nbsp;&amp;nbsp; 3510760 Bytes = 3.3 MiB&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Load Address: 80008000&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Entry Point:&amp;nbsp; 80008000&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Verifying Checksum ... OK&lt;/P&gt;&lt;P&gt;## Loading init Ramdisk from Legacy Image at 88000000 ...&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Image Name:&amp;nbsp;&amp;nbsp; fsl-image-mesh-ls1021atwr-201606&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Image Type:&amp;nbsp;&amp;nbsp; ARM Linux RAMDisk Image (gzip compressed)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Data Size:&amp;nbsp;&amp;nbsp;&amp;nbsp; 53187533 Bytes = 50.7 MiB&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Load Address: 00000000&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Entry Point:&amp;nbsp; 00000000&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Verifying Checksum ... OK&lt;/P&gt;&lt;P&gt;## Flattened Device Tree blob at 8f000000&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Booting using the fdt blob at 0x8f000000&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Loading Kernel Image ... OK&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Loading Ramdisk to bbc4c000, end bef053cd ... OK&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Loading Device Tree to bbc43000, end bbc4b469 ... OK&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Starting kernel ...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Booting Linux on physical CPU 0xf00&lt;/P&gt;&lt;P&gt;Linux version 4.1.8-rt8+gbd51baf (jenkins@mercury) (gcc version 4.9.3 20150311 (prerelease) (Linaro GCC 4.9-2015.03) ) #1 SMP Sun May 15 05:05:43 CST 2016&lt;/P&gt;&lt;P&gt;CPU: ARMv7 Processor [410fc075] revision 5 (ARMv7), cr=70c5387d&lt;/P&gt;&lt;P&gt;CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache&lt;/P&gt;&lt;P&gt;Machine model: LS1021A TWR Board&lt;/P&gt;&lt;P&gt;Forcing write-allocate cache policy for SMP&lt;/P&gt;&lt;P&gt;Memory policy: Data cache writealloc&lt;/P&gt;&lt;P&gt;PERCPU: Embedded 12 pages/cpu @bffcd000 s16640 r8192 d24320 u49152&lt;/P&gt;&lt;P&gt;Built 1 zonelists in Zone order, mobility grouping on.&amp;nbsp; Total pages: 260096&lt;/P&gt;&lt;P&gt;Kernel command line: root=/dev/ram0 rw console=ttyS0,115200 hdmi high&lt;/P&gt;&lt;P&gt;PID hash table entries: 4096 (order: 2, 16384 bytes)&lt;/P&gt;&lt;P&gt;Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)&lt;/P&gt;&lt;P&gt;Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)&lt;/P&gt;&lt;P&gt;Memory: 979732K/1048576K available (3695K kernel code, 224K rwdata, 1752K rodata, 236K init, 209K bss, 68844K reserved, 0K cma-reserved, 0K highmem)&lt;/P&gt;&lt;P&gt;Virtual kernel memory layout:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; vector&amp;nbsp; : 0xffff0000 - 0xffff1000&amp;nbsp;&amp;nbsp; (&amp;nbsp;&amp;nbsp; 4 kB)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; fixmap&amp;nbsp; : 0xffc00000 - 0xfff00000&amp;nbsp;&amp;nbsp; (3072 kB)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; vmalloc : 0xc0800000 - 0xff000000&amp;nbsp;&amp;nbsp; (1000 MB)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; lowmem&amp;nbsp; : 0x80000000 - 0xc0000000&amp;nbsp;&amp;nbsp; (1024 MB)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; pkmap&amp;nbsp;&amp;nbsp; : 0x7fe00000 - 0x80000000&amp;nbsp;&amp;nbsp; (&amp;nbsp;&amp;nbsp; 2 MB)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; modules : 0x7f800000 - 0x7fe00000&amp;nbsp;&amp;nbsp; (&amp;nbsp;&amp;nbsp; 6 MB)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .text : 0x80008000 - 0x8055a1bc&amp;nbsp;&amp;nbsp; (5449 kB)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .init : 0x8055b000 - 0x80596000&amp;nbsp;&amp;nbsp; ( 236 kB)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .data : 0x80596000 - 0x805ce358&amp;nbsp;&amp;nbsp; ( 225 kB)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .bss : 0x805d1000 - 0x80605694&amp;nbsp;&amp;nbsp; ( 210 kB)&lt;/P&gt;&lt;P&gt;SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=2, Nodes=1&lt;/P&gt;&lt;P&gt;Hierarchical RCU implementation.&lt;/P&gt;&lt;P&gt; [8CAdditional per-CPU info printed with stalls.&lt;/P&gt;&lt;P&gt; [8CRCU restricting CPUs from NR_CPUS=4 to nr_cpu_ids=2.&lt;/P&gt;&lt;P&gt;RCU: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=2&lt;/P&gt;&lt;P&gt;NR_IRQS:16 nr_irqs:16 16&lt;/P&gt;&lt;P&gt;Architected cp15 timer(s) running at 12.50MHz (phys).&lt;/P&gt;&lt;P&gt;clocksource arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x2e2049cda, max_idle_ns: 440795202628 ns&lt;/P&gt;&lt;P&gt;sched_clock: 56 bits at 12MHz, resolution 80ns, wraps every 4398046511080ns&lt;/P&gt;&lt;P&gt;Switching to timer-based delay loop, resolution 80ns&lt;/P&gt;&lt;P&gt;Console: colour dummy device 80x30&lt;/P&gt;&lt;P&gt;Calibrating delay loop (skipped), value calculated using timer frequency.. 25.00 BogoMIPS (lpj=125000)&lt;/P&gt;&lt;P&gt;pid_max: default: 32768 minimum: 301&lt;/P&gt;&lt;P&gt;Mount-cache hash table entries: 2048 (order: 1, 8192 bytes)&lt;/P&gt;&lt;P&gt;Mountpoint-cache hash table entries: 2048 (order: 1, 8192 bytes)&lt;/P&gt;&lt;P&gt;CPU: Testing write buffer coherency: ok&lt;/P&gt;&lt;P&gt;CPU0: update cpu_capacity 1024&lt;/P&gt;&lt;P&gt;CPU0: thread -1, cpu 0, socket 15, mpidr 80000f00&lt;/P&gt;&lt;P&gt;Setting up static identity map for 0x80008280 - 0x800082e4&lt;/P&gt;&lt;P&gt;CPU1: update cpu_capacity 1024&lt;/P&gt;&lt;P&gt;CPU1: thread -1, cpu 1, socket 15, mpidr 80000f01&lt;/P&gt;&lt;P&gt;Brought up 2 CPUs&lt;/P&gt;&lt;P&gt;SMP: Total of 2 processors activated (50.00 BogoMIPS).&lt;/P&gt;&lt;P&gt;CPU: All CPU(s) started in HYP mode.&lt;/P&gt;&lt;P&gt;CPU: Virtualization extensions available.&lt;/P&gt;&lt;P&gt;devtmpfs: initialized&lt;/P&gt;&lt;P&gt;VFP support v0.3: implementor 41 architecture 2 part 30 variant 7 rev 5&lt;/P&gt;&lt;P&gt;clocksource jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns&lt;/P&gt;&lt;P&gt;pinctrl core: initialized pinctrl subsystem&lt;/P&gt;&lt;P&gt;NET: Registered protocol family 16&lt;/P&gt;&lt;P&gt;DMA: preallocated 256 KiB pool for atomic coherent allocations&lt;/P&gt;&lt;P&gt;cpuidle: using governor ladder&lt;/P&gt;&lt;P&gt;cpuidle: using governor menu&lt;/P&gt;&lt;P&gt;irq: no irq domain found for /soc/uqe@2400000/qeic@80 !&lt;/P&gt;&lt;P&gt;irq: no irq domain found for /soc/uqe@2400000/qeic@80 !&lt;/P&gt;&lt;P&gt;hw-breakpoint: found 5 (+1 reserved) breakpoint and 4 watchpoint registers.&lt;/P&gt;&lt;P&gt;hw-breakpoint: maximum watchpoint size is 8 bytes.&lt;/P&gt;&lt;P&gt;register e1000-wakeup irq error, ret = -22&lt;/P&gt;&lt;P&gt;Serial: AMBA PL011 UART driver&lt;/P&gt;&lt;P&gt;vgaarb: loaded&lt;/P&gt;&lt;P&gt;SCSI subsystem initialized&lt;/P&gt;&lt;P&gt;usbcore: registered new interface driver usbfs&lt;/P&gt;&lt;P&gt;usbcore: registered new interface driver hub&lt;/P&gt;&lt;P&gt;usbcore: registered new device driver usb&lt;/P&gt;&lt;P&gt;i2c i2c-0: IMX I2C adapter registered&lt;/P&gt;&lt;P&gt;i2c i2c-0: can't use DMA&lt;/P&gt;&lt;P&gt;i2c i2c-1: IMX I2C adapter registered&lt;/P&gt;&lt;P&gt;i2c i2c-1: can't use DMA&lt;/P&gt;&lt;P&gt;pps_core: LinuxPPS API ver. 1 registered&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti &amp;lt;&lt;/SPAN&gt;&lt;A class="jive-link-email-small" href="mailto:giometti@linux.it"&gt;giometti@linux.it&lt;/A&gt;&lt;SPAN&gt;&amp;gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;PTP clock support registered&lt;/P&gt;&lt;P&gt;Advanced Linux Sound Architecture Driver Initialized.&lt;/P&gt;&lt;P&gt;Switched to clocksource arch_sys_counter&lt;/P&gt;&lt;P&gt;NET: Registered protocol family 2&lt;/P&gt;&lt;P&gt;TCP established hash table entries: 8192 (order: 3, 32768 bytes)&lt;/P&gt;&lt;P&gt;TCP bind hash table entries: 8192 (order: 4, 65536 bytes)&lt;/P&gt;&lt;P&gt;TCP: Hash tables configured (established 8192 bind 8192)&lt;/P&gt;&lt;P&gt;UDP hash table entries: 512 (order: 2, 16384 bytes)&lt;/P&gt;&lt;P&gt;UDP-Lite hash table entries: 512 (order: 2, 16384 bytes)&lt;/P&gt;&lt;P&gt;NET: Registered protocol family 1&lt;/P&gt;&lt;P&gt;RPC: Registered named UNIX socket transport module.&lt;/P&gt;&lt;P&gt;RPC: Registered udp transport module.&lt;/P&gt;&lt;P&gt;RPC: Registered tcp transport module.&lt;/P&gt;&lt;P&gt;RPC: Registered tcp NFSv4.1 backchannel transport module.&lt;/P&gt;&lt;P&gt;Trying to unpack rootfs image as initramfs...&lt;/P&gt;&lt;P&gt;rootfs image is not initramfs (no cpio magic); looks like an initrd&lt;/P&gt;&lt;P&gt;Freeing initrd memory: 51944K (bbc4c000 - bef06000)&lt;/P&gt;&lt;P&gt;kvm [1]: interrupt-controller@1404000 IRQ22&lt;/P&gt;&lt;P&gt;kvm [1]: timer IRQ18&lt;/P&gt;&lt;P&gt;kvm [1]: Hyp mode initialized successfully&lt;/P&gt;&lt;P&gt;CPU PMU: Failed to parse /pmu/interrupt-affinity[0]&lt;/P&gt;&lt;P&gt;hw perfevents: enabled with armv7_cortex_a7 PMU driver, 5 counters available&lt;/P&gt;&lt;P&gt;futex hash table entries: 512 (order: 3, 32768 bytes)&lt;/P&gt;&lt;P&gt;HugeTLB registered 2 MB page size, pre-allocated 0 pages&lt;/P&gt;&lt;P&gt;NFS: Registering the id_resolver key type&lt;/P&gt;&lt;P&gt;Key type id_resolver registered&lt;/P&gt;&lt;P&gt;Key type id_legacy registered&lt;/P&gt;&lt;P&gt;jffs2: version 2.2. (NAND) © 2001-2006 Red Hat, Inc.&lt;/P&gt;&lt;P&gt;io scheduler noop registered&lt;/P&gt;&lt;P&gt;io scheduler deadline registered&lt;/P&gt;&lt;P&gt;io scheduler cfq registered (default)&lt;/P&gt;&lt;P&gt;PCI host bridge /soc/pcie@3400000 ranges:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; IO 0x4000010000..0x400001ffff -&amp;gt; 0x00000000&lt;/P&gt;&lt;P&gt;&amp;nbsp; MEM 0x4040000000..0x407fffffff -&amp;gt; 0x40000000&lt;/P&gt;&lt;P&gt;layerscape-pcie 3400000.pcie: PCI host bridge to bus 0000:00&lt;/P&gt;&lt;P&gt;pci_bus 0000:00: root bus resource [bus 00-ff]&lt;/P&gt;&lt;P&gt;pci_bus 0000:00: root bus resource [io&amp;nbsp; 0x0000-0xffff]&lt;/P&gt;&lt;P&gt;pci_bus 0000:00: root bus resource [mem 0x4040000000-0x407fffffff] (bus address [0x40000000-0x7fffffff])&lt;/P&gt;&lt;P&gt;PCI: bus0: Fast back to back transfers disabled&lt;/P&gt;&lt;P&gt;PCI: bus1: Fast back to back transfers enabled&lt;/P&gt;&lt;P&gt;pci 0000:00:00.0: BAR 1: assigned [mem 0x4040000000-0x4043ffffff]&lt;/P&gt;&lt;P&gt;pci 0000:00:00.0: BAR 0: assigned [mem 0x4044000000-0x4044ffffff]&lt;/P&gt;&lt;P&gt;pci 0000:00:00.0: BAR 6: assigned [mem 0x4045000000-0x4045ffffff pref]&lt;/P&gt;&lt;P&gt;pci 0000:00:00.0: PCI bridge to [bus 01]&lt;/P&gt;&lt;P&gt;PCI host bridge /soc/pcie@3500000 ranges:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; IO 0x4800010000..0x480001ffff -&amp;gt; 0x00000000&lt;/P&gt;&lt;P&gt;&amp;nbsp; MEM 0x4840000000..0x487fffffff -&amp;gt; 0x40000000&lt;/P&gt;&lt;P&gt;layerscape-pcie 3500000.pcie: PCI host bridge to bus 0001:00&lt;/P&gt;&lt;P&gt;pci_bus 0001:00: root bus resource [bus 00-ff]&lt;/P&gt;&lt;P&gt;pci_bus 0001:00: root bus resource [io&amp;nbsp; 0x10000-0x1ffff] (bus address [0x0000-0xffff])&lt;/P&gt;&lt;P&gt;pci_bus 0001:00: root bus resource [mem 0x4840000000-0x487fffffff] (bus address [0x40000000-0x7fffffff])&lt;/P&gt;&lt;P&gt;PCI: bus0: Fast back to back transfers disabled&lt;/P&gt;&lt;P&gt;PCI: bus1: Fast back to back transfers enabled&lt;/P&gt;&lt;P&gt;pci 0001:00:00.0: BAR 1: assigned [mem 0x4840000000-0x4843ffffff]&lt;/P&gt;&lt;P&gt;pci 0001:00:00.0: BAR 0: assigned [mem 0x4844000000-0x4844ffffff]&lt;/P&gt;&lt;P&gt;pci 0001:00:00.0: BAR 6: assigned [mem 0x4845000000-0x4845ffffff pref]&lt;/P&gt;&lt;P&gt;pci 0001:00:00.0: PCI bridge to [bus 01]&lt;/P&gt;&lt;P&gt;Sii902x: read id = 0xB0&lt;/P&gt;&lt;P&gt;-0x02-0x03&lt;/P&gt;&lt;P&gt;-0x00&lt;/P&gt;&lt;P&gt;sii902x 1-0039: Can not read edid&lt;/P&gt;&lt;P&gt;Console: switching to colour frame buffer device 60x34&lt;/P&gt;&lt;P&gt;fb0: fb device registered successfully.&lt;/P&gt;&lt;P&gt;fb1: fb device registered successfully.&lt;/P&gt;&lt;P&gt;fb2: fb device registered successfully.&lt;/P&gt;&lt;P&gt;fb3: fb device registered successfully.&lt;/P&gt;&lt;P&gt;Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled&lt;/P&gt;&lt;P&gt;console [ttyS0] disabled&lt;/P&gt;&lt;P&gt;21c0500.serial: ttyS0 at MMIO 0x21c0500 (irq = 34, base_baud = 9375000) is a 16550A&lt;/P&gt;&lt;P&gt;console [ttyS0] enabled&lt;/P&gt;&lt;P&gt;21c0600.serial: ttyS1 at MMIO 0x21c0600 (irq = 34, base_baud = 9375000) is a 16550A&lt;/P&gt;&lt;P&gt;sii902x 1-0039: read edid fail&lt;/P&gt;&lt;P&gt;2950000.serial: ttyLP0 at MMIO 0x2950000 (irq = 40, base_baud = 6250000) is a FSL_LPUART&lt;/P&gt;&lt;P&gt;fsl-lpuart 2950000.serial: DMA tx channel request failed, operating without tx DMA&lt;/P&gt;&lt;P&gt;fsl-lpuart 2950000.serial: DMA rx channel request failed, operating without rx DMA&lt;/P&gt;&lt;P&gt;brd: module loaded&lt;/P&gt;&lt;P&gt;loop: module loaded&lt;/P&gt;&lt;P&gt;/soc/sata@3200000: could not get #clock-cells for /soc/clocking@1ee1000&lt;/P&gt;&lt;P&gt;ahci-qoriq 3200000.sata: AHCI 0001.0300 1 slots 1 ports ? Gbps 0x1 impl platform mode&lt;/P&gt;&lt;P&gt;ahci-qoriq 3200000.sata: flags: 64bit ncq sntf pm clo only pmp fbs pio slum part ccc &lt;/P&gt;&lt;P&gt;ahci-qoriq 3200000.sata: port 0 is not capable of FBS&lt;/P&gt;&lt;P&gt;scsi host0: ahci-qoriq&lt;/P&gt;&lt;P&gt;ata1: SATA max UDMA/133 mmio [mem 0x03200000-0x0320ffff] port 0x100 irq 27&lt;/P&gt;&lt;P&gt;60000000.nor: Found 1 x16 devices at 0x0 in 16-bit bank. Manufacturer ID 0x000089 Chip ID 0x00227e&lt;/P&gt;&lt;P&gt;Amd/Fujitsu Extended Query Table at 0x0040&lt;/P&gt;&lt;P&gt;&amp;nbsp; Amd/Fujitsu Extended Query version 1.3.&lt;/P&gt;&lt;P&gt;number of CFI chips: 1&lt;/P&gt;&lt;P&gt;10 ofpart partitions found on MTD device 60000000.nor&lt;/P&gt;&lt;P&gt;Creating 10 MTD partitions on "60000000.nor":&lt;/P&gt;&lt;P&gt;0x000000000000-0x000000020000 : "NOR bank0 RCW Image"&lt;/P&gt;&lt;P&gt;0x000000100000-0x000000200000 : "NOR bank0 u-boot Image"&lt;/P&gt;&lt;P&gt;0x000000200000-0x000000300000 : "NOR bank0 DTB Image"&lt;/P&gt;&lt;P&gt;0x000000300000-0x000000a00000 : "NOR bank0 Linux Kernel Image"&lt;/P&gt;&lt;P&gt;0x000000a00000-0x000004000000 : "NOR bank0 Ramdisk Root File System Image"&lt;/P&gt;&lt;P&gt;0x000004000000-0x000004020000 : "NOR bank4 RCW Image"&lt;/P&gt;&lt;P&gt;0x000004100000-0x000004200000 : "NOR bank4 u-boot Image"&lt;/P&gt;&lt;P&gt;0x000004200000-0x000004300000 : "NOR bank4 DTB Image"&lt;/P&gt;&lt;P&gt;0x000004300000-0x000004a00000 : "NOR bank4 Linux Kernel Image"&lt;/P&gt;&lt;P&gt;0x000004a00000-0x000008000000 : "NOR bank4 Ramdisk Root File System Image"&lt;/P&gt;&lt;P&gt;fsl-quadspi 1550000.quadspi: unrecognized JEDEC id bytes: 00, 00, 00&lt;/P&gt;&lt;P&gt;fsl-quadspi 1550000.quadspi: Freescale QuadSPI probe failed&lt;/P&gt;&lt;P&gt;fsl-quadspi: probe of 1550000.quadspi failed with error -2&lt;/P&gt;&lt;P&gt;m25p80 spi0.0: unrecognized JEDEC id bytes: 00, 00, 00&lt;/P&gt;&lt;P&gt;tun: Universal TUN/TAP device driver, 1.6&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;tun: (C) 1999-2004 Max Krasnyansky &amp;lt;&lt;/SPAN&gt;&lt;A class="jive-link-email-small" href="mailto:maxk@qualcomm.com"&gt;maxk@qualcomm.com&lt;/A&gt;&lt;SPAN&gt;&amp;gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;CAN device driver interface&lt;/P&gt;&lt;P&gt;2a70000.can supply xceiver not found, using dummy regulator&lt;/P&gt;&lt;P&gt;flexcan 2a70000.can: device registered (reg_base=c08bc000, irq=49)&lt;/P&gt;&lt;P&gt;2a80000.can supply xceiver not found, using dummy regulator&lt;/P&gt;&lt;P&gt;flexcan 2a80000.can: device registered (reg_base=c08be000, irq=50)&lt;/P&gt;&lt;P&gt;libphy: Freescale PowerQUICC MII Bus: probed&lt;/P&gt;&lt;P&gt;fsl-gianfar soc:ethernet@2d10000: enabled errata workarounds, flags: 0x4&lt;/P&gt;&lt;P&gt;fsl-gianfar soc:ethernet@2d10000 eth0: mac: 00:04:9f:03:f5:b1&lt;/P&gt;&lt;P&gt;fsl-gianfar soc:ethernet@2d10000 eth0: Running with NAPI enabled&lt;/P&gt;&lt;P&gt;fsl-gianfar soc:ethernet@2d10000 eth0: RX BD ring size for Q[0]: 256&lt;/P&gt;&lt;P&gt;fsl-gianfar soc:ethernet@2d10000 eth0: RX BD ring size for Q[1]: 256&lt;/P&gt;&lt;P&gt;fsl-gianfar soc:ethernet@2d10000 eth0: TX BD ring size for Q[0]: 256&lt;/P&gt;&lt;P&gt;fsl-gianfar soc:ethernet@2d10000 eth0: TX BD ring size for Q[1]: 256&lt;/P&gt;&lt;P&gt;fsl-gianfar soc:ethernet@2d50000: enabled errata workarounds, flags: 0x4&lt;/P&gt;&lt;P&gt;fsl-gianfar soc:ethernet@2d50000 eth1: mac: 00:04:9f:03:f5:b2&lt;/P&gt;&lt;P&gt;fsl-gianfar soc:ethernet@2d50000 eth1: Running with NAPI enabled&lt;/P&gt;&lt;P&gt;fsl-gianfar soc:ethernet@2d50000 eth1: RX BD ring size for Q[0]: 256&lt;/P&gt;&lt;P&gt;fsl-gianfar soc:ethernet@2d50000 eth1: RX BD ring size for Q[1]: 256&lt;/P&gt;&lt;P&gt;fsl-gianfar soc:ethernet@2d50000 eth1: TX BD ring size for Q[0]: 256&lt;/P&gt;&lt;P&gt;fsl-gianfar soc:ethernet@2d50000 eth1: TX BD ring size for Q[1]: 256&lt;/P&gt;&lt;P&gt;fsl-gianfar soc:ethernet@2d90000: enabled errata workarounds, flags: 0x4&lt;/P&gt;&lt;P&gt;fsl-gianfar soc:ethernet@2d90000 eth2: mac: 00:04:9f:03:f5:b3&lt;/P&gt;&lt;P&gt;fsl-gianfar soc:ethernet@2d90000 eth2: Running with NAPI enabled&lt;/P&gt;&lt;P&gt;fsl-gianfar soc:ethernet@2d90000 eth2: RX BD ring size for Q[0]: 256&lt;/P&gt;&lt;P&gt;fsl-gianfar soc:ethernet@2d90000 eth2: RX BD ring size for Q[1]: 256&lt;/P&gt;&lt;P&gt;fsl-gianfar soc:ethernet@2d90000 eth2: TX BD ring size for Q[0]: 256&lt;/P&gt;&lt;P&gt;fsl-gianfar soc:ethernet@2d90000 eth2: TX BD ring size for Q[1]: 256&lt;/P&gt;&lt;P&gt;pps pps0: new PPS source ptp0&lt;/P&gt;&lt;P&gt;e1000e: Intel(R) PRO/1000 Network Driver - 2.3.2-k&lt;/P&gt;&lt;P&gt;e1000e: Copyright(c) 1999 - 2014 Intel Corporation.&lt;/P&gt;&lt;P&gt;ata1: SATA link down (SStatus 0 SControl 300)&lt;/P&gt;&lt;P&gt;xhci-hcd xhci-hcd.0.auto: xHCI Host Controller&lt;/P&gt;&lt;P&gt;xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus number 1&lt;/P&gt;&lt;P&gt;xhci-hcd xhci-hcd.0.auto: hcc params 0x0220f66c hci version 0x100 quirks 0x00010010&lt;/P&gt;&lt;P&gt;xhci-hcd xhci-hcd.0.auto: irq 52, io mem 0x03100000&lt;/P&gt;&lt;P&gt;hub 1-0:1.0: USB hub found&lt;/P&gt;&lt;P&gt;hub 1-0:1.0: 1 port detected&lt;/P&gt;&lt;P&gt;xhci-hcd xhci-hcd.0.auto: xHCI Host Controller&lt;/P&gt;&lt;P&gt;xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus number 2&lt;/P&gt;&lt;P&gt;usb usb2: We don't know the algorithms for LPM for this host, disabling LPM.&lt;/P&gt;&lt;P&gt;hub 2-0:1.0: USB hub found&lt;/P&gt;&lt;P&gt;hub 2-0:1.0: 1 port detected&lt;/P&gt;&lt;P&gt;usbcore: registered new interface driver usb-storage&lt;/P&gt;&lt;P&gt;mousedev: PS/2 mouse device common for all mice&lt;/P&gt;&lt;P&gt;i2c /dev entries driver&lt;/P&gt;&lt;P&gt;ina2xx 0-0040: power monitor ina220 (Rshunt = 1000 uOhm)&lt;/P&gt;&lt;P&gt;ina2xx 0-0041: power monitor ina220 (Rshunt = 1000 uOhm)&lt;/P&gt;&lt;P&gt;0-004c supply vcc not found, using dummy regulator&lt;/P&gt;&lt;P&gt;lm90 0-004c: Register 0x4 read failed (-5)&lt;/P&gt;&lt;P&gt;lm90 0-004c: Failed to read convrate register!&lt;/P&gt;&lt;P&gt;lm90 0-004c: Register 0x3 read failed (-5)&lt;/P&gt;&lt;P&gt;lm90 0-004c: Initialization failed!&lt;/P&gt;&lt;P&gt;imx2-wdt 2ad0000.watchdog: timeout 60 sec (nowayout=0)&lt;/P&gt;&lt;P&gt;qoriq_cpufreq: Freescale QorIQ CPU frequency scaling driver&lt;/P&gt;&lt;P&gt;sdhci: Secure Digital Host Controller Interface driver&lt;/P&gt;&lt;P&gt;sdhci: Copyright(c) Pierre Ossman&lt;/P&gt;&lt;P&gt;sdhci-pltfm: SDHCI platform and OF driver helper&lt;/P&gt;&lt;P&gt;sdhci-esdhc 1560000.esdhc: No vmmc regulator found&lt;/P&gt;&lt;P&gt;sdhci-esdhc 1560000.esdhc: No vqmmc regulator found&lt;/P&gt;&lt;P&gt;mmc0: SDHCI controller on 1560000.esdhc [1560000.esdhc] using ADMA 64-bit&lt;/P&gt;&lt;P&gt;caam 1700000.crypto: Instantiated RNG4 SH1&lt;/P&gt;&lt;P&gt;caam 1700000.crypto: device ID = 0x0a14030000000000 (Era 7)&lt;/P&gt;&lt;P&gt;caam 1700000.crypto: job rings = 4, qi = 0&lt;/P&gt;&lt;P&gt;caam algorithms registered in /proc/crypto&lt;/P&gt;&lt;P&gt;caam_jr 1710000.jr: registering rng-caam&lt;/P&gt;&lt;P&gt;caam 1700000.crypto: fsl,sec-v5.0 algorithms registered in /proc/crypto&lt;/P&gt;&lt;P&gt;usbcore: registered new interface driver usbhid&lt;/P&gt;&lt;P&gt;usbhid: USB HID core driver&lt;/P&gt;&lt;P&gt;sgtl5000 1-000a: sgtl5000 revision 0x11&lt;/P&gt;&lt;P&gt;oprofile: using timer interrupt.&lt;/P&gt;&lt;P&gt;Initializing XFRM netlink socket&lt;/P&gt;&lt;P&gt;NET: Registered protocol family 17&lt;/P&gt;&lt;P&gt;NET: Registered protocol family 15&lt;/P&gt;&lt;P&gt;can: controller area network core (rev 20120528 abi 9)&lt;/P&gt;&lt;P&gt;NET: Registered protocol family 29&lt;/P&gt;&lt;P&gt;can: raw protocol (rev 20120528)&lt;/P&gt;&lt;P&gt;Key type dns_resolver registered&lt;/P&gt;&lt;P&gt;Registering SWP/SWPB emulation handler&lt;/P&gt;&lt;P&gt;sgtl5000 1-000a: Using internal LDO instead of VDDD&lt;/P&gt;&lt;P&gt;mmc0: new high speed SDHC card at address e624&lt;/P&gt;&lt;P&gt;mmcblk0: mmc0:e624 SL08G 7.40 GiB &lt;/P&gt;&lt;P&gt; mmcblk0: p1 p2 p3&lt;/P&gt;&lt;P&gt;asoc-simple-card sound: sgtl5000 &amp;lt;-&amp;gt; 2b50000.sai mapping ok&lt;/P&gt;&lt;P&gt;hctosys: unable to open rtc device (rtc0)&lt;/P&gt;&lt;P&gt;ALSA device list:&lt;/P&gt;&lt;P&gt;&amp;nbsp; #0: 2b50000.sai-sgtl5000&lt;/P&gt;&lt;P&gt;RAMDISK: gzip image found at block 0&lt;/P&gt;&lt;P&gt;random: nonblocking pool is initialized&lt;/P&gt;&lt;P&gt;RAMDISK: incomplete write (-28 != 32768)&lt;/P&gt;&lt;P&gt;write error&lt;/P&gt;&lt;P&gt;VFS: Mounted root (ext2 filesystem) on device 1:0.&lt;/P&gt;&lt;P&gt;devtmpfs: mounted&lt;/P&gt;&lt;P&gt;Freeing unused kernel memory: 236K (8055b000 - 80596000)&lt;/P&gt;&lt;P&gt;INIT: version 2.88 booting&lt;/P&gt;&lt;P&gt;EXT4-fs (mmcblk0p3): mounted filesystem with ordered data mode. Opts: (null)&lt;/P&gt;&lt;P&gt;Starting udev&lt;/P&gt;&lt;P&gt;udevd[163]: starting version 182&lt;/P&gt;&lt;P&gt;EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)&lt;/P&gt;&lt;P&gt;Populating dev cache&lt;/P&gt;&lt;P&gt;udev-cache: update failed!&lt;/P&gt;&lt;P&gt;hwclock: can't open '/dev/misc/rtc': No such file or directory&lt;/P&gt;&lt;P&gt;Tue Jun 14 12:03:56 UTC 2016&lt;/P&gt;&lt;P&gt;hwclock: can't open '/dev/misc/rtc': No such file or directory&lt;/P&gt;&lt;P&gt;update-rc.d: /etc/init.d/run-postinsts exists during rc.d purge (continuing)&lt;/P&gt;&lt;P&gt; Removing any system startup links for run-postinsts ...&lt;/P&gt;&lt;P&gt;&amp;nbsp; /etc/rcS.d/S99run-postinsINIT: Entering runlevel: 5&lt;/P&gt;&lt;P&gt;Configuring network interfaces... udhcpc (v1.23.2) started&lt;/P&gt;&lt;P&gt;Sending discover...&lt;/P&gt;&lt;P&gt;Sending discover...&lt;/P&gt;&lt;P&gt;fsl-gianfar soc:ethernet@2d10000 eth0: Link is Up - 1Gbps/Full - flow control rx/tx&lt;/P&gt;&lt;P&gt;Sending discover...&lt;/P&gt;&lt;P&gt;No lease, forking to background&lt;/P&gt;&lt;P&gt;done.&lt;/P&gt;&lt;P&gt;Starting OpenBSD Secure Shell server: sshd&lt;/P&gt;&lt;P&gt;&amp;nbsp; generating ssh RSA key...&lt;/P&gt;&lt;P&gt;hwclock: can't open '/dev/misc/rtc': No such file or directory&lt;/P&gt;&lt;P&gt;Starting syslogd/klogd: done&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Poky (Yocto Project Reference Distro) 2.0.2 ls1021atwr /dev/ttyS0&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;ls1021atwr login: ------------[ cut here ]------------&lt;/P&gt;&lt;P&gt;WARNING: CPU: 0 PID: 0 at /home/jenkins/ci/sdk/master/ls1021atwr/sources/linux/net/sched/sch_generic.c:318 dev_watchdog+0x153/0x1b4()&lt;/P&gt;&lt;P&gt;NETDEV WATCHDOG: eth0 (fsl-gianfar): transmit queue 1 timed out&lt;/P&gt;&lt;P&gt;Modules linked in:&lt;/P&gt;&lt;P&gt;CPU: 0 PID: 0 Comm: swapper/0 Not tainted 4.1.8-rt8+gbd51baf #1&lt;/P&gt;&lt;P&gt;Hardware name: Freescale LS1021A&lt;/P&gt;&lt;P&gt;[&amp;lt;8001d17d&amp;gt;] (unwind_backtrace) from [&amp;lt;8001ad13&amp;gt;] (show_stack+0xb/0xc)&lt;/P&gt;&lt;P&gt;[&amp;lt;8001ad13&amp;gt;] (show_stack) from [&amp;lt;80370741&amp;gt;] (dump_stack+0x51/0x64)&lt;/P&gt;&lt;P&gt;[&amp;lt;80370741&amp;gt;] (dump_stack) from [&amp;lt;8002f811&amp;gt;] (warn_slowpath_common+0x55/0x7c)&lt;/P&gt;&lt;P&gt;[&amp;lt;8002f811&amp;gt;] (warn_slowpath_common) from [&amp;lt;8002f853&amp;gt;] (warn_slowpath_fmt+0x1b/0x24)&lt;/P&gt;&lt;P&gt;[&amp;lt;8002f853&amp;gt;] (warn_slowpath_fmt) from [&amp;lt;8030895f&amp;gt;] (dev_watchdog+0x153/0x1b4)&lt;/P&gt;&lt;P&gt;[&amp;lt;8030895f&amp;gt;] (dev_watchdog) from [&amp;lt;8005c097&amp;gt;] (call_timer_fn.isra.28+0x15/0x5e)&lt;/P&gt;&lt;P&gt;[&amp;lt;8005c097&amp;gt;] (call_timer_fn.isra.28) from [&amp;lt;8005c707&amp;gt;] (run_timer_softirq+0x131/0x162)&lt;/P&gt;&lt;P&gt;[&amp;lt;8005c707&amp;gt;] (run_timer_softirq) from [&amp;lt;80031b91&amp;gt;] (__do_softirq+0x99/0x164)&lt;/P&gt;&lt;P&gt;[&amp;lt;80031b91&amp;gt;] (__do_softirq) from [&amp;lt;80032037&amp;gt;] (irq_exit+0x4b/0x9c)&lt;/P&gt;&lt;P&gt;[&amp;lt;80032037&amp;gt;] (irq_exit) from [&amp;lt;8005357b&amp;gt;] (__handle_domain_irq+0x57/0x74)&lt;/P&gt;&lt;P&gt;[&amp;lt;8005357b&amp;gt;] (__handle_domain_irq) from [&amp;lt;80009329&amp;gt;] (gic_handle_irq+0x29/0x40)&lt;/P&gt;&lt;P&gt;[&amp;lt;80009329&amp;gt;] (gic_handle_irq) from [&amp;lt;8037391b&amp;gt;] (__irq_svc+0x3b/0x5c)&lt;/P&gt;&lt;P&gt;Exception stack(0x80597f58 to 0x80597fa0)&lt;/P&gt;&lt;P&gt;7f40:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 00000001 00000000&lt;/P&gt;&lt;P&gt;7f60: 00000000 800238a1 80596000 00000000 00000000 80597fa8 8059041c 00000001&lt;/P&gt;&lt;P&gt;7f80: 80584850 00000000 80598180 80597fa0 80019351 80019352 40070033 ffffffff&lt;/P&gt;&lt;P&gt;[&amp;lt;8037391b&amp;gt;] (__irq_svc) from [&amp;lt;80019352&amp;gt;] (arch_cpu_idle+0x14/0x1e)&lt;/P&gt;&lt;P&gt;[&amp;lt;80019352&amp;gt;] (arch_cpu_idle) from [&amp;lt;8004e4d7&amp;gt;] (cpu_startup_entry+0x173/0x1ac)&lt;/P&gt;&lt;P&gt;[&amp;lt;8004e4d7&amp;gt;] (cpu_startup_entry) from [&amp;lt;8055b913&amp;gt;] (start_kernel+0x273/0x2dc)&lt;/P&gt;&lt;P&gt;---[ end trace 2203d1c056f202bb ]---&lt;/P&gt;&lt;P&gt;fsl-gianfar soc:ethernet@2d10000 eth0: Link is Up - 1Gbps/Full - flow control rx/tx&lt;/P&gt;&lt;P&gt;fsl-gianfar soc:ethernet@2d10000 eth0: Link is Up - 1Gbps/Full - flow control rx/tx&lt;/P&gt;&lt;P&gt;fsl-gianfar soc:ethernet@2d10000 eth0: Link is Up - 1Gbps/Full - flow control rx/tx&lt;/P&gt;&lt;P&gt;fsl-gianfar soc:ethernet@2d10000 eth0: Link is Up - 1Gbps/Full - flow control rx/tx&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Poky (Yocto Project Reference Distro) 2.0.2 ls1021atwr /dev/ttyS0&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 14 Jun 2016 14:15:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Network-driver-panic-on-TWR-LS1021A-Qoriq-SDK-v2-0/m-p/471418#M694</guid>
      <dc:creator>xkonni</dc:creator>
      <dc:date>2016-06-14T14:15:08Z</dc:date>
    </item>
    <item>
      <title>Re: Network driver panic on TWR-LS1021A - Qoriq SDK-v2.0</title>
      <link>https://community.nxp.com/t5/Layerscape/Network-driver-panic-on-TWR-LS1021A-Qoriq-SDK-v2-0/m-p/471419#M695</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;bump.&lt;/P&gt;&lt;P&gt;this is quite a serious issue. could someone please look into this?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 20 Jun 2016 10:11:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Network-driver-panic-on-TWR-LS1021A-Qoriq-SDK-v2-0/m-p/471419#M695</guid>
      <dc:creator>xkonni</dc:creator>
      <dc:date>2016-06-20T10:11:55Z</dc:date>
    </item>
    <item>
      <title>Re: Network driver panic on TWR-LS1021A - Qoriq SDK-v2.0</title>
      <link>https://community.nxp.com/t5/Layerscape/Network-driver-panic-on-TWR-LS1021A-Qoriq-SDK-v2-0/m-p/471420#M696</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please provide corresponding U-Boot log. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 20 Jun 2016 11:46:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Network-driver-panic-on-TWR-LS1021A-Qoriq-SDK-v2-0/m-p/471420#M696</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2016-06-20T11:46:18Z</dc:date>
    </item>
    <item>
      <title>Re: Network driver panic on TWR-LS1021A - Qoriq SDK-v2.0</title>
      <link>https://community.nxp.com/t5/Layerscape/Network-driver-panic-on-TWR-LS1021A-Qoriq-SDK-v2-0/m-p/471421#M697</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;sure, just created a fresh one (rootfs, uimage, dtb directly from sdk2.0).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks for your help!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 20 Jun 2016 13:59:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Network-driver-panic-on-TWR-LS1021A-Qoriq-SDK-v2-0/m-p/471421#M697</guid>
      <dc:creator>xkonni</dc:creator>
      <dc:date>2016-06-20T13:59:07Z</dc:date>
    </item>
    <item>
      <title>Re: Network driver panic on TWR-LS1021A - Qoriq SDK-v2.0</title>
      <link>https://community.nxp.com/t5/Layerscape/Network-driver-panic-on-TWR-LS1021A-Qoriq-SDK-v2-0/m-p/471422#M698</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Were you using SDK 2.0 pre-built images?&lt;/P&gt;&lt;P&gt;If "not" - what were the kernel build options?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 Jun 2016 17:07:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Network-driver-panic-on-TWR-LS1021A-Qoriq-SDK-v2-0/m-p/471422#M698</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2016-06-23T17:07:05Z</dc:date>
    </item>
    <item>
      <title>Re: Network driver panic on TWR-LS1021A - Qoriq SDK-v2.0</title>
      <link>https://community.nxp.com/t5/Layerscape/Network-driver-panic-on-TWR-LS1021A-Qoriq-SDK-v2-0/m-p/471423#M699</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes this log was with the pre-built sdk uImage, dtb, rootfs. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But custom images with a slightly modified ls1021a_defconfig, yocto sdk2 branch lead to the same issue.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 Jun 2016 17:11:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Network-driver-panic-on-TWR-LS1021A-Qoriq-SDK-v2-0/m-p/471423#M699</guid>
      <dc:creator>xkonni</dc:creator>
      <dc:date>2016-06-23T17:11:14Z</dc:date>
    </item>
    <item>
      <title>Re: Network driver panic on TWR-LS1021A - Qoriq SDK-v2.0</title>
      <link>https://community.nxp.com/t5/Layerscape/Network-driver-panic-on-TWR-LS1021A-Qoriq-SDK-v2-0/m-p/471424#M700</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please check the board switch settings - what are they? &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Jun 2016 18:34:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Network-driver-panic-on-TWR-LS1021A-Qoriq-SDK-v2-0/m-p/471424#M700</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2016-06-28T18:34:51Z</dc:date>
    </item>
    <item>
      <title>Re: Network driver panic on TWR-LS1021A - Qoriq SDK-v2.0</title>
      <link>https://community.nxp.com/t5/Layerscape/Network-driver-panic-on-TWR-LS1021A-Qoriq-SDK-v2-0/m-p/471425#M701</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;SW2[1:8] = 0010 1111&lt;/P&gt;&lt;P&gt;SW3[1:8] = 0110 0001&lt;/P&gt;&lt;P&gt;like described in the demo pdf.&lt;/P&gt;&lt;P&gt;but apparently the issue was that I didnt flash the new u-boot to the sdcard. issue seems resolved.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 29 Jun 2016 14:12:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Network-driver-panic-on-TWR-LS1021A-Qoriq-SDK-v2-0/m-p/471425#M701</guid>
      <dc:creator>xkonni</dc:creator>
      <dc:date>2016-06-29T14:12:41Z</dc:date>
    </item>
    <item>
      <title>Re: Network driver panic on TWR-LS1021A - Qoriq SDK-v2.0</title>
      <link>https://community.nxp.com/t5/Layerscape/Network-driver-panic-on-TWR-LS1021A-Qoriq-SDK-v2-0/m-p/471426#M702</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;All images of u-boot, rcw and kernel 4.1.8-rt8 are booting fine and network driver is also working fine on TWR-LS1021A-PB Rev 2.0. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 Jul 2016 11:17:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Network-driver-panic-on-TWR-LS1021A-Qoriq-SDK-v2-0/m-p/471426#M702</guid>
      <dc:creator>skrishnakar</dc:creator>
      <dc:date>2016-07-15T11:17:44Z</dc:date>
    </item>
  </channel>
</rss>