<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LayerscapeのトピックRe: ls1028ardb gpio control(/sys/class/gpio/export)</title>
    <link>https://community.nxp.com/t5/Layerscape/ls1028ardb-gpio-control-sys-class-gpio-export/m-p/1176890#M6909</link>
    <description>&lt;P&gt;&lt;SPAN&gt;If you need to trigger gpiolib operations from device tree at bootup itself then you will need to either have this logic in our existing driver's probe function or write your own driver. Basically you need to use API's like- gpiod_request, gpiod_export, gpiod_export_link etc in your driver.&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Tue, 03 Nov 2020 02:33:53 GMT</pubDate>
    <dc:creator>yipingwang</dc:creator>
    <dc:date>2020-11-03T02:33:53Z</dc:date>
    <item>
      <title>ls1028ardb gpio control(/sys/class/gpio/export)</title>
      <link>https://community.nxp.com/t5/Layerscape/ls1028ardb-gpio-control-sys-class-gpio-export/m-p/1173859#M6869</link>
      <description>&lt;P&gt;Hi, I'm using ls1028ardb and&amp;nbsp;&lt;SPAN&gt;Trying to control gpio.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;It is possible to control gpio with the command below.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;echo 500 &amp;gt; /sys/class/gpio/export&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Entering the command creates the gpio500 folder.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#0000FF"&gt;&lt;SPAN&gt;What I want to do is to have the gpio500 folder present without having to enter a command at boot time.&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;So I'm modifying the dts file and I don't know how to modify it.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Below is the file contents of fsl-ls1028a.dtsi.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="4"&gt;gpio1: gpio@2300000 {&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="4"&gt;compatible = "fsl,ls1028a-gpio","fsl,qoriq-gpio";&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="4"&gt;reg = &amp;lt;0x0 0x2300000 0x0 0x10000&amp;gt;;&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="4"&gt;interrupts = &amp;lt;GIC_SPI 36 IRQ_TYPE_LEVEL_HIGH&amp;gt;;&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="4"&gt;gpio-controller;&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="4"&gt;#gpio-cells = &amp;lt;2&amp;gt;;&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="4"&gt;interrupt-controller;&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="4"&gt;#interrupt-cells = &amp;lt;2&amp;gt;;&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="4"&gt;little-endian;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="4"&gt;};&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="4"&gt;gpio2: gpio@2310000 {&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="4"&gt;compatible = "fsl,ls1028a-gpio","fsl,qoriq-gpio";&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="4"&gt;reg = &amp;lt;0x0 0x2310000 0x0 0x10000&amp;gt;;&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="4"&gt;interrupts = &amp;lt;GIC_SPI 36 IRQ_TYPE_LEVEL_HIGH&amp;gt;;&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="4"&gt;gpio-controller;&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="4"&gt;#gpio-cells = &amp;lt;2&amp;gt;;&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="4"&gt;interrupt-controller;&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="4"&gt;#interrupt-cells = &amp;lt;2&amp;gt;;&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="4"&gt;little-endian;&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="4"&gt;};&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="4"&gt;gpio3: gpio@2320000 {&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="4"&gt;compatible = "fsl,ls1028a-gpio","fsl,qoriq-gpio";&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="4"&gt;reg = &amp;lt;0x0 0x2320000 0x0 0x10000&amp;gt;;&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="4"&gt;interrupts = &amp;lt;GIC_SPI 37 IRQ_TYPE_LEVEL_HIGH&amp;gt;;&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="4"&gt;gpio-controller;&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="4"&gt;#gpio-cells = &amp;lt;2&amp;gt;;&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="4"&gt;interrupt-controller;&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="4"&gt;#interrupt-cells = &amp;lt;2&amp;gt;;&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="4"&gt;little-endian;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="4"&gt;};&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;And nothing is written in the dts file.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;So, as a result of inputting below, "test1" was created in&amp;nbsp;/sys/firmware/devicetree/base/soc/gpio@2300000/gpio but not in /sys/class/gpio/.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;FONT size="4"&gt;&amp;amp;gpio3 {&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="4"&gt;compatible="gpio-test";&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="4"&gt;pinctrl-names="default";&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="4"&gt;pinctrl-0 = &amp;lt;&amp;amp;gpio3&amp;gt;;&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="4"&gt;status = "okay";&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="4"&gt;test1{&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="4"&gt;label="test1";&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="4"&gt;gpios = &amp;lt;&amp;amp;gpio3 9 0&amp;gt;;&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="4"&gt;default-state = "on";&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="4"&gt;};&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="4"&gt;};&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Please let me know if it is right to modify dts file and how to modify it if right.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 27 Oct 2020 13:06:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/ls1028ardb-gpio-control-sys-class-gpio-export/m-p/1173859#M6869</guid>
      <dc:creator>pjw</dc:creator>
      <dc:date>2020-10-27T13:06:56Z</dc:date>
    </item>
    <item>
      <title>Re: ls1028ardb gpio control(/sys/class/gpio/export)</title>
      <link>https://community.nxp.com/t5/Layerscape/ls1028ardb-gpio-control-sys-class-gpio-export/m-p/1176890#M6909</link>
      <description>&lt;P&gt;&lt;SPAN&gt;If you need to trigger gpiolib operations from device tree at bootup itself then you will need to either have this logic in our existing driver's probe function or write your own driver. Basically you need to use API's like- gpiod_request, gpiod_export, gpiod_export_link etc in your driver.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 03 Nov 2020 02:33:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/ls1028ardb-gpio-control-sys-class-gpio-export/m-p/1176890#M6909</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2020-11-03T02:33:53Z</dc:date>
    </item>
  </channel>
</rss>