<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: How and Which CWSIS-DAP adapter i should use to program the LS1201A in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/How-and-Which-CWSIS-DAP-adapter-i-should-use-to-program-the/m-p/1170638#M6815</link>
    <description>&lt;P&gt;It looks like that the LS1021a is used.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The TWR-LS1021a board uses USB-to-UART bridge - MK20DX128VFM5. This bridge is used for CMSIS-DAP from MBED:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://os.mbed.com/handbook/CMSIS-DAP" target="_blank"&gt;https://os.mbed.com/handbook/CMSIS-DAP&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Use the following page for downloading CMSIS-DAP driver:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://os.mbed.com/handbook/Windows-serial-configuration#1-download-the-mbed-windows-serial-port" target="_blank"&gt;https://os.mbed.com/handbook/Windows-serial-configuration#1-download-the-mbed-windows-serial-port&lt;/A&gt;&lt;/P&gt;</description>
    <pubDate>Wed, 21 Oct 2020 02:46:34 GMT</pubDate>
    <dc:creator>Pavel</dc:creator>
    <dc:date>2020-10-21T02:46:34Z</dc:date>
    <item>
      <title>How and Which CWSIS-DAP adapter i should use to program the LS1201A</title>
      <link>https://community.nxp.com/t5/Layerscape/How-and-Which-CWSIS-DAP-adapter-i-should-use-to-program-the/m-p/1170225#M6812</link>
      <description>&lt;P&gt;How and Which CWSIS-DAP adapter i should use to program the LS1201A&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I don't have the&amp;nbsp;CodeWarrior TAP, and i see the&amp;nbsp;CodeWarrior TAP studio can use&amp;nbsp; CWSIS-DAP,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I want to know which adapter should i use to program the LS1201A&lt;/P&gt;</description>
      <pubDate>Tue, 20 Oct 2020 08:54:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/How-and-Which-CWSIS-DAP-adapter-i-should-use-to-program-the/m-p/1170225#M6812</guid>
      <dc:creator>nxpaudiencedong</dc:creator>
      <dc:date>2020-10-20T08:54:39Z</dc:date>
    </item>
    <item>
      <title>Re: How and Which CWSIS-DAP adapter i should use to program the LS1201A</title>
      <link>https://community.nxp.com/t5/Layerscape/How-and-Which-CWSIS-DAP-adapter-i-should-use-to-program-the/m-p/1170638#M6815</link>
      <description>&lt;P&gt;It looks like that the LS1021a is used.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The TWR-LS1021a board uses USB-to-UART bridge - MK20DX128VFM5. This bridge is used for CMSIS-DAP from MBED:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://os.mbed.com/handbook/CMSIS-DAP" target="_blank"&gt;https://os.mbed.com/handbook/CMSIS-DAP&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Use the following page for downloading CMSIS-DAP driver:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://os.mbed.com/handbook/Windows-serial-configuration#1-download-the-mbed-windows-serial-port" target="_blank"&gt;https://os.mbed.com/handbook/Windows-serial-configuration#1-download-the-mbed-windows-serial-port&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 21 Oct 2020 02:46:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/How-and-Which-CWSIS-DAP-adapter-i-should-use-to-program-the/m-p/1170638#M6815</guid>
      <dc:creator>Pavel</dc:creator>
      <dc:date>2020-10-21T02:46:34Z</dc:date>
    </item>
    <item>
      <title>Re: How and Which CWSIS-DAP adapter i should use to program the LS1201A</title>
      <link>https://community.nxp.com/t5/Layerscape/How-and-Which-CWSIS-DAP-adapter-i-should-use-to-program-the/m-p/1171820#M6837</link>
      <description>&lt;P&gt;i donwload the driver and config the codewarrior to connect the board ls1201a and start debug and get the error:&lt;/P&gt;&lt;P&gt;启动1111-core0_RAM_LS1021ATWR_Download出错&lt;BR /&gt;CCSProtocolPlugin : Failed to correctly configure the JTAG chain&lt;/P&gt;</description>
      <pubDate>Thu, 22 Oct 2020 12:05:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/How-and-Which-CWSIS-DAP-adapter-i-should-use-to-program-the/m-p/1171820#M6837</guid>
      <dc:creator>nxpaudiencedong</dc:creator>
      <dc:date>2020-10-22T12:05:46Z</dc:date>
    </item>
    <item>
      <title>Re: How and Which CWSIS-DAP adapter i should use to program the LS1201A</title>
      <link>https://community.nxp.com/t5/Layerscape/How-and-Which-CWSIS-DAP-adapter-i-should-use-to-program-the/m-p/1172103#M6840</link>
      <description>&lt;P&gt;IN LS1201A, here are J12, J2 and J10,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;J12 - connect to&amp;nbsp;LS1021ASE7MQB's jtag&lt;/P&gt;&lt;P&gt;J2 - connect to&amp;nbsp;MK20DX128VFM5's jtag&amp;nbsp;&lt;/P&gt;&lt;P&gt;J10 - connect to&amp;nbsp;LCMXO1200C-3FTN256C's jtag&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;if i want to use CWSIS-DAP to debug the board, which connectter should i use?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 23 Oct 2020 01:16:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/How-and-Which-CWSIS-DAP-adapter-i-should-use-to-program-the/m-p/1172103#M6840</guid>
      <dc:creator>nxpaudiencedong</dc:creator>
      <dc:date>2020-10-23T01:16:03Z</dc:date>
    </item>
    <item>
      <title>Re: How and Which CWSIS-DAP adapter i should use to program the LS1201A</title>
      <link>https://community.nxp.com/t5/Layerscape/How-and-Which-CWSIS-DAP-adapter-i-should-use-to-program-the/m-p/1172913#M6856</link>
      <description>&lt;P&gt;Use the J12 for connection to the LS1012a.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Look at the Section 8.2 of the CW_ARMv7_Targeting_Manual.pdf file.&lt;/P&gt;
&lt;P&gt;RCW override is not supported with a CMSIS-DAP connection.&lt;/P&gt;
&lt;P&gt;When using the CMSIS-DAP probe, it is recommended to verify operation parameters and RCW correctness before continuing. Failure to program a compatible RCW may result problem for connection using CMSIS-DAP&lt;/P&gt;
&lt;P&gt;Check RCW on your board.&lt;/P&gt;</description>
      <pubDate>Mon, 26 Oct 2020 07:11:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/How-and-Which-CWSIS-DAP-adapter-i-should-use-to-program-the/m-p/1172913#M6856</guid>
      <dc:creator>Pavel</dc:creator>
      <dc:date>2020-10-26T07:11:02Z</dc:date>
    </item>
  </channel>
</rss>