<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: How to demonstrate LS1043A-VNP' DPAA function? in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/How-to-demonstrate-LS1043A-VNP-DPAA-function/m-p/1168572#M6795</link>
    <description>&lt;P&gt;The dts&amp;nbsp;&lt;SPAN&gt;fsl-ls1043a-rdb-usdpaa.dts is used for DPDK, all Ethernet ports are assigned to the user space.&amp;nbsp;DPDK is an user space packet processing framework.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;File fsl-ls1043a-rdb-sdk.dtb is the normal dts file for Linux Kernel.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;DPAA is the hardware mechanism to provide hardware acceleration of packet queues. DPAA module cannot be disabled in networking packets processing.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Fri, 16 Oct 2020 03:43:40 GMT</pubDate>
    <dc:creator>yipingwang</dc:creator>
    <dc:date>2020-10-16T03:43:40Z</dc:date>
    <item>
      <title>How to demonstrate LS1043A-VNP' DPAA function?</title>
      <link>https://community.nxp.com/t5/Layerscape/How-to-demonstrate-LS1043A-VNP-DPAA-function/m-p/1166099#M6757</link>
      <description>&lt;P&gt;How to demonstrate&amp;nbsp; DPAA function on the LS1043A-VNP board?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I only refer to this manual:&amp;nbsp;MPC-LS-VNP-RD-UM.pdf to burn the firmware:&amp;nbsp;RDB-EAR0.1-Binaries&lt;/P&gt;&lt;P&gt;All the steps are same as the manual,except the dtb file.&lt;/P&gt;&lt;P&gt;One burn the default dtb file:&amp;nbsp;fsl-ls1043a-rdb-sdk.dtb in&amp;nbsp; emmc block.the kernel boot logs and the rootfs ifconfig result are in this file: ls1043_vnp_without_dpaa_001.txt.&amp;nbsp; &amp;nbsp;And the ifconfig result looks normal.&lt;/P&gt;&lt;P&gt;Another burn the usdpaa dtb file: fsl-ls1043a-rdb-usdpaa.dtb (from LSDK source) in emmc block, and fix the uboot mmcboot string.&amp;nbsp;the kernel boot logs and the rootfs ifconfig result are in this file: ls1043_vnp_usdpaa_001.txt. And the ifconfig result looks abnormal: a lot of net devices like eth0 ... are lost.&lt;/P&gt;</description>
      <pubDate>Mon, 12 Oct 2020 13:21:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/How-to-demonstrate-LS1043A-VNP-DPAA-function/m-p/1166099#M6757</guid>
      <dc:creator>d-z-c</dc:creator>
      <dc:date>2020-10-12T13:21:40Z</dc:date>
    </item>
    <item>
      <title>Re: How to demonstrate LS1043A-VNP' DPAA function?</title>
      <link>https://community.nxp.com/t5/Layerscape/How-to-demonstrate-LS1043A-VNP-DPAA-function/m-p/1166531#M6763</link>
      <description>&lt;P&gt;When you use USDPAA dts file&amp;nbsp;&lt;SPAN&gt;&amp;nbsp;fsl-ls1043a-rdb-usdpaa.dtb, all Ethernet ports have been assigned to USDPAA, so you cannot see any Ethernet port in Linux.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;In fsl,dpaa device node definition in&amp;nbsp;arch/arm64/boot/dts/freescale/fsl-ls1043a-rdb-usdpaa.dts, if you delete&amp;nbsp; &lt;A href="mailto:ethernet@0" target="_blank"&gt;ethernet@0&lt;/A&gt;&amp;nbsp;definition, you will find eth0 is assigned to Linux,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks,&lt;/P&gt;
&lt;P&gt;Yiping&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 13 Oct 2020 06:58:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/How-to-demonstrate-LS1043A-VNP-DPAA-function/m-p/1166531#M6763</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2020-10-13T06:58:05Z</dc:date>
    </item>
    <item>
      <title>Re: How to demonstrate LS1043A-VNP' DPAA function?</title>
      <link>https://community.nxp.com/t5/Layerscape/How-to-demonstrate-LS1043A-VNP-DPAA-function/m-p/1166544#M6764</link>
      <description>&lt;P&gt;Hi, YiPing&lt;/P&gt;&lt;P&gt;&amp;nbsp;Thank for you answer&lt;/P&gt;&lt;P&gt;&amp;nbsp;I could understand why there are no any ethernet port on Linux.&lt;/P&gt;&lt;P&gt;And do you have any idea to build a simple demo about the DPAA function(uboot,kernel configure,Linux rootfs references, and so on)，I just want to know how to use it and&amp;nbsp;How does it work.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;TIC.&lt;/P&gt;</description>
      <pubDate>Tue, 13 Oct 2020 07:15:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/How-to-demonstrate-LS1043A-VNP-DPAA-function/m-p/1166544#M6764</guid>
      <dc:creator>d-z-c</dc:creator>
      <dc:date>2020-10-13T07:15:39Z</dc:date>
    </item>
    <item>
      <title>Re: How to demonstrate LS1043A-VNP' DPAA function?</title>
      <link>https://community.nxp.com/t5/Layerscape/How-to-demonstrate-LS1043A-VNP-DPAA-function/m-p/1167227#M6779</link>
      <description>&lt;P&gt;DPAA driver is enabled in Linux Kernel by default. You could run any networking related application(eg. ping, iperf).&lt;/P&gt;
&lt;P&gt;You could refer to section "8.2 DPAA1-specific Software" in LSDK 20.04 user manual for how DPAA1 works.&lt;/P&gt;</description>
      <pubDate>Wed, 14 Oct 2020 07:07:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/How-to-demonstrate-LS1043A-VNP-DPAA-function/m-p/1167227#M6779</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2020-10-14T07:07:42Z</dc:date>
    </item>
    <item>
      <title>Re: How to demonstrate LS1043A-VNP' DPAA function?</title>
      <link>https://community.nxp.com/t5/Layerscape/How-to-demonstrate-LS1043A-VNP-DPAA-function/m-p/1167367#M6780</link>
      <description>&lt;P&gt;Hi YiPing:&lt;BR /&gt;Do you mean both the two dtbs:fsl-ls1043a-rdb-sdk.dtb and fsl-ls1043a-rdb-usdpaa.dts&lt;BR /&gt;are DPAA driver enabled in Linux Kernel by default?&lt;BR /&gt;&lt;BR /&gt;And How to enable / disable the DPAA function? then we could Compare their effects.&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;TIC&lt;/P&gt;</description>
      <pubDate>Wed, 14 Oct 2020 09:46:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/How-to-demonstrate-LS1043A-VNP-DPAA-function/m-p/1167367#M6780</guid>
      <dc:creator>d-z-c</dc:creator>
      <dc:date>2020-10-14T09:46:05Z</dc:date>
    </item>
    <item>
      <title>Re: How to demonstrate LS1043A-VNP' DPAA function?</title>
      <link>https://community.nxp.com/t5/Layerscape/How-to-demonstrate-LS1043A-VNP-DPAA-function/m-p/1168572#M6795</link>
      <description>&lt;P&gt;The dts&amp;nbsp;&lt;SPAN&gt;fsl-ls1043a-rdb-usdpaa.dts is used for DPDK, all Ethernet ports are assigned to the user space.&amp;nbsp;DPDK is an user space packet processing framework.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;File fsl-ls1043a-rdb-sdk.dtb is the normal dts file for Linux Kernel.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;DPAA is the hardware mechanism to provide hardware acceleration of packet queues. DPAA module cannot be disabled in networking packets processing.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 16 Oct 2020 03:43:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/How-to-demonstrate-LS1043A-VNP-DPAA-function/m-p/1168572#M6795</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2020-10-16T03:43:40Z</dc:date>
    </item>
  </channel>
</rss>