<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic OpenIL on the LS2028ARDB-PA in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/OpenIL-on-the-LS2028ARDB-PA/m-p/1163983#M6750</link>
    <description>&lt;P&gt;Doing an OpenIL 1.9 build on the&amp;nbsp;LS2028ARDB-PA. Follow instructions in the users manual (V1.9). Used the make on a&amp;nbsp; fii-ls1028tsn-64b defconfig for an SD card. The sdcard.img file&amp;nbsp; created sets the DDR memory to 2 GB DDR4, 32-Bit,Cl=11, ECC off. It should be&amp;nbsp;&amp;nbsp;4 GB DDR4, 32-Bit,Cl=11, ECC on. The boot hangs&amp;nbsp; because of this. What file needs to be modified in order to set the DDR config correctly?.&lt;/P&gt;</description>
    <pubDate>Wed, 07 Oct 2020 14:46:17 GMT</pubDate>
    <dc:creator>tsn_development</dc:creator>
    <dc:date>2020-10-07T14:46:17Z</dc:date>
    <item>
      <title>OpenIL on the LS2028ARDB-PA</title>
      <link>https://community.nxp.com/t5/Layerscape/OpenIL-on-the-LS2028ARDB-PA/m-p/1163983#M6750</link>
      <description>&lt;P&gt;Doing an OpenIL 1.9 build on the&amp;nbsp;LS2028ARDB-PA. Follow instructions in the users manual (V1.9). Used the make on a&amp;nbsp; fii-ls1028tsn-64b defconfig for an SD card. The sdcard.img file&amp;nbsp; created sets the DDR memory to 2 GB DDR4, 32-Bit,Cl=11, ECC off. It should be&amp;nbsp;&amp;nbsp;4 GB DDR4, 32-Bit,Cl=11, ECC on. The boot hangs&amp;nbsp; because of this. What file needs to be modified in order to set the DDR config correctly?.&lt;/P&gt;</description>
      <pubDate>Wed, 07 Oct 2020 14:46:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/OpenIL-on-the-LS2028ARDB-PA/m-p/1163983#M6750</guid>
      <dc:creator>tsn_development</dc:creator>
      <dc:date>2020-10-07T14:46:17Z</dc:date>
    </item>
    <item>
      <title>Re: OpenIL on the LS2028ARDB-PA</title>
      <link>https://community.nxp.com/t5/Layerscape/OpenIL-on-the-LS2028ARDB-PA/m-p/1166134#M6758</link>
      <description>&lt;P&gt;LS2028ARDB-PA is an invalid part number, so it is not clear what board you are trying to build for. If it is LS1028ARDB-PA, the valid build target for it is nxp_ls1028ardb-64b_defconfig. Building this target should generate all files necessary for SD card boot.&amp;nbsp; Memory size is detected in&amp;nbsp; DDR initialization code in TF-A. If you want to know the details, see the code in this directory:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://source.codeaurora.org/external/qoriq/qoriq-components/atf/tree/plat/nxp/soc-ls1028/ls1028ardb" target="_blank"&gt;https://source.codeaurora.org/external/qoriq/qoriq-components/atf/tree/plat/nxp/soc-ls1028/ls1028ardb&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;BR /&gt;Platon&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 12 Oct 2020 14:11:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/OpenIL-on-the-LS2028ARDB-PA/m-p/1166134#M6758</guid>
      <dc:creator>bpe</dc:creator>
      <dc:date>2020-10-12T14:11:14Z</dc:date>
    </item>
  </channel>
</rss>