<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Kernel panic occurs during operation after booting the LS1012A. in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/Kernel-panic-occurs-during-operation-after-booting-the-LS1012A/m-p/1163852#M6749</link>
    <description>&lt;P&gt;Again I solved it!!&lt;/P&gt;&lt;P&gt;I found that the DDR part marked on the circuit diagram of XFRWY-LS1012A RevB and the DDR mounted on the board are different.&lt;/P&gt;&lt;P&gt;The circuit diagram is 512MB, and the board is equipped with 1GB.&lt;/P&gt;&lt;P&gt;So, by modifying the two parts as below, kernel panic did not occur.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;vi plat/nxp/soc-ls1012/ls1012afrwy/platform_def.h&lt;/P&gt;&lt;P&gt;#define PLAT_DEF_DRAM0_SIZE &lt;FONT color="#FF0000"&gt;0x20000000&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;vi board/freescale/ls1012afrdm/ls1012afrdm.c&lt;/P&gt;&lt;P&gt;gd-&amp;gt;ram_size = &lt;FONT color="#FF0000"&gt;SYS_SDRAM_SIZE_512&lt;/FONT&gt;;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Gyosun.&lt;/P&gt;</description>
    <pubDate>Wed, 07 Oct 2020 10:46:40 GMT</pubDate>
    <dc:creator>gyosunshim</dc:creator>
    <dc:date>2020-10-07T10:46:40Z</dc:date>
    <item>
      <title>Kernel panic occurs during operation after booting the LS1012A.</title>
      <link>https://community.nxp.com/t5/Layerscape/Kernel-panic-occurs-during-operation-after-booting-the-LS1012A/m-p/1163452#M6746</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am using the LS1012A-FRWY custom board.&lt;/P&gt;&lt;P&gt;I normally ported to the Linux console using an SD card.&lt;/P&gt;&lt;P&gt;The SDK used LSDK18.12-kernel4.9.&lt;/P&gt;&lt;P&gt;I haven't tested a lot, but if I use the cp command or the tar command, a kernel panic occurs.&lt;/P&gt;&lt;P&gt;When testing on the LS1012A-FRWY board, kernel panic does not occur. Why are you doing this?&lt;/P&gt;&lt;TABLE border="1" width="100%"&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD width="100%"&gt;&lt;P&gt;U-Boot 2018.09-dirty (Oct 06 2020 - 11:34:29 +0000)&lt;/P&gt;&lt;P&gt;SoC: LS1012AE Rev2.0 (0x87040020)&lt;BR /&gt;Clock Configuration:&lt;BR /&gt;CPU0(A53):1000 MHz&lt;BR /&gt;Bus: 250 MHz DDR: 1000 MT/s&lt;BR /&gt;Reset Configuration Word (RCW):&lt;BR /&gt;00000000: 0800000a 00000000 00000000 00000000&lt;BR /&gt;00000010: 33050000 c000000c 40000000 00001800&lt;BR /&gt;00000020: 00000000 00000000 00000000 000c4572&lt;BR /&gt;00000030: 00000000 1082a120 00000096 00000000&lt;BR /&gt;I2C: ready&lt;BR /&gt;DRAM: 958 MiB&lt;BR /&gt;WARNING: Calling __hwconfig without a buffer and before environment is ready&lt;BR /&gt;Using SERDES1 Protocol: 13061 (0x3305)&lt;BR /&gt;MMC: FSL_SDHC: 0, FSL_SDHC: 1&lt;BR /&gt;Loading Environment from SPI Flash... SF: Detected mx25u25645g with page size 256 Bytes, erase size 64 KiB, total 32 MiB&lt;BR /&gt;SF: Warning - Only lower 16MiB accessible, Full access #define CONFIG_SPI_FLASH_BAR&lt;BR /&gt;OK&lt;BR /&gt;In: serial&lt;BR /&gt;Out: serial&lt;BR /&gt;Err: serial&lt;BR /&gt;Model: FRWY-LS1012A Board&lt;BR /&gt;Board: FRWY-LS1012A Version: unknownNet: PFE class pe firmware&lt;BR /&gt;PFE tmu pe firmware&lt;BR /&gt;eth0: pfe_eth0, eth1: pfe_eth1&lt;BR /&gt;Hit any key to stop autoboot: 0&lt;BR /&gt;=&amp;gt;&lt;BR /&gt;=&amp;gt;&lt;BR /&gt;=&amp;gt;&lt;BR /&gt;=&amp;gt;&lt;BR /&gt;=&amp;gt; setenv mmc_boot 'pfe stop; if mmc dev ${devnum}; then setenv devtype mmc; run scan_dev_for_boot_part; fi'&lt;BR /&gt;=&amp;gt; setenv bootargs 'console=ttyS0,115200 root=/dev/mmcblk0p3 rw earlycon=uart8250,mmio,0x21c0500 rootdelay=3'&lt;BR /&gt;=&amp;gt; setenv bootcmd 'run distro_bootcmd; run sd_bootcmd; env exists secureboot &amp;amp;&amp;amp; esbc_halt;'&lt;BR /&gt;=&amp;gt; saveenv&lt;BR /&gt;Saving Environment to SPI Flash... SF: Detected mx25u25645g with page size 256 Bytes, erase size 64 KiB, total 32 MiB&lt;BR /&gt;SF: Warning - Only lower 16MiB accessible, Full access #define CONFIG_SPI_FLASH_BAR&lt;BR /&gt;Erasing SPI flash...Writing to SPI flash...done&lt;BR /&gt;OK&lt;BR /&gt;=&amp;gt; boot&lt;BR /&gt;Stopping PFE...&lt;BR /&gt;switch to partitions #0, OK&lt;BR /&gt;mmc0 is current device&lt;BR /&gt;Scanning mmc 0:1...&lt;BR /&gt;Scanning mmc 0:2...&lt;BR /&gt;Found U-Boot script /ls1012afrwy_boot.scr&lt;BR /&gt;964 bytes read in 5 ms (187.5 KiB/s)&lt;BR /&gt;## Executing script at 80000000&lt;BR /&gt;17504768 bytes read in 892 ms (18.7 MiB/s)&lt;BR /&gt;14295 bytes read in 9 ms (1.5 MiB/s)&lt;BR /&gt;## Flattened Device Tree blob at 90000000&lt;BR /&gt;Booting using the fdt blob at 0x90000000&lt;BR /&gt;Using Device Tree in place at 0000000090000000, end 00000000900067d6&lt;BR /&gt;WARNING: fdt_fixup_stdout: could not read serial0 alias: FDT_ERR_NOTFOUND&lt;BR /&gt;NOTICE: RNG: INSTANTIATED&lt;BR /&gt;PCIe0: pcie@3400000 Root Complex: no link&lt;/P&gt;&lt;P&gt;Starting kernel ...&lt;/P&gt;&lt;P&gt;[ 0.000000] Booting Linux on physical CPU 0x0&lt;BR /&gt;[ 0.000000] Linux version 4.9.140-dirty (root@fbubuntu) (gcc version 7.5.0 (Ubuntu/Linaro 7.5.0-3ubuntu1~18.04) ) #1 SMP PREEMPT Tue Oct 6 11:29:58 UTC 2020&lt;BR /&gt;[ 0.000000] Boot CPU: AArch64 Processor [410fd034]&lt;BR /&gt;[ 0.000000] earlycon: uart8250 at MMIO 0x00000000021c0500 (options '')&lt;BR /&gt;[ 0.000000] bootconsole [uart8250] enabled&lt;BR /&gt;[ 0.000000] efi: Getting EFI parameters from FDT:&lt;BR /&gt;[ 0.000000] efi: UEFI not found.&lt;BR /&gt;[ 0.000000] cma: Reserved 16 MiB at 0x00000000bac00000&lt;BR /&gt;[ 0.000000] NUMA: No NUMA configuration found&lt;BR /&gt;[ 0.000000] NUMA: Faking a node at [mem 0x0000000000000000-0x00000000bbdfffff]&lt;BR /&gt;[ 0.000000] NUMA: Adding memblock [0x80000000 - 0xbbdfffff] on node 0&lt;BR /&gt;[ 0.000000] NUMA: Initmem setup node 0 [mem 0x80000000-0xbbdfffff]&lt;BR /&gt;[ 0.000000] NUMA: NODE_DATA [mem 0xbbdde800-0xbbddffbf]&lt;BR /&gt;[ 0.000000] Zone ranges:&lt;BR /&gt;[ 0.000000] DMA [mem 0x0000000080000000-0x00000000bbdfffff]&lt;BR /&gt;[ 0.000000] Normal empty&lt;BR /&gt;[ 0.000000] Movable zone start for each node&lt;BR /&gt;[ 0.000000] Early memory node ranges&lt;BR /&gt;[ 0.000000] node 0: [mem 0x0000000080000000-0x00000000bbdfffff]&lt;BR /&gt;[ 0.000000] Initmem setup node 0 [mem 0x0000000080000000-0x00000000bbdfffff]&lt;BR /&gt;[ 0.000000] psci: probing for conduit method from DT.&lt;BR /&gt;[ 0.000000] psci: PSCIv1.1 detected in firmware.&lt;BR /&gt;[ 0.000000] psci: Using standard PSCI v0.2 function IDs&lt;BR /&gt;[ 0.000000] psci: MIGRATE_INFO_TYPE not supported.&lt;BR /&gt;[ 0.000000] psci: SMC Calling Convention v1.1&lt;BR /&gt;[ 0.000000] percpu: Embedded 22 pages/cpu @ffff80003bdc3000 s50904 r8192 d31016 u90112&lt;BR /&gt;[ 0.000000] Detected VIPT I-cache on CPU0&lt;BR /&gt;[ 0.000000] CPU features: enabling workaround for ARM erratum 845719&lt;BR /&gt;[ 0.000000] Built 1 zonelists in Node order, mobility grouping on. Total pages: 241416&lt;BR /&gt;[ 0.000000] Policy zone: DMA&lt;BR /&gt;[ 0.000000] Kernel command line: console=ttyS0,115200 earlycon=uart8250,mmio,0x21c0500 root=PARTUUID=000068a6-03 rw rootwait&lt;BR /&gt;[ 0.000000] PID hash table entries: 4096 (order: 3, 32768 bytes)&lt;BR /&gt;[ 0.000000] Memory: 917620K/980992K available (10876K kernel code, 966K rwdata, 4144K rodata, 1088K init, 916K bss, 46988K reserved, 16384K cma-reserved)&lt;BR /&gt;[ 0.000000] Virtual kernel memory layout:&lt;BR /&gt;[ 0.000000] modules : 0xffff000000000000 - 0xffff000008000000 ( 128 MB)&lt;BR /&gt;[ 0.000000] vmalloc : 0xffff000008000000 - 0xffff7dffbfff0000 (129022 GB)&lt;BR /&gt;[ 0.000000] .text : 0xffff000008080000 - 0xffff000008b20000 ( 10880 KB)&lt;BR /&gt;[ 0.000000] .rodata : 0xffff000008b20000 - 0xffff000008f30000 ( 4160 KB)&lt;BR /&gt;[ 0.000000] .init : 0xffff000008f30000 - 0xffff000009040000 ( 1088 KB)&lt;BR /&gt;[ 0.000000] .data : 0xffff000009040000 - 0xffff000009131a00 ( 967 KB)&lt;BR /&gt;[ 0.000000] .bss : 0xffff000009131a00 - 0xffff000009216dbc ( 917 KB)&lt;BR /&gt;[ 0.000000] fixed : 0xffff7dfffe7fb000 - 0xffff7dfffec00000 ( 4116 KB)&lt;BR /&gt;[ 0.000000] PCI I/O : 0xffff7dfffee00000 - 0xffff7dffffe00000 ( 16 MB)&lt;BR /&gt;[ 0.000000] vmemmap : 0xffff7e0000000000 - 0xffff800000000000 ( 2048 GB maximum)&lt;BR /&gt;[ 0.000000] 0xffff7e0000000000 - 0xffff7e0000ef8000 ( 14 MB actual)&lt;BR /&gt;[ 0.000000] memory : 0xffff800000000000 - 0xffff80003be00000 ( 958 MB)&lt;BR /&gt;[ 0.000000] Preemptible hierarchical RCU implementation.&lt;BR /&gt;[ 0.000000] Build-time adjustment of leaf fanout to 64.&lt;BR /&gt;[ 0.000000] RCU restricting CPUs from NR_CPUS=64 to nr_cpu_ids=1.&lt;BR /&gt;[ 0.000000] RCU: Adjusting geometry for rcu_fanout_leaf=64, nr_cpu_ids=1&lt;BR /&gt;[ 0.000000] NR_IRQS:64 nr_irqs:64 0&lt;BR /&gt;[ 0.000000] GIC: Using split EOI/Deactivate mode&lt;BR /&gt;[ 0.000000] arm_arch_timer: Architected cp15 timer(s) running at 25.00MHz (phys).&lt;BR /&gt;[ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x5c40939b5, max_idle_ns: 440795202646 ns&lt;BR /&gt;[ 0.000004] sched_clock: 56 bits at 25MHz, resolution 40ns, wraps every 4398046511100ns&lt;BR /&gt;[ 0.008508] Console: colour dummy device 80x25&lt;BR /&gt;[ 0.013042] Calibrating delay loop (skipped), value calculated using timer frequency.. 50.00 BogoMIPS (lpj=100000)&lt;BR /&gt;[ 0.023486] pid_max: default: 32768 minimum: 301&lt;BR /&gt;[ 0.028225] Security Framework initialized&lt;BR /&gt;[ 0.032602] Dentry cache hash table entries: 131072 (order: 8, 1048576 bytes)&lt;BR /&gt;[ 0.040710] Inode-cache hash table entries: 65536 (order: 7, 524288 bytes)&lt;BR /&gt;[ 0.048054] Mount-cache hash table entries: 2048 (order: 2, 16384 bytes)&lt;BR /&gt;[ 0.054823] Mountpoint-cache hash table entries: 2048 (order: 2, 16384 bytes)&lt;BR /&gt;[ 0.062913] ASID allocator initialised with 32768 entries&lt;BR /&gt;[ 0.100969] EFI services will not be available.&lt;BR /&gt;[ 0.121589] Brought up 1 CPUs&lt;BR /&gt;[ 0.124576] SMP: Total of 1 processors activated.&lt;BR /&gt;[ 0.129330] CPU features: detected feature: 32-bit EL0 Support&lt;BR /&gt;[ 0.135213] CPU features: detected feature: Kernel page table isolation (KPTI)&lt;BR /&gt;[ 0.145735] CPU: All CPU(s) started at EL2&lt;BR /&gt;[ 0.149873] alternatives: patching kernel code&lt;BR /&gt;[ 0.155233] devtmpfs: initialized&lt;BR /&gt;[ 0.162740] DMI not present or invalid.&lt;BR /&gt;[ 0.166943] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns&lt;BR /&gt;[ 0.176812] futex hash table entries: 256 (order: 2, 16384 bytes)&lt;BR /&gt;[ 0.183578] xor: measuring software checksum speed&lt;BR /&gt;[ 0.228530] 8regs : 1919.000 MB/sec&lt;BR /&gt;[ 0.272796] 8regs_prefetch: 1710.000 MB/sec&lt;BR /&gt;[ 0.317410] 32regs : 2359.000 MB/sec&lt;BR /&gt;[ 0.361665] 32regs_prefetch: 1982.000 MB/sec&lt;BR /&gt;[ 0.366319] xor: using function: 32regs (2359.000 MB/sec)&lt;BR /&gt;[ 0.371766] pinctrl core: initialized pinctrl subsystem&lt;BR /&gt;[ 0.378875] NET: Registered protocol family 16&lt;BR /&gt;[ 0.395691] cpuidle: using governor menu&lt;BR /&gt;[ 0.400204] vdso: 2 pages (1 code @ ffff000008b27000, 1 data @ ffff000009045000)&lt;BR /&gt;[ 0.407820] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.&lt;BR /&gt;[ 0.415392] DMA: preallocated 256 KiB pool for atomic allocations&lt;BR /&gt;[ 0.422162] Serial: AMBA PL011 UART driver&lt;BR /&gt;[ 0.470987] HugeTLB registered 2 MB page size, pre-allocated 0 pages&lt;BR /&gt;[ 0.561650] raid6: int64x1 gen() 394 MB/s&lt;BR /&gt;[ 0.634114] raid6: int64x1 xor() 371 MB/s&lt;BR /&gt;[ 0.706571] raid6: int64x2 gen() 598 MB/s&lt;BR /&gt;[ 0.778982] raid6: int64x2 xor() 509 MB/s&lt;BR /&gt;[ 0.851397] raid6: int64x4 gen() 903 MB/s&lt;BR /&gt;[ 0.923782] raid6: int64x4 xor() 645 MB/s&lt;BR /&gt;[ 0.996238] raid6: int64x8 gen() 836 MB/s&lt;BR /&gt;[ 1.068641] raid6: int64x8 xor() 631 MB/s&lt;BR /&gt;[ 1.141056] raid6: neonx1 gen() 623 MB/s&lt;BR /&gt;[ 1.213468] raid6: neonx1 xor() 619 MB/s&lt;BR /&gt;[ 1.285884] raid6: neonx2 gen() 1025 MB/s&lt;BR /&gt;[ 1.358300] raid6: neonx2 xor() 879 MB/s&lt;BR /&gt;[ 1.430723] raid6: neonx4 gen() 1323 MB/s&lt;BR /&gt;[ 1.503123] raid6: neonx4 xor() 1007 MB/s&lt;BR /&gt;[ 1.575532] raid6: neonx8 gen() 1433 MB/s&lt;BR /&gt;[ 1.647944] raid6: neonx8 xor() 1051 MB/s&lt;BR /&gt;[ 1.652249] raid6: using algorithm neonx8 gen() 1433 MB/s&lt;BR /&gt;[ 1.657693] raid6: .... xor() 1051 MB/s, rmw enabled&lt;BR /&gt;[ 1.662697] raid6: using intx1 recovery algorithm&lt;BR /&gt;[ 1.673704] RCPM: layerscape_rcpm_init: The RCPM driver initialized.&lt;BR /&gt;[ 1.682359] i2c i2c-0: IMX I2C adapter registered&lt;BR /&gt;[ 1.688087] i2c i2c-0: can't use DMA, using PIO instead.&lt;BR /&gt;[ 1.694128] pps_core: LinuxPPS API ver. 1 registered&lt;BR /&gt;[ 1.699474] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti &amp;lt;giometti@linux.it&amp;gt;&lt;BR /&gt;[ 1.708828] PTP clock support registered&lt;BR /&gt;[ 1.713194] dmi: Firmware registration failed.&lt;BR /&gt;[ 1.718018] No BMan portals available!&lt;BR /&gt;[ 1.722237] QMan: Allocated lookup table at ffff000009451000, entry count 65537&lt;BR /&gt;[ 1.729754] No QMan portals available!&lt;BR /&gt;[ 1.733761] No USDPAA memory, no 'fsl,usdpaa-mem' in device-tree&lt;BR /&gt;[ 1.741446] clocksource: Switched to clocksource arch_sys_counter&lt;BR /&gt;[ 1.747937] VFS: Disk quotas dquot_6.6.0&lt;BR /&gt;[ 1.751977] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes)&lt;BR /&gt;[ 1.774592] NET: Registered protocol family 2&lt;BR /&gt;[ 1.780115] TCP established hash table entries: 8192 (order: 4, 65536 bytes)&lt;BR /&gt;[ 1.787450] TCP bind hash table entries: 8192 (order: 5, 131072 bytes)&lt;BR /&gt;[ 1.794252] TCP: Hash tables configured (established 8192 bind 8192)&lt;BR /&gt;[ 1.800796] UDP hash table entries: 512 (order: 2, 16384 bytes)&lt;BR /&gt;[ 1.806816] UDP-Lite hash table entries: 512 (order: 2, 16384 bytes)&lt;BR /&gt;[ 1.813454] NET: Registered protocol family 1&lt;BR /&gt;[ 1.826188] RPC: Registered named UNIX socket transport module.&lt;BR /&gt;[ 1.832187] RPC: Registered udp transport module.&lt;BR /&gt;[ 1.836932] RPC: Registered tcp transport module.&lt;BR /&gt;[ 1.841674] RPC: Registered tcp NFSv4.1 backchannel transport module.&lt;BR /&gt;[ 1.848636] hw perfevents: enabled with armv8_pmuv3 PMU driver, 7 counters available&lt;BR /&gt;[ 1.858633] audit: initializing netlink subsys (disabled)&lt;BR /&gt;[ 1.864806] audit: type=2000 audit(1.752:1): initialized&lt;BR /&gt;[ 1.875257] workingset: timestamp_bits=44 max_order=18 bucket_order=0&lt;BR /&gt;[ 1.882380] squashfs: version 4.0 (2009/01/31) Phillip Lougher&lt;BR /&gt;[ 1.892522] NFS: Registering the id_resolver key type&lt;BR /&gt;[ 1.897650] Key type id_resolver registered&lt;BR /&gt;[ 1.901870] Key type id_legacy registered&lt;BR /&gt;[ 1.905921] nfs4filelayout_init: NFSv4 File Layout Driver Registering...&lt;BR /&gt;[ 1.912948] fuse init (API version 7.26)&lt;BR /&gt;[ 1.917218] SGI XFS with ACLs, security attributes, realtime, no debug enabled&lt;BR /&gt;[ 1.937106] 9p: Installing v9fs 9p2000 file system support&lt;BR /&gt;[ 1.942731] ceph: loaded (mds proto 32)&lt;BR /&gt;[ 1.949386] async_tx: api initialized (async)&lt;BR /&gt;[ 1.954034] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 245)&lt;BR /&gt;[ 1.965704] io scheduler noop registered&lt;BR /&gt;[ 1.969762] io scheduler cfq registered (default)&lt;BR /&gt;[ 1.976004] libphy: mdio_driver_register: phy-bcm-ns2-pci&lt;BR /&gt;[ 1.983874] pci_hotplug: PCI Hot Plug PCI Core version: 0.5&lt;BR /&gt;[ 1.990457] pciehp: PCI Express Hot Plug Controller Driver version: 0.4&lt;BR /&gt;[ 1.998121] OF: PCI: host bridge /soc/pcie@3400000 ranges:&lt;BR /&gt;[ 2.003904] OF: PCI: IO 0x4000010000..0x400001ffff -&amp;gt; 0x00000000&lt;BR /&gt;[ 2.010297] OF: PCI: MEM 0x4040000000..0x407fffffff -&amp;gt; 0x40000000&lt;BR /&gt;[ 2.016976] layerscape-pcie 3400000.pcie: PCI host bridge to bus 0000:00&lt;BR /&gt;[ 2.023826] pci_bus 0000:00: root bus resource [bus 00-ff]&lt;BR /&gt;[ 2.029379] pci_bus 0000:00: root bus resource [io 0x0000-0xffff]&lt;BR /&gt;[ 2.035631] pci_bus 0000:00: root bus resource [mem 0x4040000000-0x407fffffff] (bus address [0x40000000-0x7fffffff])&lt;BR /&gt;[ 2.046795] pci 0000:00:00.0: BAR 6: assigned [mem 0x4040000000-0x40400007ff pref]&lt;BR /&gt;[ 2.054562] pci 0000:00:00.0: PCI bridge to [bus 01-ff]&lt;BR /&gt;[ 2.060209] pcieport 0000:00:00.0: Signaling PME through PCIe PME interrupt&lt;BR /&gt;[ 2.071368] Freescale LS2 console driver&lt;BR /&gt;[ 2.076748] fsl-ls2-console: device fsl_mc_console registered&lt;BR /&gt;[ 2.082840] fsl-ls2-console: device fsl_aiop_console registered&lt;BR /&gt;[ 2.090261] xenfs: not registering filesystem on non-xen platform&lt;BR /&gt;[ 2.103763] Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled&lt;BR /&gt;[ 2.112949] console [ttyS0] disabled&lt;BR /&gt;[ 2.117324] 21c0500.serial: ttyS0 at MMIO 0x21c0500 (irq = 15, base_baud = 7812500) is a 16550A&lt;BR /&gt;[ 2.126287] console [ttyS0] enabled&lt;BR /&gt;[ 2.126287] console [ttyS0] enabled&lt;BR /&gt;[ 2.133380] bootconsole [uart8250] disabled&lt;BR /&gt;[ 2.133380] bootconsole [uart8250] disabled&lt;BR /&gt;[ 2.142444] SuperH (H)SCI(F) driver initialized&lt;BR /&gt;[ 2.147631] msm_serial: driver initialized&lt;BR /&gt;[ 2.152769] Unable to detect cache hierarchy for CPU 0&lt;BR /&gt;[ 2.235262] brd: module loaded&lt;BR /&gt;[ 2.277575] loop: module loaded&lt;BR /&gt;[ 2.283761] libphy: Fixed MDIO Bus: probed&lt;BR /&gt;[ 2.290556] tun: Universal TUN/TAP device driver, 1.6&lt;BR /&gt;[ 2.296886] tun: (C) 1999-2004 Max Krasnyansky &amp;lt;maxk@qualcomm.com&amp;gt;&lt;BR /&gt;[ 2.304277] Freescale FM module, FMD API version 21.1.0&lt;BR /&gt;[ 2.310342] Freescale FM Ports module&lt;BR /&gt;[ 2.314111] fsl_mac: fsl_mac: FSL FMan MAC API based driver&lt;BR /&gt;[ 2.319976] fsl_dpa: FSL DPAA Ethernet driver&lt;BR /&gt;[ 2.324557] fsl_advanced: FSL DPAA Advanced drivers:&lt;BR /&gt;[ 2.329601] fsl_proxy: FSL DPAA Proxy initialization driver&lt;BR /&gt;[ 2.335333] fsl_oh: FSL FMan Offline Parsing port driver&lt;BR /&gt;[ 2.341160] e1000: Intel(R) PRO/1000 Network Driver - version 7.3.21-k8-NAPI&lt;BR /&gt;[ 2.348425] e1000: Copyright (c) 1999-2006 Intel Corporation.&lt;BR /&gt;[ 2.354349] e1000e: Intel(R) PRO/1000 Network Driver - 3.2.6-k&lt;BR /&gt;[ 2.360263] e1000e: Copyright(c) 1999 - 2015 Intel Corporation.&lt;BR /&gt;[ 2.366348] igb: Intel(R) Gigabit Ethernet Network Driver - version 5.4.0-k&lt;BR /&gt;[ 2.373382] igb: Copyright (c) 2007-2014 Intel Corporation.&lt;BR /&gt;[ 2.379079] igbvf: Intel(R) Gigabit Virtual Function Network Driver - version 2.4.0-k&lt;BR /&gt;[ 2.386981] igbvf: Copyright (c) 2009 - 2012 Intel Corporation.&lt;BR /&gt;[ 2.393032] sky2: driver version 1.30&lt;BR /&gt;[ 2.398331] VFIO - User Level meta-driver version: 0.3&lt;BR /&gt;[ 2.409114] i2c /dev entries driver&lt;BR /&gt;[ 2.417290] imx2-wdt 2ad0000.wdog: timeout 60 sec (nowayout=0)&lt;BR /&gt;[ 2.425241] qoriq_cpufreq: Freescale QorIQ CPU frequency scaling driver&lt;BR /&gt;[ 2.432822] sdhci: Secure Digital Host Controller Interface driver&lt;BR /&gt;[ 2.439416] sdhci: Copyright(c) Pierre Ossman&lt;BR /&gt;[ 2.444154] Synopsys Designware Multimedia Card Interface Driver&lt;BR /&gt;[ 2.450927] sdhci-pltfm: SDHCI platform and OF driver helper&lt;BR /&gt;[ 2.457399] [k] sdhci_add_host,3668, 1560000.esdhc&lt;BR /&gt;[ 2.501468] mmc0: SDHCI controller on 1560000.esdhc [1560000.esdhc] using ADMA 64-bit&lt;BR /&gt;[ 2.509572] [k] sdhci_add_host,3668, 1580000.esdhc&lt;BR /&gt;[ 2.561461] mmc1: SDHCI controller on 1580000.esdhc [1580000.esdhc] using ADMA 64-bit&lt;BR /&gt;[ 2.573646] caam-dma 1700000.crypto:caam-dma: Defer probing after JR driver probing&lt;BR /&gt;[ 2.604246] caam 1700000.crypto: Instantiated RNG4 SH1&lt;BR /&gt;[ 2.611469] caam 1700000.crypto: device ID = 0x0a14040000000000 (Era &lt;LI-EMOJI id="lia_smiling-face-with-sunglasses" title=":smiling_face_with_sunglasses:"&gt;&lt;/LI-EMOJI&gt;&lt;BR /&gt;[ 2.620277] caam 1700000.crypto: job rings = 3, qi = 0&lt;BR /&gt;[ 2.636855] caam algorithms registered in /proc/crypto&lt;BR /&gt;[ 2.647440] caam_jr 1710000.jr: registering rng-caam&lt;BR /&gt;[ 2.652611] caam 1700000.crypto: caam pkc algorithms registered in /proc/crypto&lt;BR /&gt;[ 2.661571] DPAA2-ETH: debugfs created&lt;BR /&gt;[ 2.667009] No fsl,qman node&lt;BR /&gt;[ 2.670499] Freescale USDPAA process driver&lt;BR /&gt;[ 2.674775] fsl-usdpaa: no region found&lt;BR /&gt;[ 2.678824] Freescale USDPAA process IRQ driver&lt;BR /&gt;[ 2.687352] optee: probing for conduit method from DT.&lt;BR /&gt;[ 2.692769] mmc0: new high speed SDHC card at address 59b4&lt;BR /&gt;[ 2.699127] optee: api uid mismatch&lt;BR /&gt;[ 2.702797] mmcblk0: mmc0:59b4 USDU1 7.51 GiB&lt;BR /&gt;[ 2.708078] mmcblk0: p1 p2 p3&lt;BR /&gt;[ 2.718800] Netfilter messages via NETLINK v0.30.&lt;BR /&gt;[ 2.726736] nf_conntrack version 0.5.0 (7680 buckets, 30720 max)&lt;BR /&gt;[ 2.735001] nf_tables: (c) 2007-2009 Patrick McHardy &amp;lt;kaber@trash.net&amp;gt;&lt;BR /&gt;[ 2.741582] nf_tables_compat: (c) 2012 Pablo Neira Ayuso &amp;lt;pablo@netfilter.org&amp;gt;&lt;BR /&gt;[ 2.748855] mmc1: new HS200 MMC card at address 0001&lt;BR /&gt;[ 2.754546] ip_tables: (C) 2000-2006 Netfilter Core Team&lt;BR /&gt;[ 2.760162] Initializing XFRM netlink socket&lt;BR /&gt;[ 2.764482] mmcblk1: mmc1:0001 R1J55A 7.28 GiB&lt;BR /&gt;[ 2.769412] NET: Registered protocol family 10&lt;BR /&gt;[ 2.773906] mmcblk1boot0: mmc1:0001 R1J55A partition 1 8.00 MiB&lt;BR /&gt;[ 2.780433] mmcblk1boot1: mmc1:0001 R1J55A partition 2 8.00 MiB&lt;BR /&gt;[ 2.790670] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver&lt;BR /&gt;[ 2.796833] mmcblk1rpmb: mmc1:0001 R1J55A partition 3 4.00 MiB&lt;BR /&gt;[ 2.803500] mmcblk1: p1&lt;BR /&gt;[ 2.809221] NET: Registered protocol family 17&lt;BR /&gt;[ 2.813892] NET: Registered protocol family 15&lt;BR /&gt;[ 2.818416] Bridge firewalling registered&lt;BR /&gt;[ 2.822527] Ebtables v2.0 registered&lt;BR /&gt;[ 2.826233] 8021q: 802.1Q VLAN Support v1.8&lt;BR /&gt;[ 2.830480] 9pnet: Installing 9P2000 support&lt;BR /&gt;[ 2.834908] Key type dns_resolver registered&lt;BR /&gt;[ 2.839282] Key type ceph registered&lt;BR /&gt;[ 2.847028] libceph: loaded (mon/osd proto 15/24)&lt;BR /&gt;[ 2.852587] registered taskstats version 1&lt;BR /&gt;[ 2.861729] Btrfs loaded, crc32c=crc32c-generic&lt;BR /&gt;[ 2.867812] caam-dma 1700000.crypto:caam-dma: caam dma support with 3 job rings&lt;BR /&gt;[ 2.875580] hctosys: unable to open rtc device (rtc0)&lt;BR /&gt;[ 2.882135] EXT4-fs (mmcblk0p3): couldn't mount as ext3 due to feature incompatibilities&lt;BR /&gt;[ 3.119229] random: fast init done&lt;BR /&gt;[ 3.344088] EXT4-fs (mmcblk0p3): recovery complete&lt;BR /&gt;[ 3.351416] EXT4-fs (mmcblk0p3): mounted filesystem with ordered data mode. Opts: (null)&lt;BR /&gt;[ 3.359577] VFS: Mounted root (ext4 filesystem) on device 179:3.&lt;BR /&gt;[ 3.365704] devtmpfs: mounted&lt;BR /&gt;[ 3.369463] Freeing unused kernel memory: 1088K&lt;BR /&gt;[ 3.519841] EXT4-fs (mmcblk0p3): re-mounted. Opts: (null)&lt;BR /&gt;Starting logging: OK&lt;BR /&gt;Populating /dev using udev: [ 4.079106] udevd[1114]: starting version 3.2.5&lt;BR /&gt;[ 4.089292] random: udevd: uninitialized urandom read (16 bytes read)&lt;BR /&gt;[ 4.096124] random: udevd: uninitialized urandom read (16 bytes read)&lt;BR /&gt;[ 4.102903] random: udevd: uninitialized urandom read (16 bytes read)&lt;BR /&gt;[ 4.120726] udevd[1114]: specified group 'input' unknown&lt;BR /&gt;[ 4.145047] udevd[1115]: starting eudev-3.2.5&lt;BR /&gt;[ 4.577634] pfe: module is from the staging directory, the quality is unknown, you have been warned.&lt;BR /&gt;[ 4.620274] cbus_baseaddr: ffff00000a000000, ddr_baseaddr: ffff800003400000, ddr_phys_baseaddr: 83400000, ddr_size: c00000&lt;BR /&gt;[ 4.677592] pfe_hw_init&lt;BR /&gt;[ 4.680045] CLASS version: 20&lt;BR /&gt;[ 4.695715] TMU version: 1011231&lt;BR /&gt;[ 4.699295] BMU1 version: 21&lt;BR /&gt;[ 4.702317] BMU2 version: 21&lt;BR /&gt;[ 4.705198] EGPI1 version: 50&lt;BR /&gt;[ 4.708268] EGPI2 version: 50&lt;BR /&gt;[ 4.711304] HGPI version: 50&lt;BR /&gt;[ 4.714252] HIF version: 10&lt;BR /&gt;[ 4.717045] HIF NOPCY version: 10&lt;BR /&gt;[ 4.720457] bmu_init(1) done&lt;BR /&gt;[ 4.723405] bmu_init(2) done&lt;BR /&gt;[ 4.728575] class_init() done&lt;BR /&gt;[ 4.741644] tmu_init() done&lt;BR /&gt;[ 4.744439] gpi_init(1) done&lt;BR /&gt;[ 4.747413] gpi_init(2) done&lt;BR /&gt;[ 4.750364] gpi_init(hif) done&lt;BR /&gt;[ 4.753417] bmu_enable(1) done&lt;BR /&gt;[ 4.756565] bmu_enable(2) done&lt;BR /&gt;[ 4.759688] pfe_hif_lib_init&lt;BR /&gt;[ 4.762768] pfe_hif_init&lt;BR /&gt;[ 4.765301] pfe_hif_alloc_descr&lt;BR /&gt;[ 4.768729] pfe_hif_init_buffers&lt;BR /&gt;[ 4.772840] pfe_firmware_init&lt;BR /&gt;[ 4.780002] pfe_load_elf&lt;BR /&gt;[ 4.782625] pe_load_ddr_section: load address(3fb0000) and elf file address(ffff0000095fb000) rcvd&lt;BR /&gt;[ 4.814888] PFE binary version: pfe_ls1012a_slowpath_06&lt;BR /&gt;[ 4.820129] pfe_load_elf&lt;BR /&gt;[ 4.823818] pfe_ctrl_init&lt;BR /&gt;[ 4.826518] pfe_ctrl_init finished&lt;BR /&gt;[ 4.829989] pfe_eth_init&lt;BR /&gt;[ 4.832558] pfe_eth_mdio_init&lt;BR /&gt;[ 4.847082] libphy: ls1012a MDIO Bus: probed&lt;BR /&gt;[ 4.854625] pfe_phy_init interface 3&lt;BR /&gt;[ 4.858591] pfe 4000000.pfe eth0: pfe_eth_init_one: created interface, baseaddr: ffff00000a200000&lt;BR /&gt;[ 4.870768] pfe_phy_init interface 3&lt;BR /&gt;[ 4.874712] pfe 4000000.pfe eth1: pfe_eth_init_one: created interface, baseaddr: ffff00000a220000&lt;BR /&gt;[ 4.883901] pfe_debugfs_init&lt;BR /&gt;done&lt;BR /&gt;Initializing random number generator... done.&lt;BR /&gt;Mounting cgroupfs hierarchy: OK&lt;BR /&gt;Starting system message bus: [ 5.095283] urandom_read: 3 callbacks suppressed&lt;BR /&gt;[ 5.095289] random: dbus-uuidgen: uninitialized urandom read (12 bytes read)&lt;BR /&gt;[ 5.107152] random: dbus-uuidgen: uninitialized urandom read (8 bytes read)&lt;BR /&gt;[ 5.132420] random: dbus-daemon: uninitialized urandom read (12 bytes read)&lt;BR /&gt;dbus-daemon[1178]: Failed to start message bus: Could not get UID and GID for username "dbus"&lt;BR /&gt;done&lt;BR /&gt;Starting network: OK&lt;BR /&gt;Starting dhcpcd...&lt;BR /&gt;no interfaces ha[ 5.274929] pfe 4000000.pfe eth0: pfe_eth_open&lt;BR /&gt;ve a carrier&lt;BR /&gt;forked to background, child pid [ 5.282415] hif_process_client_req: register client_id 0&lt;BR /&gt;1207&lt;BR /&gt;[ 5.289038] pfe_hif_client_register&lt;BR /&gt;[ 5.296298] pfe 4000000.pfe eth0: pfe_gemac_init&lt;BR /&gt;[ 5.301937] IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready&lt;BR /&gt;[ 5.309123] pfe 4000000.pfe eth1: pfe_eth_open&lt;BR /&gt;[ 5.314395] hif_process_client_req: register client_id 1&lt;BR /&gt;[ 5.319763] pfe_hif_client_register&lt;BR /&gt;[ 5.323895] pfe 4000000.pfe eth1: pfe_gemac_init&lt;BR /&gt;ssh-keygen: generating new host keys: RSA [ 5.869471] IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready&lt;BR /&gt;[ 6.317936] pfe 4000000.pfe eth0: Link is Up - 1Gbps/Full - flow control rx/tx&lt;BR /&gt;DSA ECDSA ED25519&lt;BR /&gt;Starting sshd: Privilege separation user sshd does not exist&lt;BR /&gt;OK&lt;/P&gt;&lt;P&gt;LSDK Buildroot&lt;BR /&gt;LSDK login: root&lt;BR /&gt;[root@LSDK ~]# ls&lt;BR /&gt;rootfs_buildroot_arm64_moderate.tar&lt;BR /&gt;[root@LSDK ~]# df -hT&lt;BR /&gt;Filesystem Type Size Used Available Use% Mounted on&lt;BR /&gt;/dev/root ext4 6.2G 255.3M 5.6G 4% /&lt;BR /&gt;devtmpfs devtmpfs 448.1M 0 448.1M 0% /dev&lt;BR /&gt;tmpfs tmpfs 456.6M 0 456.6M 0% /dev/shm&lt;BR /&gt;tmpfs tmpfs 456.6M 44.0K 456.5M 0% /tmp&lt;BR /&gt;tmpfs tmpfs 456.6M 100.0K 456.5M 0% /run&lt;BR /&gt;cgroup tmpfs 456.6M 0 456.6M 0% /sys/fs/cgroup&lt;/P&gt;&lt;P&gt;[root@LSDK ~]# uname -a&lt;BR /&gt;Linux LSDK 4.9.140-dirty #1 SMP PREEMPT Tue Oct 6 11:29:58 UTC 2020 aarch64 GNU/Linux&lt;BR /&gt;[root@LSDK ~]# rdate -s time.bora.net&lt;BR /&gt;&lt;FONT color="#FF0000"&gt;[root@LSDK ~]# tar xf rootfs_buildroot_arm64_moderate.tar&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT color="#FF0000"&gt;[ 40.615952] Kernel panic - not syncing: Attempted to kill init! exitcode=0x0000000b&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT color="#FF0000"&gt;[ 40.615952]&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT color="#FF0000"&gt;[ 40.625115] CPU: 0 PID: 1 Comm: init Tainted: G C 4.9.140-dirty #1&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT color="#FF0000"&gt;[ 40.632433] Hardware name: LS1012A FRWY Board (DT)&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT color="#FF0000"&gt;[ 40.637227] Call trace:&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT color="#FF0000"&gt;[ 40.639682] [&amp;lt;ffff000008089570&amp;gt;] dump_backtrace+0x0/0x238&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT color="#FF0000"&gt;[ 40.645089] [&amp;lt;ffff0000080897bc&amp;gt;] show_stack+0x14/0x20&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT color="#FF0000"&gt;[ 40.650149] [&amp;lt;ffff0000084f1054&amp;gt;] dump_stack+0xa0/0xc4&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT color="#FF0000"&gt;[ 40.655209] [&amp;lt;ffff00000816064c&amp;gt;] panic+0x120/0x290&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT color="#FF0000"&gt;[ 40.660007] [&amp;lt;ffff0000080aafe8&amp;gt;] complete_and_exit+0x0/0x20&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT color="#FF0000"&gt;[ 40.665587] [&amp;lt;ffff0000080ab050&amp;gt;] do_group_exit+0x38/0xa0&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT color="#FF0000"&gt;[ 40.670907] [&amp;lt;ffff0000080b57d4&amp;gt;] get_signal+0xfc/0x4d0&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT color="#FF0000"&gt;[ 40.676052] [&amp;lt;ffff00000808871c&amp;gt;] do_signal+0x174/0x990&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT color="#FF0000"&gt;[ 40.681196] [&amp;lt;ffff0000080892a8&amp;gt;] do_notify_resume+0x88/0xa8&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT color="#FF0000"&gt;[ 40.686776] [&amp;lt;ffff000008083884&amp;gt;] work_pending+0x8/0x10&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT color="#FF0000"&gt;[ 40.691921] Kernel Offset: disabled&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT color="#FF0000"&gt;[ 40.695409] Memory Limit: none&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT color="#FF0000"&gt;[ 40.698466] ---[ end Kernel panic - not syncing: Attempted to kill init! exitcode=0x0000000b&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT color="#FF0000"&gt;[ 40.698466]&lt;/FONT&gt;&lt;/P&gt;&lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any pointers are greatly appreciated!&lt;/P&gt;&lt;P&gt;Thank you!&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Gyosun.&lt;/P&gt;</description>
      <pubDate>Tue, 06 Oct 2020 14:09:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Kernel-panic-occurs-during-operation-after-booting-the-LS1012A/m-p/1163452#M6746</guid>
      <dc:creator>gyosunshim</dc:creator>
      <dc:date>2020-10-06T14:09:09Z</dc:date>
    </item>
    <item>
      <title>Re: Kernel panic occurs during operation after booting the LS1012A.</title>
      <link>https://community.nxp.com/t5/Layerscape/Kernel-panic-occurs-during-operation-after-booting-the-LS1012A/m-p/1163852#M6749</link>
      <description>&lt;P&gt;Again I solved it!!&lt;/P&gt;&lt;P&gt;I found that the DDR part marked on the circuit diagram of XFRWY-LS1012A RevB and the DDR mounted on the board are different.&lt;/P&gt;&lt;P&gt;The circuit diagram is 512MB, and the board is equipped with 1GB.&lt;/P&gt;&lt;P&gt;So, by modifying the two parts as below, kernel panic did not occur.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;vi plat/nxp/soc-ls1012/ls1012afrwy/platform_def.h&lt;/P&gt;&lt;P&gt;#define PLAT_DEF_DRAM0_SIZE &lt;FONT color="#FF0000"&gt;0x20000000&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;vi board/freescale/ls1012afrdm/ls1012afrdm.c&lt;/P&gt;&lt;P&gt;gd-&amp;gt;ram_size = &lt;FONT color="#FF0000"&gt;SYS_SDRAM_SIZE_512&lt;/FONT&gt;;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Gyosun.&lt;/P&gt;</description>
      <pubDate>Wed, 07 Oct 2020 10:46:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Kernel-panic-occurs-during-operation-after-booting-the-LS1012A/m-p/1163852#M6749</guid>
      <dc:creator>gyosunshim</dc:creator>
      <dc:date>2020-10-07T10:46:40Z</dc:date>
    </item>
  </channel>
</rss>