<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic packets are discarded by ls1043 in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/packets-are-discarded-by-ls1043/m-p/1163846#M6748</link>
    <description>I'm developing a board useing LS1043A，the lsdk is 19.06. The board has 7 ports just like LS1043ARDB. When I use IXIA to test packet forwarding between fm1-mac1 and fm1-mac2, some packets lost. The topology of my test is: IXIA port1 -- fm1-mac1, IXIA port2 -- fm1-mac2, IXIA port1 and port2 send packets which length is 64 bytes. port1 receive packets sent by port2, and port2 recieve pakcets sent by port1. I use testpmd to do the test, the command is : testpmd -c 0xf -n 1 -- -i --portmask=0x3f --nb-core=3 --coremask=0xe I checked the statistics of the ports: fm0-port-rx2 counter: 14236221 fm0-port-rx2 counter: 14236221 fm0-port-rx2 counter: 128736103 fm0-port-rx2 counter: 128736103 fm0-port-rx2 counter: 0 fm0-port-rx2 counter: 0 The value of port_dealloc_buf and port_discard_frame is equal to the lost packetes. My question is: what do port_dealloc_buf and port_discard_frame mean? How can I solve this problem?</description>
    <pubDate>Wed, 07 Oct 2020 10:34:04 GMT</pubDate>
    <dc:creator>flymice</dc:creator>
    <dc:date>2020-10-07T10:34:04Z</dc:date>
    <item>
      <title>packets are discarded by ls1043</title>
      <link>https://community.nxp.com/t5/Layerscape/packets-are-discarded-by-ls1043/m-p/1163846#M6748</link>
      <description>I'm developing a board useing LS1043A，the lsdk is 19.06. The board has 7 ports just like LS1043ARDB. When I use IXIA to test packet forwarding between fm1-mac1 and fm1-mac2, some packets lost. The topology of my test is: IXIA port1 -- fm1-mac1, IXIA port2 -- fm1-mac2, IXIA port1 and port2 send packets which length is 64 bytes. port1 receive packets sent by port2, and port2 recieve pakcets sent by port1. I use testpmd to do the test, the command is : testpmd -c 0xf -n 1 -- -i --portmask=0x3f --nb-core=3 --coremask=0xe I checked the statistics of the ports: fm0-port-rx2 counter: 14236221 fm0-port-rx2 counter: 14236221 fm0-port-rx2 counter: 128736103 fm0-port-rx2 counter: 128736103 fm0-port-rx2 counter: 0 fm0-port-rx2 counter: 0 The value of port_dealloc_buf and port_discard_frame is equal to the lost packetes. My question is: what do port_dealloc_buf and port_discard_frame mean? How can I solve this problem?</description>
      <pubDate>Wed, 07 Oct 2020 10:34:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/packets-are-discarded-by-ls1043/m-p/1163846#M6748</guid>
      <dc:creator>flymice</dc:creator>
      <dc:date>2020-10-07T10:34:04Z</dc:date>
    </item>
    <item>
      <title>Re: packets are discarded by ls1043</title>
      <link>https://community.nxp.com/t5/Layerscape/packets-are-discarded-by-ls1043/m-p/1165135#M6752</link>
      <description>&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;port_dealloc_buf reflects BMI RBDC port_discard_frame reflects RFDC. You can find a&lt;BR /&gt;description of these registers in LS1043ADPAARM, Sections 5.5.4.5.30 and 5.5.4.5.33&lt;BR /&gt;The most likely reason for these counters growth is that you are simply hitting&lt;BR /&gt;the application throughput limit. Additional details can be found in the same document&lt;BR /&gt;Sections 5.5.6.8 and 3.3.14. Suggestions for DPDK performance tuning are &lt;BR /&gt;provided in the online documentation:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://docs.nxp.com/bundle/GUID-C3A436DA-E944-4F73-9811-2335DEBD04D6/page/GUID-AD9EFB28-7C53-4D17-BC52-232F85E7F908.html" target="_blank" rel="noopener"&gt;https://docs.nxp.com/bundle/GUID-C3A436DA-E944-4F73-9811-2335DEBD04D6/page/GUID-AD9EFB28-7C53-4D17-BC52-232F85E7F908.html&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Hope this helps,&lt;BR /&gt;Platon&lt;/P&gt;</description>
      <pubDate>Fri, 09 Oct 2020 11:12:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/packets-are-discarded-by-ls1043/m-p/1165135#M6752</guid>
      <dc:creator>bpe</dc:creator>
      <dc:date>2020-10-09T11:12:57Z</dc:date>
    </item>
  </channel>
</rss>