<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Enabling the Ethernet Switch on LS1028ARDB in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/Enabling-the-Ethernet-Switch-on-LS1028ARDB/m-p/1152223#M6642</link>
    <description>&lt;P&gt;I am trying to follow this documentation to enable the Switch on the LS1028ARDB:&lt;BR /&gt;&lt;BR /&gt;&lt;A href="https://docs.nxp.com/bundle/GUID-C3A436DA-E944-4F73-9811-2335DEBD04D6/page/GUID-558A9D18-5FA4-4E88-B428-B306849225A2.html" target="_blank" rel="noopener"&gt;https://docs.nxp.com/bundle/GUID-C3A436DA-E944-4F73-9811-2335DEBD04D6/page/GUID-558A9D18-5FA4-4E88-B428-B306849225A2.html&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;All mentioned commands fail with the same error message:&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="c"&gt;root@localhost:~# restool dpsw create --num-ifs=5 --max-vlans=16 --max-fdbs=1 --options="DPSW_OPT_CTRL_IF_DIS"
error: Did not find a device file&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;The documentation also contains this line:&lt;BR /&gt;&lt;BR /&gt;&lt;EM&gt;The following section describes the main commands to create a switch starting from the &lt;STRONG&gt;dpl-eth.0x2A_0x41.dtb&lt;/STRONG&gt; DPL file.&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;Is there any description what this file is, where to find it, how to use it?&lt;/P&gt;</description>
    <pubDate>Fri, 11 Sep 2020 15:34:09 GMT</pubDate>
    <dc:creator>sebastian_plama</dc:creator>
    <dc:date>2020-09-11T15:34:09Z</dc:date>
    <item>
      <title>Enabling the Ethernet Switch on LS1028ARDB</title>
      <link>https://community.nxp.com/t5/Layerscape/Enabling-the-Ethernet-Switch-on-LS1028ARDB/m-p/1152223#M6642</link>
      <description>&lt;P&gt;I am trying to follow this documentation to enable the Switch on the LS1028ARDB:&lt;BR /&gt;&lt;BR /&gt;&lt;A href="https://docs.nxp.com/bundle/GUID-C3A436DA-E944-4F73-9811-2335DEBD04D6/page/GUID-558A9D18-5FA4-4E88-B428-B306849225A2.html" target="_blank" rel="noopener"&gt;https://docs.nxp.com/bundle/GUID-C3A436DA-E944-4F73-9811-2335DEBD04D6/page/GUID-558A9D18-5FA4-4E88-B428-B306849225A2.html&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;All mentioned commands fail with the same error message:&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="c"&gt;root@localhost:~# restool dpsw create --num-ifs=5 --max-vlans=16 --max-fdbs=1 --options="DPSW_OPT_CTRL_IF_DIS"
error: Did not find a device file&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;The documentation also contains this line:&lt;BR /&gt;&lt;BR /&gt;&lt;EM&gt;The following section describes the main commands to create a switch starting from the &lt;STRONG&gt;dpl-eth.0x2A_0x41.dtb&lt;/STRONG&gt; DPL file.&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;Is there any description what this file is, where to find it, how to use it?&lt;/P&gt;</description>
      <pubDate>Fri, 11 Sep 2020 15:34:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Enabling-the-Ethernet-Switch-on-LS1028ARDB/m-p/1152223#M6642</guid>
      <dc:creator>sebastian_plama</dc:creator>
      <dc:date>2020-09-11T15:34:09Z</dc:date>
    </item>
    <item>
      <title>Re: Enabling the Ethernet Switch on LS1028ARDB</title>
      <link>https://community.nxp.com/t5/Layerscape/Enabling-the-Ethernet-Switch-on-LS1028ARDB/m-p/1152755#M6646</link>
      <description>&lt;P&gt;restool and DPL files are valid only for devices equipped with DPAA2. LS1028A does not have it. Study &lt;A href="https://docs.nxp.com/bundle/GUID-C3A436DA-E944-4F73-9811-2335DEBD04D6/page/GUID-4652F8E0-14DC-4BE4-B8A7-DE03EFABB667.html" target="_blank" rel="noopener"&gt;this section&lt;/A&gt; of LSDK online documentation on how to work with LS1028A on-chip switch.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Hope this helps&lt;/P&gt;
&lt;P&gt;Platon&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 14 Sep 2020 08:49:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Enabling-the-Ethernet-Switch-on-LS1028ARDB/m-p/1152755#M6646</guid>
      <dc:creator>bpe</dc:creator>
      <dc:date>2020-09-14T08:49:25Z</dc:date>
    </item>
    <item>
      <title>Re: Enabling the Ethernet Switch on LS1028ARDB</title>
      <link>https://community.nxp.com/t5/Layerscape/Enabling-the-Ethernet-Switch-on-LS1028ARDB/m-p/1153530#M6652</link>
      <description>&lt;P&gt;Thanks, I will try this.&lt;BR /&gt;&lt;BR /&gt;Is there any way to know which parts of this very long document are relevant for which boards?&lt;/P&gt;</description>
      <pubDate>Tue, 15 Sep 2020 14:01:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Enabling-the-Ethernet-Switch-on-LS1028ARDB/m-p/1153530#M6652</guid>
      <dc:creator>sebastian_plama</dc:creator>
      <dc:date>2020-09-15T14:01:53Z</dc:date>
    </item>
  </channel>
</rss>