<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LayerscapeのトピックRe: LS1043A DPAA debug on CodeWarrior</title>
    <link>https://community.nxp.com/t5/Layerscape/LS1043A-DPAA-debug-on-CodeWarrior/m-p/1151139#M6615</link>
    <description>&lt;P&gt;Thank you. I dont know how to set up the IP address for the LS1043A board. That is what I want to ask&lt;/P&gt;</description>
    <pubDate>Wed, 09 Sep 2020 22:38:02 GMT</pubDate>
    <dc:creator>smruthi_ramesh</dc:creator>
    <dc:date>2020-09-09T22:38:02Z</dc:date>
    <item>
      <title>LS1043A DPAA debug on CodeWarrior</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1043A-DPAA-debug-on-CodeWarrior/m-p/1132759#M6552</link>
      <description>&lt;P&gt;Hi, I have the DPDK driver running on the LS1043A. is there a way to debug the application via CodeWarrior? I would like to step through the code and understand how the DPAA driver works.&lt;/P&gt;</description>
      <pubDate>Tue, 01 Sep 2020 00:19:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1043A-DPAA-debug-on-CodeWarrior/m-p/1132759#M6552</guid>
      <dc:creator>smruthi_ramesh</dc:creator>
      <dc:date>2020-09-01T00:19:43Z</dc:date>
    </item>
    <item>
      <title>Re: LS1043A DPAA debug on CodeWarrior</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1043A-DPAA-debug-on-CodeWarrior/m-p/1132887#M6554</link>
      <description>&lt;P&gt;After installing CodeWarrior for ARMv8, you could refer to section "8.2 Linux application debug" in document&amp;nbsp;C:\Freescale\CW4NET_v2020.06\CW_ARMv8\ARMv8\Help\PDF\ARMv8_Targeting_Manual.pdf.&lt;/P&gt;</description>
      <pubDate>Tue, 01 Sep 2020 06:56:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1043A-DPAA-debug-on-CodeWarrior/m-p/1132887#M6554</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2020-09-01T06:56:54Z</dc:date>
    </item>
    <item>
      <title>Re: LS1043A DPAA debug on CodeWarrior</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1043A-DPAA-debug-on-CodeWarrior/m-p/1133358#M6562</link>
      <description>&lt;P&gt;Thank you. I went through the manual, that talks about setting up a remote connection. But the board is connected via CodeWarrior TAP as USB serial port and not an IP address. What is to be done in that case?&lt;/P&gt;</description>
      <pubDate>Tue, 01 Sep 2020 21:36:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1043A-DPAA-debug-on-CodeWarrior/m-p/1133358#M6562</guid>
      <dc:creator>smruthi_ramesh</dc:creator>
      <dc:date>2020-09-01T21:36:23Z</dc:date>
    </item>
    <item>
      <title>Re: LS1043A DPAA debug on CodeWarrior</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1043A-DPAA-debug-on-CodeWarrior/m-p/1149449#M6591</link>
      <description>&lt;P&gt;In Linux application debugging, CodeWarrior TAP is not used, Ethernet is used to connect the host PC and the target board.&lt;/P&gt;</description>
      <pubDate>Mon, 07 Sep 2020 05:31:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1043A-DPAA-debug-on-CodeWarrior/m-p/1149449#M6591</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2020-09-07T05:31:40Z</dc:date>
    </item>
    <item>
      <title>Re: LS1043A DPAA debug on CodeWarrior</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1043A-DPAA-debug-on-CodeWarrior/m-p/1150540#M6607</link>
      <description>&lt;P&gt;Okay thanks for the reply. How do I set up the ethernet connection between the board and my PC? I tried looking for it in the CodeWarrior guide, but didnt find any instructions&lt;/P&gt;</description>
      <pubDate>Tue, 08 Sep 2020 19:27:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1043A-DPAA-debug-on-CodeWarrior/m-p/1150540#M6607</guid>
      <dc:creator>smruthi_ramesh</dc:creator>
      <dc:date>2020-09-08T19:27:17Z</dc:date>
    </item>
    <item>
      <title>Re: LS1043A DPAA debug on CodeWarrior</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1043A-DPAA-debug-on-CodeWarrior/m-p/1150940#M6613</link>
      <description>&lt;P&gt;Please refer to the section "8.2.2.2 Updating remote connection" in the document.&lt;/P&gt;
&lt;P&gt;Please click Run-&amp;gt;Debug Configuration-&amp;gt;C/C++ Remote Application-&amp;gt;Edit&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="yipingwang_0-1599637943169.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/124750iC22563945B950517/image-size/medium?v=v2&amp;amp;px=400" role="button" title="yipingwang_0-1599637943169.png" alt="yipingwang_0-1599637943169.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Please specify the IP address of the Linux target board, specify the user name and password to login in the target board.&lt;/P&gt;</description>
      <pubDate>Wed, 09 Sep 2020 08:00:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1043A-DPAA-debug-on-CodeWarrior/m-p/1150940#M6613</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2020-09-09T08:00:38Z</dc:date>
    </item>
    <item>
      <title>Re: LS1043A DPAA debug on CodeWarrior</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1043A-DPAA-debug-on-CodeWarrior/m-p/1151139#M6615</link>
      <description>&lt;P&gt;Thank you. I dont know how to set up the IP address for the LS1043A board. That is what I want to ask&lt;/P&gt;</description>
      <pubDate>Wed, 09 Sep 2020 22:38:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1043A-DPAA-debug-on-CodeWarrior/m-p/1151139#M6615</guid>
      <dc:creator>smruthi_ramesh</dc:creator>
      <dc:date>2020-09-09T22:38:02Z</dc:date>
    </item>
    <item>
      <title>Re: LS1043A DPAA debug on CodeWarrior</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1043A-DPAA-debug-on-CodeWarrior/m-p/1151259#M6620</link>
      <description>&lt;P&gt;You could configure IP address on LS1043ARDB as the following&lt;/P&gt;&lt;P&gt;ifconfig&amp;nbsp;fm1-mac1 10.171.171.10&lt;/P&gt;&lt;P&gt;Then try whether you could use ssh to access the target board, with the user name and password specified in CodeWarrior IDE.&lt;/P&gt;</description>
      <pubDate>Thu, 10 Sep 2020 03:42:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1043A-DPAA-debug-on-CodeWarrior/m-p/1151259#M6620</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2020-09-10T03:42:02Z</dc:date>
    </item>
    <item>
      <title>Re: LS1043A DPAA debug on CodeWarrior</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1043A-DPAA-debug-on-CodeWarrior/m-p/1151761#M6632</link>
      <description>&lt;P&gt;I tried that and am getting the following error:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="smruthi_ramesh_0-1599774403919.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/124870iC8B839967039FCEA/image-size/medium?v=v2&amp;amp;px=400" role="button" title="smruthi_ramesh_0-1599774403919.png" alt="smruthi_ramesh_0-1599774403919.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I tried to ssh into the IP address but it gave a connection timeout error.&lt;/P&gt;</description>
      <pubDate>Thu, 10 Sep 2020 21:47:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1043A-DPAA-debug-on-CodeWarrior/m-p/1151761#M6632</guid>
      <dc:creator>smruthi_ramesh</dc:creator>
      <dc:date>2020-09-10T21:47:18Z</dc:date>
    </item>
    <item>
      <title>Re: LS1043A DPAA debug on CodeWarrior</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1043A-DPAA-debug-on-CodeWarrior/m-p/1152055#M6638</link>
      <description>&lt;P&gt;Which version SDK/LSDK are you using on the target board?&lt;/P&gt;
&lt;P&gt;How do you boot up the target board? Would you please provide the whole console log booting up the target board?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 11 Sep 2020 08:50:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1043A-DPAA-debug-on-CodeWarrior/m-p/1152055#M6638</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2020-09-11T08:50:23Z</dc:date>
    </item>
    <item>
      <title>Re: LS1043A DPAA debug on CodeWarrior</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1043A-DPAA-debug-on-CodeWarrior/m-p/1152352#M6643</link>
      <description>&lt;P&gt;I am using LSDK 2004. I am booting the board with an SD card that has the LSDK 2004 version&lt;/P&gt;&lt;P&gt;I am attaching screenshots of the boot log.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="7.jpg" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/124973iC4D5A32A1229EB32/image-size/medium?v=v2&amp;amp;px=400" role="button" title="7.jpg" alt="7.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="6.jpg" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/124970i087234293EC75633/image-size/medium?v=v2&amp;amp;px=400" role="button" title="6.jpg" alt="6.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="5.jpg" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/124971iF2D3548ACD6CC801/image-size/medium?v=v2&amp;amp;px=400" role="button" title="5.jpg" alt="5.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="4.jpg" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/124975iAE1A133BCA0D00B1/image-size/medium?v=v2&amp;amp;px=400" role="button" title="4.jpg" alt="4.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="3.jpg" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/124972i2E618F1813372A26/image-size/medium?v=v2&amp;amp;px=400" role="button" title="3.jpg" alt="3.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="2.jpg" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/124974i516ECD8CA81C86FB/image-size/medium?v=v2&amp;amp;px=400" role="button" title="2.jpg" alt="2.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="1.jpg" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/124976iD1F3EDBC05D64787/image-size/medium?v=v2&amp;amp;px=400" role="button" title="1.jpg" alt="1.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="9.jpg" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/124978i8D5ACB3B0569B04F/image-size/medium?v=v2&amp;amp;px=400" role="button" title="9.jpg" alt="9.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="8.jpg" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/124977i3680874D96A0A96B/image-size/medium?v=v2&amp;amp;px=400" role="button" title="8.jpg" alt="8.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;         &lt;/P&gt;</description>
      <pubDate>Sat, 12 Sep 2020 00:51:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1043A-DPAA-debug-on-CodeWarrior/m-p/1152352#M6643</guid>
      <dc:creator>smruthi_ramesh</dc:creator>
      <dc:date>2020-09-12T00:51:23Z</dc:date>
    </item>
    <item>
      <title>Re: LS1043A DPAA debug on CodeWarrior</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1043A-DPAA-debug-on-CodeWarrior/m-p/1154869#M6669</link>
      <description>&lt;P&gt;why don't you use gdb for debugging?&amp;nbsp;&lt;/P&gt;
&lt;P&gt;you can use gdbserver and gdb client for line by line debugging.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 17 Sep 2020 14:29:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1043A-DPAA-debug-on-CodeWarrior/m-p/1154869#M6669</guid>
      <dc:creator>hemantagrawal</dc:creator>
      <dc:date>2020-09-17T14:29:11Z</dc:date>
    </item>
    <item>
      <title>Re: LS1043A DPAA debug on CodeWarrior</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1043A-DPAA-debug-on-CodeWarrior/m-p/1155103#M6672</link>
      <description>&lt;P&gt;Okay will try that. Thanks&lt;/P&gt;</description>
      <pubDate>Fri, 18 Sep 2020 00:13:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1043A-DPAA-debug-on-CodeWarrior/m-p/1155103#M6672</guid>
      <dc:creator>smruthi_ramesh</dc:creator>
      <dc:date>2020-09-18T00:13:29Z</dc:date>
    </item>
    <item>
      <title>Re: LS1043A DPAA debug on CodeWarrior</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1043A-DPAA-debug-on-CodeWarrior/m-p/1156036#M6686</link>
      <description>&lt;P&gt;In USDPAA dts file&amp;nbsp;fsl-ls1043a-rdb-usdpaa.dts, all Ethernet ports have been assigned to DPDK, you need to delete one Ethernet port definition in the dts file to assign it to Linux Kernel.&lt;/P&gt;
&lt;P&gt;fsl,dpaa {&lt;BR /&gt;compatible = "fsl,ls1043a", "fsl,dpaa", "simple-bus";&lt;BR /&gt;dma-coherent;&lt;/P&gt;
&lt;P&gt;/* ethernet@0 {&lt;BR /&gt;compatible = "fsl,dpa-ethernet-init";&lt;BR /&gt;fsl,bman-buffer-pools = &amp;lt;&amp;amp;bp7 &amp;amp;bp8 &amp;amp;bp9&amp;gt;;&lt;BR /&gt;fsl,qman-frame-queues-rx = &amp;lt;0x50 1 0x51 1&amp;gt;;&lt;BR /&gt;fsl,qman-frame-queues-tx = &amp;lt;0x70 1 0x71 1&amp;gt;;&lt;BR /&gt;};*/&lt;/P&gt;
&lt;P&gt;... ...&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 21 Sep 2020 06:56:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1043A-DPAA-debug-on-CodeWarrior/m-p/1156036#M6686</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2020-09-21T06:56:53Z</dc:date>
    </item>
  </channel>
</rss>