<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Layerscape中的主题 Re: LS1046A USB Controller VBUS requirements</title>
    <link>https://community.nxp.com/t5/Layerscape/LS1046A-USB-Controller-VBUS-requirements/m-p/1150725#M6609</link>
    <description>&lt;P&gt;The nominal voltage for this pin is 5 V.&lt;/P&gt;
&lt;P&gt;There is an internal comparator; if VBUS drops below about 4.4v, an over-current is signaled and the port is shut down.&lt;/P&gt;</description>
    <pubDate>Wed, 09 Sep 2020 02:53:21 GMT</pubDate>
    <dc:creator>ufedor</dc:creator>
    <dc:date>2020-09-09T02:53:21Z</dc:date>
    <item>
      <title>LS1046A USB Controller VBUS requirements</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1046A-USB-Controller-VBUS-requirements/m-p/1064237#M6083</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm currently designing a PCB using an LS1046A, and wish to use the USB controllers.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm trying to figure out how to connect the VBUS pins on the controllers.The devices&amp;nbsp;I am communicating with do not require a VBUS connection, just the data lines. I also do not have a 5V supply currently on my PCB, so I would have to place down a supply just for this VBUS connection. It seems unusual that a 5V supply is required in addition to the 3V3 and 1V0 USB supplies.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I think that connection is required but I can't find much documentation on this. The datasheet doesn't give requirements for the VBUS pins. AN5252 Table 22 says that&amp;nbsp;connection is&amp;nbsp;compulsory and the pins have a voltage range of "0-5.25V", but does not give an estimated current draw.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The LS1046ARDB schematic appears to connect the USB_3 VBUS to USB_P2_PWR, but this&amp;nbsp;net is not powered (pin C1 of U3 is tied low). Does this mean that the USB3 bus is non functional on&amp;nbsp;&lt;SPAN&gt;LS1046ARDB?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Are the VBUS pins compulsory for operation of the USB busses? if so, how much current do they draw? And are there any sequencing requirements for this power supply?&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 18 Jun 2020 14:00:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1046A-USB-Controller-VBUS-requirements/m-p/1064237#M6083</guid>
      <dc:creator>jlt1</dc:creator>
      <dc:date>2020-06-18T14:00:14Z</dc:date>
    </item>
    <item>
      <title>Re: LS1046A USB Controller VBUS requirements</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1046A-USB-Controller-VBUS-requirements/m-p/1064238#M6084</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;gt; Are the VBUS pins compulsory for operation of the USB busses?&lt;/P&gt;&lt;P&gt;Yes.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;gt; if so, how much current do they draw?&lt;/P&gt;&lt;P&gt;The current is negligibly small.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;gt; And are there any sequencing requirements for this power supply?&lt;/P&gt;&lt;P&gt;No.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;gt; pin C1 of U3 is tied low&lt;/P&gt;&lt;P&gt;USB2_PWREN is controlled by U8.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 18 Jun 2020 16:23:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1046A-USB-Controller-VBUS-requirements/m-p/1064238#M6084</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2020-06-18T16:23:15Z</dc:date>
    </item>
    <item>
      <title>Re: LS1046A USB Controller VBUS requirements</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1046A-USB-Controller-VBUS-requirements/m-p/1064239#M6085</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks very much for the prompt reply&amp;nbsp;&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/ufedor"&gt;ufedor&lt;/A&gt;!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;&amp;gt; USB2_PWREN is controlled by U8.&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;Oops, not sure how I missed that IC, sorry!&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;&lt;/P&gt;&lt;P style="border: 0px;"&gt;&amp;gt;The current is negligibly small.&lt;/P&gt;&lt;P style="border: 0px;"&gt;Negligibly small being &amp;lt;5mA? Just asking to see if it is feasible to use an LDO from my input rail, without burning too much power.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 18 Jun 2020 16:30:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1046A-USB-Controller-VBUS-requirements/m-p/1064239#M6085</guid>
      <dc:creator>jlt1</dc:creator>
      <dc:date>2020-06-18T16:30:45Z</dc:date>
    </item>
    <item>
      <title>Re: LS1046A USB Controller VBUS requirements</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1046A-USB-Controller-VBUS-requirements/m-p/1064240#M6086</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;gt; Negligibly small being &amp;lt;5mA?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;lt;50uA&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 18 Jun 2020 16:38:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1046A-USB-Controller-VBUS-requirements/m-p/1064240#M6086</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2020-06-18T16:38:22Z</dc:date>
    </item>
    <item>
      <title>Re: LS1046A USB Controller VBUS requirements</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1046A-USB-Controller-VBUS-requirements/m-p/1150537#M6606</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/56916"&gt;@ufedor&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is it mandatory to feed that pin with 5V ? or 3.3V would be ok ?&lt;/P&gt;&lt;P&gt;What is the use of this pin for the LS1046 internally ?&lt;/P&gt;&lt;P&gt;What is the VIH of this pin ?&lt;/P&gt;&lt;P&gt;Thanks in advance !&lt;/P&gt;</description>
      <pubDate>Tue, 08 Sep 2020 19:15:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1046A-USB-Controller-VBUS-requirements/m-p/1150537#M6606</guid>
      <dc:creator>spoulin</dc:creator>
      <dc:date>2020-09-08T19:15:14Z</dc:date>
    </item>
    <item>
      <title>Re: LS1046A USB Controller VBUS requirements</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1046A-USB-Controller-VBUS-requirements/m-p/1150725#M6609</link>
      <description>&lt;P&gt;The nominal voltage for this pin is 5 V.&lt;/P&gt;
&lt;P&gt;There is an internal comparator; if VBUS drops below about 4.4v, an over-current is signaled and the port is shut down.&lt;/P&gt;</description>
      <pubDate>Wed, 09 Sep 2020 02:53:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1046A-USB-Controller-VBUS-requirements/m-p/1150725#M6609</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2020-09-09T02:53:21Z</dc:date>
    </item>
    <item>
      <title>Re: LS1046A USB Controller VBUS requirements</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1046A-USB-Controller-VBUS-requirements/m-p/1156340#M6694</link>
      <description>&lt;P&gt;Thanks Ufedor, it is appreciated.&lt;/P&gt;&lt;P&gt;Regards !&lt;/P&gt;&lt;P&gt;Sylvain&lt;/P&gt;</description>
      <pubDate>Mon, 21 Sep 2020 14:56:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1046A-USB-Controller-VBUS-requirements/m-p/1156340#M6694</guid>
      <dc:creator>spoulin</dc:creator>
      <dc:date>2020-09-21T14:56:14Z</dc:date>
    </item>
    <item>
      <title>Re: LS1046A USB Controller VBUS requirements</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1046A-USB-Controller-VBUS-requirements/m-p/1662765#M12599</link>
      <description>&lt;P&gt;When USB is configured as a USB host, VBUS pin is not used. It is only used when USB is configured as USB device. Connect a 3.3V to VBUS should work even it is configured as a USB device.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 02 Jun 2023 15:45:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1046A-USB-Controller-VBUS-requirements/m-p/1662765#M12599</guid>
      <dc:creator>jimmy_zhao</dc:creator>
      <dc:date>2023-06-02T15:45:19Z</dc:date>
    </item>
  </channel>
</rss>