<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Using a different nor flash chip with ls1021a twr board in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/Using-a-different-nor-flash-chip-with-ls1021a-twr-board/m-p/1147682#M6584</link>
    <description>&lt;P&gt;I'm using a custom board based on ls1021a-twr board,&lt;/P&gt;&lt;P&gt;The reference board uses mt28ew01gaba1hjs-0sit as the nor flash chip connected to the ifc bus,&lt;/P&gt;&lt;P&gt;But the custom board uses is29gl256-70flet,&lt;/P&gt;&lt;P&gt;what changes should I make to the source?&lt;/P&gt;</description>
    <pubDate>Fri, 04 Sep 2020 11:13:14 GMT</pubDate>
    <dc:creator>sujay1</dc:creator>
    <dc:date>2020-09-04T11:13:14Z</dc:date>
    <item>
      <title>Using a different nor flash chip with ls1021a twr board</title>
      <link>https://community.nxp.com/t5/Layerscape/Using-a-different-nor-flash-chip-with-ls1021a-twr-board/m-p/1147682#M6584</link>
      <description>&lt;P&gt;I'm using a custom board based on ls1021a-twr board,&lt;/P&gt;&lt;P&gt;The reference board uses mt28ew01gaba1hjs-0sit as the nor flash chip connected to the ifc bus,&lt;/P&gt;&lt;P&gt;But the custom board uses is29gl256-70flet,&lt;/P&gt;&lt;P&gt;what changes should I make to the source?&lt;/P&gt;</description>
      <pubDate>Fri, 04 Sep 2020 11:13:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Using-a-different-nor-flash-chip-with-ls1021a-twr-board/m-p/1147682#M6584</guid>
      <dc:creator>sujay1</dc:creator>
      <dc:date>2020-09-04T11:13:14Z</dc:date>
    </item>
    <item>
      <title>Re: Using a different nor flash chip with ls1021a twr board</title>
      <link>https://community.nxp.com/t5/Layerscape/Using-a-different-nor-flash-chip-with-ls1021a-twr-board/m-p/1149238#M6587</link>
      <description>&lt;P&gt;It is needed to download datasheets of both NOR Flash devices, compare them and accordingly modify the board's header file, for example 'ls1021atwr.h':&lt;/P&gt;
&lt;P&gt;&lt;A href="https://source.codeaurora.org/external/qoriq/qoriq-components/u-boot/tree/include/configs/ls1021atwr.h?h=v2020.07" target="_blank"&gt;https://source.codeaurora.org/external/qoriq/qoriq-components/u-boot/tree/include/configs/ls1021atwr.h?h=v2020.07&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Sat, 05 Sep 2020 09:09:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Using-a-different-nor-flash-chip-with-ls1021a-twr-board/m-p/1149238#M6587</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2020-09-05T09:09:09Z</dc:date>
    </item>
    <item>
      <title>Re: Using a different nor flash chip with ls1021a twr board</title>
      <link>https://community.nxp.com/t5/Layerscape/Using-a-different-nor-flash-chip-with-ls1021a-twr-board/m-p/1149248#M6588</link>
      <description>&lt;P&gt;Hi Ufedor,&lt;/P&gt;&lt;P&gt;Thanks for the support, However it's unclear what I need to change could you give me an example of a field I should modify?&lt;/P&gt;</description>
      <pubDate>Sat, 05 Sep 2020 11:37:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Using-a-different-nor-flash-chip-with-ls1021a-twr-board/m-p/1149248#M6588</guid>
      <dc:creator>sujay1</dc:creator>
      <dc:date>2020-09-05T11:37:23Z</dc:date>
    </item>
    <item>
      <title>Re: Using a different nor flash chip with ls1021a twr board</title>
      <link>https://community.nxp.com/t5/Layerscape/Using-a-different-nor-flash-chip-with-ls1021a-twr-board/m-p/1149280#M6589</link>
      <description>&lt;P&gt;Please refer to the section "* IFC Definitions".&lt;/P&gt;</description>
      <pubDate>Sun, 06 Sep 2020 03:02:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Using-a-different-nor-flash-chip-with-ls1021a-twr-board/m-p/1149280#M6589</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2020-09-06T03:02:15Z</dc:date>
    </item>
  </channel>
</rss>