<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Layerscape中的主题 Re: LS1046A DDR4 Hyperlynx simulation</title>
    <link>https://community.nxp.com/t5/Layerscape/LS1046A-DDR4-Hyperlynx-simulation/m-p/1096464#M6526</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Moshe&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 21 May 2020 05:28:47 GMT</pubDate>
    <dc:creator>moshemarcu</dc:creator>
    <dc:date>2020-05-21T05:28:47Z</dc:date>
    <item>
      <title>LS1046A DDR4 Hyperlynx simulation</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1046A-DDR4-Hyperlynx-simulation/m-p/1096458#M6520</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using LS1046A and I am trying to simulate its DDR4 interface (at 2100MT/s) using Hyperlynx of Mentor.&lt;/P&gt;&lt;P&gt;I am a bit confused regarding filling two parameters for the controller (LS1046A) for the Read cycles.&lt;/P&gt;&lt;P&gt;The Hyperlynx requires two parameters, TDIVW&amp;nbsp; (RX mask) and TDIPW (minimum required pulse width)&lt;/P&gt;&lt;P&gt;The datasheet gives only TCISKEW (±80ps).&lt;/P&gt;&lt;P&gt;Does the TCISKEW equivalent to the TDIVW? What values should I fill for those 2 parameters?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Moshe&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 18 May 2020 06:35:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1046A-DDR4-Hyperlynx-simulation/m-p/1096458#M6520</guid>
      <dc:creator>moshemarcu</dc:creator>
      <dc:date>2020-05-18T06:35:54Z</dc:date>
    </item>
    <item>
      <title>Re: LS1046A DDR4 Hyperlynx simulation</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1046A-DDR4-Hyperlynx-simulation/m-p/1096459#M6521</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;DDR controller requires minimum data input valid window to be equal to &lt;SPAN class=""&gt;tCISKEWmax - tCISKEWmin, for 2100MT/S it is 160ps.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Regards,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Bulat&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 18 May 2020 16:23:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1046A-DDR4-Hyperlynx-simulation/m-p/1096459#M6521</guid>
      <dc:creator>Bulat</dc:creator>
      <dc:date>2020-05-18T16:23:17Z</dc:date>
    </item>
    <item>
      <title>Re: LS1046A DDR4 Hyperlynx simulation</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1046A-DDR4-Hyperlynx-simulation/m-p/1096460#M6522</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Thanks for the answer,&lt;/P&gt;&lt;P&gt;Does the valid window need to be centered relative to the DQS? Does the LS1046A support read leveling?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Moshe&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 18 May 2020 18:31:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1046A-DDR4-Hyperlynx-simulation/m-p/1096460#M6522</guid>
      <dc:creator>moshemarcu</dc:creator>
      <dc:date>2020-05-18T18:31:40Z</dc:date>
    </item>
    <item>
      <title>Re: LS1046A DDR4 Hyperlynx simulation</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1046A-DDR4-Hyperlynx-simulation/m-p/1096461#M6523</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, the LS1046A supports read leveling. No special actions like "centering" is required, the LS1046A performs all required calibrations internally.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Bulat&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 May 2020 09:09:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1046A-DDR4-Hyperlynx-simulation/m-p/1096461#M6523</guid>
      <dc:creator>Bulat</dc:creator>
      <dc:date>2020-05-20T09:09:30Z</dc:date>
    </item>
    <item>
      <title>Re: LS1046A DDR4 Hyperlynx simulation</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1046A-DDR4-Hyperlynx-simulation/m-p/1096462#M6524</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Bulat,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What kind of read leveling does the LS1046A supports?&lt;/P&gt;&lt;P&gt;Does each DQ can be individually delayed to optimize it with respect to the DQS or&lt;/P&gt;&lt;P&gt;only the DQS signal can be adjusted to optimize it to all the DQ signals?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I could not find any information regarding the read leveling support in the reference manual, how do I configure the LS1046A to activate this process?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Moshe&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 May 2020 14:51:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1046A-DDR4-Hyperlynx-simulation/m-p/1096462#M6524</guid>
      <dc:creator>moshemarcu</dc:creator>
      <dc:date>2020-05-20T14:51:21Z</dc:date>
    </item>
    <item>
      <title>Re: LS1046A DDR4 Hyperlynx simulation</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1046A-DDR4-Hyperlynx-simulation/m-p/1096463#M6525</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Read leveling assumes that the DDR controller calibrates the time when the DQS comes from the SDRAM, and then shifts DQS to the center of the data valid window. This is done individually for each byte lane after the DDR controller is enabled with MEM_EN=1. No individual DQ delays, the user must follow DDR4 layout rules, for 2100MT/s rate DQ signals should be trace-matched within +/-5 mils to respective DQS.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Bulat&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 May 2020 16:12:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1046A-DDR4-Hyperlynx-simulation/m-p/1096463#M6525</guid>
      <dc:creator>Bulat</dc:creator>
      <dc:date>2020-05-20T16:12:01Z</dc:date>
    </item>
    <item>
      <title>Re: LS1046A DDR4 Hyperlynx simulation</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1046A-DDR4-Hyperlynx-simulation/m-p/1096464#M6526</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Moshe&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 May 2020 05:28:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1046A-DDR4-Hyperlynx-simulation/m-p/1096464#M6526</guid>
      <dc:creator>moshemarcu</dc:creator>
      <dc:date>2020-05-21T05:28:47Z</dc:date>
    </item>
  </channel>
</rss>