<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LayerscapeのトピックLS1028A DP firmware load failed</title>
    <link>https://community.nxp.com/t5/Layerscape/LS1028A-DP-firmware-load-failed/m-p/1086004#M6398</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;I conducted some tests on the LSDK1909 on the ls1028a-rdb platform, and I found that the probabilistic loading of the firmware of the mali-dp failed during the startup process, resulting in the inability to display images after startup&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;[ 2.549298] [drm] Started firmware!&lt;BR /&gt;[ 17.549461] [drm:hdp_fw_init] *ERROR* CDN_API_CheckAlive failed - check firmware!&lt;BR /&gt;[ 17.556973] [drm:imx_hdp_imx_bind] *ERROR* Failed to initialise HDP firmware&lt;BR /&gt;[ 17.564067] mali-dp f080000.malidp: failed to bind f200000.hdp (ops imx_hdp_imx_ops): -6&lt;BR /&gt;[ 17.572195] [drm:malidp_bind] *ERROR* Failed to bind all components&lt;BR /&gt;[ 17.578566] mali-dp f080000.malidp: master bind failed: -6&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;High probability, easy to reproduce，Is there a solution to this problem？&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;In addition, I have an additional question. Does the dp of ls1028a not support audio?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 28 Apr 2020 01:11:03 GMT</pubDate>
    <dc:creator>lizuobin</dc:creator>
    <dc:date>2020-04-28T01:11:03Z</dc:date>
    <item>
      <title>LS1028A DP firmware load failed</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1028A-DP-firmware-load-failed/m-p/1086004#M6398</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;I conducted some tests on the LSDK1909 on the ls1028a-rdb platform, and I found that the probabilistic loading of the firmware of the mali-dp failed during the startup process, resulting in the inability to display images after startup&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;[ 2.549298] [drm] Started firmware!&lt;BR /&gt;[ 17.549461] [drm:hdp_fw_init] *ERROR* CDN_API_CheckAlive failed - check firmware!&lt;BR /&gt;[ 17.556973] [drm:imx_hdp_imx_bind] *ERROR* Failed to initialise HDP firmware&lt;BR /&gt;[ 17.564067] mali-dp f080000.malidp: failed to bind f200000.hdp (ops imx_hdp_imx_ops): -6&lt;BR /&gt;[ 17.572195] [drm:malidp_bind] *ERROR* Failed to bind all components&lt;BR /&gt;[ 17.578566] mali-dp f080000.malidp: master bind failed: -6&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;High probability, easy to reproduce，Is there a solution to this problem？&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;In addition, I have an additional question. Does the dp of ls1028a not support audio?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Apr 2020 01:11:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1028A-DP-firmware-load-failed/m-p/1086004#M6398</guid>
      <dc:creator>lizuobin</dc:creator>
      <dc:date>2020-04-28T01:11:03Z</dc:date>
    </item>
    <item>
      <title>Re: LS1028A DP firmware load failed</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1028A-DP-firmware-load-failed/m-p/1086005#M6399</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HDP firmware binary is loaded during U-Boot. At U-Boot prompt, copy the firmware binary from any storage medium (NOR flash or SD/eMMC) to DDR memory. Use the following command to load the binary:&lt;/P&gt;&lt;P&gt;=&amp;gt; hdp load &amp;lt;address&amp;gt; &amp;lt;offset&amp;gt;&lt;/P&gt;&lt;ADDRESS&gt;&lt;/ADDRESS&gt;&lt;ADDRESS&gt;&lt;/ADDRESS&gt;&lt;ADDRESS&gt;where: • address - address where the firmware binary starts in DDR memory&lt;/ADDRESS&gt;&lt;ADDRESS&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;• offset - IRAM offset in the firmware binary (8192 default)&lt;/ADDRESS&gt;&lt;ADDRESS&gt;For example: =&amp;gt;hdp load 0x98000000 0x2000&lt;/ADDRESS&gt;&lt;ADDRESS&gt;&lt;/ADDRESS&gt;&lt;ADDRESS&gt;a. Get DP firmware with XSPI flash boot:&lt;/ADDRESS&gt;&lt;ADDRESS&gt;=&amp;gt; run xspi_hdploadcmd&lt;/ADDRESS&gt;&lt;ADDRESS&gt;b. Get DP firmware with SD boot&lt;/ADDRESS&gt;&lt;ADDRESS&gt;=&amp;gt; run sd_hdploadcmd&lt;/ADDRESS&gt;&lt;ADDRESS&gt;c. Get DP firmware with EMMC boot&lt;/ADDRESS&gt;&lt;ADDRESS&gt;=&amp;gt; run emmc_hdploadcmd&lt;/ADDRESS&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Apr 2020 02:50:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1028A-DP-firmware-load-failed/m-p/1086005#M6399</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2020-04-28T02:50:43Z</dc:date>
    </item>
    <item>
      <title>Re: LS1028A DP firmware load failed</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1028A-DP-firmware-load-failed/m-p/1086006#M6400</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;This may be a hardware design issue. When the software is reset, the SD card is still in 1.8V mode, which causes the SD card to fail to load firmware.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does the dp of ls1028 support audio output?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Apr 2020 03:09:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1028A-DP-firmware-load-failed/m-p/1086006#M6400</guid>
      <dc:creator>lizuobin</dc:creator>
      <dc:date>2020-04-28T03:09:04Z</dc:date>
    </item>
    <item>
      <title>Re: LS1028A DP firmware load failed</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1028A-DP-firmware-load-failed/m-p/1086007#M6401</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You could refer to "7.2.12 Synchronous Audio Interface (SAI)" in LSDK 19.09 user guide for audio.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Apr 2020 03:32:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1028A-DP-firmware-load-failed/m-p/1086007#M6401</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2020-04-28T03:32:19Z</dc:date>
    </item>
  </channel>
</rss>