<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: CCSR Block Address in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/CCSR-Block-Address/m-p/1085878#M6397</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please refer to the QorIQ LS1021A Reference Manual, Table 9-2. Required format of data structure used by PBL, note 2:&lt;/P&gt;&lt;P&gt;"SYS_ADDR = 0x61_0040 is a PBI CRC check command (PBL block base address 0x161_0000, but only 24-bits address are used here)."&lt;/P&gt;&lt;P&gt;Also consider that "write" in PBI corresponds to the ACS=0 (CCSR space) and "awrite" corresponds to the ACS=1.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 11 Jul 2020 06:18:18 GMT</pubDate>
    <dc:creator>ufedor</dc:creator>
    <dc:date>2020-07-11T06:18:18Z</dc:date>
    <item>
      <title>CCSR Block Address</title>
      <link>https://community.nxp.com/t5/Layerscape/CCSR-Block-Address/m-p/1085877#M6396</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;The CCSR Block_Base_Address starts from 1000000...Why are we excluding 1 in rcw files?? like for ex in file rcw_1200_qspiboot.rcw , it is written as write 0x57015c, 0x40100000??&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 10 Jul 2020 09:17:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/CCSR-Block-Address/m-p/1085877#M6396</guid>
      <dc:creator>rashmikj</dc:creator>
      <dc:date>2020-07-10T09:17:24Z</dc:date>
    </item>
    <item>
      <title>Re: CCSR Block Address</title>
      <link>https://community.nxp.com/t5/Layerscape/CCSR-Block-Address/m-p/1085878#M6397</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please refer to the QorIQ LS1021A Reference Manual, Table 9-2. Required format of data structure used by PBL, note 2:&lt;/P&gt;&lt;P&gt;"SYS_ADDR = 0x61_0040 is a PBI CRC check command (PBL block base address 0x161_0000, but only 24-bits address are used here)."&lt;/P&gt;&lt;P&gt;Also consider that "write" in PBI corresponds to the ACS=0 (CCSR space) and "awrite" corresponds to the ACS=1.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 11 Jul 2020 06:18:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/CCSR-Block-Address/m-p/1085878#M6397</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2020-07-11T06:18:18Z</dc:date>
    </item>
  </channel>
</rss>