<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LS1043A-RGW boot failure in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/LS1043A-RGW-boot-failure/m-p/1082262#M6371</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I compared the flex-installer for the newest SDK with this - and there was one parameter I added.&lt;/P&gt;&lt;P&gt;Still no luck....&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a couple more questions about this:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It says here that it successfully mounted it:&lt;/P&gt;&lt;P&gt;&amp;nbsp; [&amp;nbsp;&amp;nbsp;&amp;nbsp; 3.637912] EXT4-fs (mmcblk0p3): couldn't mount as ext3 due to feature incompatibilities&lt;BR /&gt;&amp;nbsp; [&amp;nbsp;&amp;nbsp;&amp;nbsp; 3.673534] EXT4-fs (mmcblk0p3): mounted filesystem with ordered data mode. Opts: (null)&lt;BR /&gt;&amp;nbsp; &lt;STRONG&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 3.681636] VFS: Mounted root (ext4 filesystem) on device 179:3.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Why it is trying to mount as ext3 first, I also did an e2fsck on this partition:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&lt;STRONG&gt;&amp;nbsp; tom@newSNIPC:~$ sudo e2fsck /dev/sdd4&lt;/STRONG&gt;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;&lt;STRONG&gt;&amp;nbsp; e2fsck 1.44.1 (24-Mar-2018)&lt;/STRONG&gt;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;&lt;STRONG&gt;&amp;nbsp; system: clean, 71311/1479856 files, 645570/5912960 blocks&lt;/STRONG&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So, I am confused why it is having an issue. There is a &lt;EM&gt;&lt;STRONG&gt;/sbin/init&lt;/STRONG&gt;&lt;/EM&gt; (points to /&lt;STRONG&gt;lib/systemd/systemd&lt;/STRONG&gt;)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Tom&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 10 Apr 2020 23:27:25 GMT</pubDate>
    <dc:creator>tmorrison</dc:creator>
    <dc:date>2020-04-10T23:27:25Z</dc:date>
    <item>
      <title>LS1043A-RGW boot failure</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1043A-RGW-boot-failure/m-p/1082259#M6368</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We have a custom board - largely based upon the NXP LS1043A-RGW Development board&lt;/P&gt;&lt;P&gt;We are using the LSDK 18.03 with some patches to be able to customize it. We are having&lt;/P&gt;&lt;P&gt;some problems in several different areas, but I have patched around those to try to get linux&lt;/P&gt;&lt;P&gt;to boot all the way.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The LSDK is flex-builder based and I have built a firmware,&amp;nbsp; bootpartition, and rootfs. I load&lt;/P&gt;&lt;P&gt;that onto a sd card, and try to boot from that SD Card. I get this at the end:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&lt;STRONG&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 3.411691] EXT4-fs (mmcblk0p3): couldn't mount as ext3 due to feature incompatibilities&lt;/STRONG&gt;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;&lt;STRONG&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 3.453190] EXT4-fs (mmcblk0p3): mounted filesystem with ordered data mode. Opts: (null)&lt;/STRONG&gt;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;&lt;STRONG&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 3.461292] VFS: Mounted root (ext4 filesystem) on device 179:3.&lt;/STRONG&gt;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;&lt;STRONG&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 3.468133] devtmpfs: error mounting -2&lt;/STRONG&gt;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;&lt;STRONG&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 3.472210] Freeing unused kernel memory: 832K&lt;/STRONG&gt;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;&lt;STRONG&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 3.476726] Kernel panic - not syncing: No working init found.&amp;nbsp; Try passing init= option to kernel. See Linux Documentation/admin-guide/init.rst for guidance.&lt;/STRONG&gt;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;&lt;STRONG&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 3.490883] CPU: 1 PID: 1 Comm: swapper/0 Not tainted 4.14.16-dirty #6&lt;/STRONG&gt;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;&lt;STRONG&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 3.497397] Hardware name: LS1043A RGW Board (DT)&lt;/STRONG&gt;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;&lt;STRONG&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 3.502089] Call trace:&lt;/STRONG&gt;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;&lt;STRONG&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 3.504531] [&amp;lt;ffff000008088c70&amp;gt;] dump_backtrace+0x0/0x370&lt;/STRONG&gt;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;&lt;STRONG&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 3.509920] [&amp;lt;ffff000008088ff4&amp;gt;] show_stack+0x14/0x20&lt;/STRONG&gt;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;&lt;STRONG&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 3.514963] [&amp;lt;ffff000008b0e380&amp;gt;] dump_stack+0x9c/0xbc&lt;/STRONG&gt;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;&lt;STRONG&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 3.520004] [&amp;lt;ffff0000080c7b18&amp;gt;] panic+0x11c/0x28c&lt;/STRONG&gt;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;&lt;STRONG&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 3.524785] [&amp;lt;ffff000008b2093c&amp;gt;] kernel_init+0xec/0x100&lt;/STRONG&gt;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;&lt;STRONG&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 3.529999] [&amp;lt;ffff000008084be0&amp;gt;] ret_from_fork+0x10/0x18&lt;/STRONG&gt;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;&lt;STRONG&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 3.535301] SMP: stopping secondary CPUs&lt;/STRONG&gt;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;&lt;STRONG&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 3.539215] Kernel Offset: disabled&lt;/STRONG&gt;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;&lt;STRONG&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 3.542692] CPU features: 0x002004&lt;/STRONG&gt;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;&lt;STRONG&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 3.546082] Memory Limit: none&lt;/STRONG&gt;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;&lt;STRONG&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 3.549129] ---[ end Kernel panic - not syncing: No working init found.&amp;nbsp; Try passing init= option to kernel. See Linux Documentation/admin-guide/init.rst for guidance.&lt;/STRONG&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am assuming that the lsdk shouldn't have any of the problems that Linux Documentation/admin-guide/init.rst &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 10 Apr 2020 00:16:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1043A-RGW-boot-failure/m-p/1082259#M6368</guid>
      <dc:creator>tmorrison</dc:creator>
      <dc:date>2020-04-10T00:16:03Z</dc:date>
    </item>
    <item>
      <title>Re: LS1043A-RGW boot failure</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1043A-RGW-boot-failure/m-p/1082260#M6369</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Your Linux cannot mount the root filesystem due to certain FS feature&lt;BR /&gt;incompatibility. It is important how you format your SD card partitions&lt;BR /&gt;to put the images created by flex-builder. Use flex-installer from the&lt;BR /&gt;same LSDK release to populate your boot SD card. If you prefer to &lt;BR /&gt;format it by hand, look at flex-installer code, procedure partition_format_storage_device()&lt;BR /&gt;for the mkfs.ext4&amp;nbsp; invocation options. Note that you are &lt;BR /&gt;working with a pretty much obsolete LSDK version. You need to use &lt;BR /&gt;Ubuntu 16.04 on your build host for everything to work smoothly. Also, if it &lt;BR /&gt;is a heavily customized kernel, compare the LSDK default kernel configuration&lt;BR /&gt;with your one to ensure all necessary filesystem support options are &lt;BR /&gt;enabled.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please keep in mind, that we can provide a very limited support to &lt;BR /&gt;historical (l)SDK releases. If the suggestions above do not help,&lt;BR /&gt;our recommendation is to move to the most recent LSDK.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Platon&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 10 Apr 2020 08:05:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1043A-RGW-boot-failure/m-p/1082260#M6369</guid>
      <dc:creator>bpe</dc:creator>
      <dc:date>2020-04-10T08:05:11Z</dc:date>
    </item>
    <item>
      <title>Re: LS1043A-RGW boot failure</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1043A-RGW-boot-failure/m-p/1082261#M6370</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Platon,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for your quick response.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using the flex-installer that came with this LSDK.&lt;/P&gt;&lt;P&gt;I am sorry that this was NOT clear.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I will look at hand formatting.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using Ubuntu 18.04 because that was required for some of&lt;/P&gt;&lt;P&gt;the other LSDKs that I've unsuccessfully had no luck getting it to&lt;/P&gt;&lt;P&gt;work with a LS1043A-RGW.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am not sure how to  "downgrade" my Ubuntu to support this?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In addition, I am using this version of the LSDK because I was given&lt;/P&gt;&lt;P&gt;patches from you guys (&lt;STRONG&gt;NXP/Freescale&lt;/STRONG&gt;) that explicitly patch this version&lt;/P&gt;&lt;P&gt;of LSDK to support the LS1043A-RGW BSP. There are no supported&lt;/P&gt;&lt;P&gt;patches for newer LSDK's - I certainly would use them if I could.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I will update after I try hand formatting.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Tom&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 10 Apr 2020 12:40:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1043A-RGW-boot-failure/m-p/1082261#M6370</guid>
      <dc:creator>tmorrison</dc:creator>
      <dc:date>2020-04-10T12:40:20Z</dc:date>
    </item>
    <item>
      <title>Re: LS1043A-RGW boot failure</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1043A-RGW-boot-failure/m-p/1082262#M6371</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I compared the flex-installer for the newest SDK with this - and there was one parameter I added.&lt;/P&gt;&lt;P&gt;Still no luck....&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a couple more questions about this:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It says here that it successfully mounted it:&lt;/P&gt;&lt;P&gt;&amp;nbsp; [&amp;nbsp;&amp;nbsp;&amp;nbsp; 3.637912] EXT4-fs (mmcblk0p3): couldn't mount as ext3 due to feature incompatibilities&lt;BR /&gt;&amp;nbsp; [&amp;nbsp;&amp;nbsp;&amp;nbsp; 3.673534] EXT4-fs (mmcblk0p3): mounted filesystem with ordered data mode. Opts: (null)&lt;BR /&gt;&amp;nbsp; &lt;STRONG&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 3.681636] VFS: Mounted root (ext4 filesystem) on device 179:3.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Why it is trying to mount as ext3 first, I also did an e2fsck on this partition:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&lt;STRONG&gt;&amp;nbsp; tom@newSNIPC:~$ sudo e2fsck /dev/sdd4&lt;/STRONG&gt;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;&lt;STRONG&gt;&amp;nbsp; e2fsck 1.44.1 (24-Mar-2018)&lt;/STRONG&gt;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;&lt;STRONG&gt;&amp;nbsp; system: clean, 71311/1479856 files, 645570/5912960 blocks&lt;/STRONG&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So, I am confused why it is having an issue. There is a &lt;EM&gt;&lt;STRONG&gt;/sbin/init&lt;/STRONG&gt;&lt;/EM&gt; (points to /&lt;STRONG&gt;lib/systemd/systemd&lt;/STRONG&gt;)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Tom&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 10 Apr 2020 23:27:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1043A-RGW-boot-failure/m-p/1082262#M6371</guid>
      <dc:creator>tmorrison</dc:creator>
      <dc:date>2020-04-10T23:27:25Z</dc:date>
    </item>
    <item>
      <title>Re: LS1043A-RGW boot failure</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1043A-RGW-boot-failure/m-p/1082263#M6372</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I don't think this is answered completely - still not working for me - and I have verified everything I can.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 13 Apr 2020 15:29:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1043A-RGW-boot-failure/m-p/1082263#M6372</guid>
      <dc:creator>tmorrison</dc:creator>
      <dc:date>2020-04-13T15:29:04Z</dc:date>
    </item>
    <item>
      <title>Re: LS1043A-RGW boot failure</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1043A-RGW-boot-failure/m-p/1082264#M6373</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;can you please answer my questions I have asked about&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 13 Apr 2020 15:29:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1043A-RGW-boot-failure/m-p/1082264#M6373</guid>
      <dc:creator>tmorrison</dc:creator>
      <dc:date>2020-04-13T15:29:20Z</dc:date>
    </item>
    <item>
      <title>Re: LS1043A-RGW boot failure</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1043A-RGW-boot-failure/m-p/1082265#M6374</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Your recent inputs are not quite inline with the oirginal problem description. I particular, you are running fsck over /dev/sdd4 which should be a HDD based on it's name, but the problem is,&amp;nbsp; according to what you wrote earlier,&amp;nbsp; with a bootable SD card. fsck can help, but only if used in the proper way: if you can boot your system with a tinydistro ramdisk, try mounting the problematic partition by hand and running fsck on the target.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Platon&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 14 Apr 2020 08:00:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1043A-RGW-boot-failure/m-p/1082265#M6374</guid>
      <dc:creator>bpe</dc:creator>
      <dc:date>2020-04-14T08:00:14Z</dc:date>
    </item>
    <item>
      <title>Re: LS1043A-RGW boot failure</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1043A-RGW-boot-failure/m-p/1082266#M6375</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I will try this test soon!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 14 Apr 2020 18:53:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1043A-RGW-boot-failure/m-p/1082266#M6375</guid>
      <dc:creator>tmorrison</dc:creator>
      <dc:date>2020-04-14T18:53:11Z</dc:date>
    </item>
  </channel>
</rss>