<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Need final answer:  Sata on ls1043ardb in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/Need-final-answer-Sata-on-ls1043ardb/m-p/1074474#M6237</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;To make technical things clear at first please refer to the&amp;nbsp; QorIQ LS1043A Reference Manual, Table 33-1. Supported SerDes options.&lt;/P&gt;&lt;P&gt;In the table it is shown that there are several SerDes protocols (configurations) supporting SATA.&lt;/P&gt;&lt;P&gt;I.e., formally, LS1043A SerDes can be configured to expose SATA on lane D (3).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Concerning the LS1043ARDB.&lt;/P&gt;&lt;P&gt;Refer to the QorIQ LS1043A Reference Design Board Reference Manual, Figure 2-8. LS1043ARDB SerDes lane connections:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="serdes.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/114918i0895D7AEDC07E0CE/image-size/large?v=v2&amp;amp;px=999" role="button" title="serdes.jpg" alt="serdes.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;From this figure it is clear that SATA can be probed using a converter add-in card inserted into the PCIe x1 slot.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It is important to note that the RDB board has fixed connections of SerDes lanes, corresponding to protocol 1455.&lt;/P&gt;&lt;P&gt;If a SerDes protocol with SATA will be selected in RCW it will be impossible to use &lt;STRONG&gt;all&lt;/STRONG&gt; Ethernet ports connected to the SerDes lanes 0 and 1.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 08 Jul 2020 03:34:26 GMT</pubDate>
    <dc:creator>ufedor</dc:creator>
    <dc:date>2020-07-08T03:34:26Z</dc:date>
    <item>
      <title>Need final answer:  Sata on ls1043ardb</title>
      <link>https://community.nxp.com/t5/Layerscape/Need-final-answer-Sata-on-ls1043ardb/m-p/1074473#M6236</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Several shallow threads out there on the Sata ls1043ardb question.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;From a previous thread:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;gt;&amp;gt; it's posible run sata at LS1043ARDB. SATA serdes is multiplexing with PCIe. You only need is simple reduction from &amp;gt;&amp;gt; pcie connector to sata connector. Next step is change rcw to enable SATA and switch SW3[4] to 0 (100MHz clock). I &amp;gt;&amp;gt; work on LS1043ARDB with SATA without problems.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;From another previous thread where the question was Sata on ls1043a:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;gt;&amp;gt; This is not possible because SATA could be configured only on SerDes lane 3 (D), while mPCIe slot is connected to the lane 2 (C).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have done some work in this area myself.&amp;nbsp;&amp;nbsp;&amp;nbsp; I have changed the rcw to 0x3358 (verified upon boot), and also set the Switch SW3[4] to 0.&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; It booted up fine, but no Sata.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a simple PCIE to msata board.&amp;nbsp;&amp;nbsp;&amp;nbsp; Pretty sure the board (have 2 of them) is fine.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;At least need to know if the HW can do this, as I've already gone down a pretty deep rabbit hole.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Greatly appreciate any help.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;JR&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 08 Jul 2020 00:40:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Need-final-answer-Sata-on-ls1043ardb/m-p/1074473#M6236</guid>
      <dc:creator>john_reed</dc:creator>
      <dc:date>2020-07-08T00:40:10Z</dc:date>
    </item>
    <item>
      <title>Re: Need final answer:  Sata on ls1043ardb</title>
      <link>https://community.nxp.com/t5/Layerscape/Need-final-answer-Sata-on-ls1043ardb/m-p/1074474#M6237</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;To make technical things clear at first please refer to the&amp;nbsp; QorIQ LS1043A Reference Manual, Table 33-1. Supported SerDes options.&lt;/P&gt;&lt;P&gt;In the table it is shown that there are several SerDes protocols (configurations) supporting SATA.&lt;/P&gt;&lt;P&gt;I.e., formally, LS1043A SerDes can be configured to expose SATA on lane D (3).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Concerning the LS1043ARDB.&lt;/P&gt;&lt;P&gt;Refer to the QorIQ LS1043A Reference Design Board Reference Manual, Figure 2-8. LS1043ARDB SerDes lane connections:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="serdes.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/114918i0895D7AEDC07E0CE/image-size/large?v=v2&amp;amp;px=999" role="button" title="serdes.jpg" alt="serdes.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;From this figure it is clear that SATA can be probed using a converter add-in card inserted into the PCIe x1 slot.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It is important to note that the RDB board has fixed connections of SerDes lanes, corresponding to protocol 1455.&lt;/P&gt;&lt;P&gt;If a SerDes protocol with SATA will be selected in RCW it will be impossible to use &lt;STRONG&gt;all&lt;/STRONG&gt; Ethernet ports connected to the SerDes lanes 0 and 1.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 08 Jul 2020 03:34:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Need-final-answer-Sata-on-ls1043ardb/m-p/1074474#M6237</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2020-07-08T03:34:26Z</dc:date>
    </item>
    <item>
      <title>Re: Need final answer:  Sata on ls1043ardb</title>
      <link>https://community.nxp.com/t5/Layerscape/Need-final-answer-Sata-on-ls1043ardb/m-p/1074475#M6238</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Awesome!!&amp;nbsp;&amp;nbsp;&amp;nbsp; And thanks for that.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;A sidenote to my original post is that I also have a LS1012ARDB platform.&amp;nbsp;&amp;nbsp;&amp;nbsp; It has a sata interface on that board, with an actual SATA connector (not through PCIE).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I looked at the schematic for the pins feeding into the SATA connector.&amp;nbsp;&amp;nbsp;&amp;nbsp; On the 1012:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; - SD1_RX2_xx&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; - SD1_TX2_xx&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;On the LS1043arbd, mini pci-express, &lt;STRONG&gt;the same pins are being used:&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; - SD1_RX2_xx&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; - SD1_TX2_xx&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Assumption:&amp;nbsp; using same pins, so must work the same.&amp;nbsp;&amp;nbsp;&amp;nbsp; Turns out NOT TRUE.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Digging more today.....&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; The RX2/TX2 on 1012 is Lane D (sata works there).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; RX2/TX2 on 1043 is Lane C (sata does not work there)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Slowly figuring out things here......&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;JR&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 08 Jul 2020 20:56:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Need-final-answer-Sata-on-ls1043ardb/m-p/1074475#M6238</guid>
      <dc:creator>john_reed</dc:creator>
      <dc:date>2020-07-08T20:56:46Z</dc:date>
    </item>
    <item>
      <title>Re: Need final answer:  Sata on ls1043ardb</title>
      <link>https://community.nxp.com/t5/Layerscape/Need-final-answer-Sata-on-ls1043ardb/m-p/1074476#M6239</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="SATA_LaneD.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/115027iA74A05558C9D94E8/image-size/large?v=v2&amp;amp;px=999" role="button" title="SATA_LaneD.jpg" alt="SATA_LaneD.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="LaneD_3.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/115028i7DA02B394A099E52/image-size/large?v=v2&amp;amp;px=999" role="button" title="LaneD_3.jpg" alt="LaneD_3.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 09 Jul 2020 03:06:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Need-final-answer-Sata-on-ls1043ardb/m-p/1074476#M6239</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2020-07-09T03:06:09Z</dc:date>
    </item>
  </channel>
</rss>