<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Layerscape中的主题 rx_align_err in Testpmd</title>
    <link>https://community.nxp.com/t5/Layerscape/rx-align-err-in-Testpmd/m-p/1074389#M6235</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello dear,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would like to understand why I have rx_align_err counter increasing in my DPDK testpmd application.&lt;/P&gt;&lt;P&gt;I have one LS1043 board running pktgen connected to a LS1046 board over the 10G copper port running testpmd. I'm using LSDK 19.09. The forwarding works good however when I print the xstats in testpmd I have the following :&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="align_err.PNG"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/116562i64437C25B16E6119/image-size/large?v=v2&amp;amp;px=999" role="button" title="align_err.PNG" alt="align_err.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;After googling this type of issue it seems that it comes from CRC errors or odd bytes number.&lt;/P&gt;&lt;P&gt;I tried different setups (also with a lx2160 board) and different cables but the issue still remains.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Tanks for your help,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Etienne Cordroc'h&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 22 Jul 2020 07:09:42 GMT</pubDate>
    <dc:creator>etienne_cordroc</dc:creator>
    <dc:date>2020-07-22T07:09:42Z</dc:date>
    <item>
      <title>rx_align_err in Testpmd</title>
      <link>https://community.nxp.com/t5/Layerscape/rx-align-err-in-Testpmd/m-p/1074389#M6235</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello dear,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would like to understand why I have rx_align_err counter increasing in my DPDK testpmd application.&lt;/P&gt;&lt;P&gt;I have one LS1043 board running pktgen connected to a LS1046 board over the 10G copper port running testpmd. I'm using LSDK 19.09. The forwarding works good however when I print the xstats in testpmd I have the following :&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="align_err.PNG"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/116562i64437C25B16E6119/image-size/large?v=v2&amp;amp;px=999" role="button" title="align_err.PNG" alt="align_err.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;After googling this type of issue it seems that it comes from CRC errors or odd bytes number.&lt;/P&gt;&lt;P&gt;I tried different setups (also with a lx2160 board) and different cables but the issue still remains.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Tanks for your help,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Etienne Cordroc'h&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Jul 2020 07:09:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/rx-align-err-in-Testpmd/m-p/1074389#M6235</guid>
      <dc:creator>etienne_cordroc</dc:creator>
      <dc:date>2020-07-22T07:09:42Z</dc:date>
    </item>
  </channel>
</rss>