<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Layerscape中的主题 TWR-LS1021A</title>
    <link>https://community.nxp.com/t5/Layerscape/TWR-LS1021A/m-p/1069074#M6127</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;正准备使用LS1021,并参考SPF-28673_C1 Demo,有几个问题想请教下:&lt;/P&gt;&lt;P&gt;1、 LS1020的时钟，哪些是必须的，哪些是可选的？&lt;/P&gt;&lt;P&gt;2、 供电芯片MC34VR500V7ES，选择LS1020+DDR4的情况，3.3V供电和Serdes供电会因为电压域原因导致不能同时上电，是否OK？&lt;BR /&gt;3、 SPF-28673_C1评估板上在MC34VR500V7ES输出部分使用了2颗INA220AIDGST输出电流/电压/功率监控器，是必须的吗？&lt;BR /&gt;4、 SPF-28673_C1评估板上在LS1020A的MAC部分又输入了一路125M时钟，这个是必须的吗？&lt;BR /&gt;5、 Serdes有2路时钟，他们与Serdes数据lane对应关系如何？是必须都给的吗？&lt;/P&gt;&lt;P&gt;请帮忙解答下,感谢!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 06 Aug 2020 15:04:17 GMT</pubDate>
    <dc:creator>lizboxy</dc:creator>
    <dc:date>2020-08-06T15:04:17Z</dc:date>
    <item>
      <title>TWR-LS1021A</title>
      <link>https://community.nxp.com/t5/Layerscape/TWR-LS1021A/m-p/1069074#M6127</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;正准备使用LS1021,并参考SPF-28673_C1 Demo,有几个问题想请教下:&lt;/P&gt;&lt;P&gt;1、 LS1020的时钟，哪些是必须的，哪些是可选的？&lt;/P&gt;&lt;P&gt;2、 供电芯片MC34VR500V7ES，选择LS1020+DDR4的情况，3.3V供电和Serdes供电会因为电压域原因导致不能同时上电，是否OK？&lt;BR /&gt;3、 SPF-28673_C1评估板上在MC34VR500V7ES输出部分使用了2颗INA220AIDGST输出电流/电压/功率监控器，是必须的吗？&lt;BR /&gt;4、 SPF-28673_C1评估板上在LS1020A的MAC部分又输入了一路125M时钟，这个是必须的吗？&lt;BR /&gt;5、 Serdes有2路时钟，他们与Serdes数据lane对应关系如何？是必须都给的吗？&lt;/P&gt;&lt;P&gt;请帮忙解答下,感谢!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Aug 2020 15:04:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/TWR-LS1021A/m-p/1069074#M6127</guid>
      <dc:creator>lizboxy</dc:creator>
      <dc:date>2020-08-06T15:04:17Z</dc:date>
    </item>
    <item>
      <title>Re: TWR-LS1021A</title>
      <link>https://community.nxp.com/t5/Layerscape/TWR-LS1021A/m-p/1069075#M6128</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please pose the questions in English.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 07 Aug 2020 04:19:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/TWR-LS1021A/m-p/1069075#M6128</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2020-08-07T04:19:25Z</dc:date>
    </item>
    <item>
      <title>Re: TWR-LS1021A</title>
      <link>https://community.nxp.com/t5/Layerscape/TWR-LS1021A/m-p/1069076#M6129</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;Our customer is using LS1021 and check the reference design of the Demo TWR-LS1021A,&amp;nbsp;&lt;SPAN&gt;SPF-28673_C1&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;1、 For the clock of LS1020,which must be needed and which one is &lt;SPAN style="color: #333333;"&gt;Optional?&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;2、 For PMIC MC34VR5100，if as power for LS1020+DDR4,&amp;nbsp; support for both 3.3V and Serdes&amp;nbsp; is ok or not due to the 2different domain power&amp;nbsp;which can not powered at the same time?&lt;BR /&gt;3、 In the SPF-28673_C1, 2pcs INA220AIDGST used&amp;nbsp;as monitor of &lt;SPAN style="color: #333333;"&gt;Voltage and Current&lt;/SPAN&gt;&amp;nbsp;at output of MC34VR500V7ES，so INA220 must be needed？&lt;BR /&gt;4、 In the SPF-28673_C1, another 125M clock is used for MAC of LS1021A, tt's necessary？&lt;BR /&gt;5、 For the 2clock for Serders ，how about the relationship about the Serdes' LANS? I&lt;SPAN&gt;t's&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;necessary&lt;/SPAN&gt;？&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 10 Aug 2020 09:23:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/TWR-LS1021A/m-p/1069076#M6129</guid>
      <dc:creator>lizboxy</dc:creator>
      <dc:date>2020-08-10T09:23:19Z</dc:date>
    </item>
    <item>
      <title>Re: TWR-LS1021A</title>
      <link>https://community.nxp.com/t5/Layerscape/TWR-LS1021A/m-p/1069077#M6130</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;1) Please refer to the QorIQ LS1021A Reference Manual, 4.4.7 Clocking to select a clocking mode.&lt;/P&gt;&lt;P&gt;2) The question is not clear.&lt;/P&gt;&lt;P&gt;3) Usage of INA220 is not a must.&lt;/P&gt;&lt;P&gt;4) External 125 MHz reference clock (ECn_GTX_CLK125) is needed if RGMII interface is used.&lt;/P&gt;&lt;P&gt;5) Please refer to the QorIQ LS1021A Reference Manual, Table 33-2. Supported SerDes options, column "Per lane PLL mapping":&lt;/P&gt;&lt;P&gt;"1" corresponds to the PLL1&lt;/P&gt;&lt;P&gt;"2" corresponds to the PLL2&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Example:&lt;/P&gt;&lt;P&gt;SRDS_PRTCL_S1 = 0x10&lt;/P&gt;&lt;P&gt;Per lane PLL mapping: 1211&lt;/P&gt;&lt;P&gt;Lanes A, C, D - PLL1&lt;/P&gt;&lt;P&gt;Lane B - PLL2&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If PLLn is not used then it has to be powered down and corresponding reference clock is not needed.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 10 Aug 2020 09:45:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/TWR-LS1021A/m-p/1069077#M6130</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2020-08-10T09:45:09Z</dc:date>
    </item>
  </channel>
</rss>