<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LayerscapeのトピックQuestion regarding System Memory and RAM ls1021a</title>
    <link>https://community.nxp.com/t5/Layerscape/Question-regarding-System-Memory-and-RAM-ls1021a/m-p/1067484#M6115</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Please see this below:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/107354i69650108E0E2F681/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;A 32-bit CPU the system memory for it is from 0x00000000 - 0xFFFFFFFFF&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;(1)So system memory is not only RAM is that correct? if so when I/O mapped devices are accessed by the CPU the physical memory addresses (I know it will map to virtual memory first) are on the RAM or the system memory?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;(2) the RAM is made up of kernel memory and usersapce memory, when a CPU wants to access a driver and configure it let's say ethernet (for example whenever the kernel gets loaded) is this access done from system memory or in the RAM?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 24 May 2020 16:36:34 GMT</pubDate>
    <dc:creator>jiye</dc:creator>
    <dc:date>2020-05-24T16:36:34Z</dc:date>
    <item>
      <title>Question regarding System Memory and RAM ls1021a</title>
      <link>https://community.nxp.com/t5/Layerscape/Question-regarding-System-Memory-and-RAM-ls1021a/m-p/1067484#M6115</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Please see this below:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/107354i69650108E0E2F681/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;A 32-bit CPU the system memory for it is from 0x00000000 - 0xFFFFFFFFF&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;(1)So system memory is not only RAM is that correct? if so when I/O mapped devices are accessed by the CPU the physical memory addresses (I know it will map to virtual memory first) are on the RAM or the system memory?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;(2) the RAM is made up of kernel memory and usersapce memory, when a CPU wants to access a driver and configure it let's say ethernet (for example whenever the kernel gets loaded) is this access done from system memory or in the RAM?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 24 May 2020 16:36:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Question-regarding-System-Memory-and-RAM-ls1021a/m-p/1067484#M6115</guid>
      <dc:creator>jiye</dc:creator>
      <dc:date>2020-05-24T16:36:34Z</dc:date>
    </item>
    <item>
      <title>Re: Question regarding System Memory and RAM ls1021a</title>
      <link>https://community.nxp.com/t5/Layerscape/Question-regarding-System-Memory-and-RAM-ls1021a/m-p/1067485#M6116</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;1) Please refer to the QorIQ LS1021A Reference Manual, Table 2-1. System memory map.&lt;/P&gt;&lt;P&gt;2) Concerning the eTSEC Ethernet driver refer to the LSDK Documentation:&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://docs.nxp.com/bundle/GUID-51EEFEDB-ABD5-40C0-BEBD-6527B3494D57/page/GUID-3859CD3C-A399-48B1-AEBE-BD4EC0ED9CA2.html" title="https://docs.nxp.com/bundle/GUID-51EEFEDB-ABD5-40C0-BEBD-6527B3494D57/page/GUID-3859CD3C-A399-48B1-AEBE-BD4EC0ED9CA2.html"&gt;Linux Ethernet Driver for eTSEC&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 24 May 2020 17:15:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Question-regarding-System-Memory-and-RAM-ls1021a/m-p/1067485#M6116</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2020-05-24T17:15:18Z</dc:date>
    </item>
  </channel>
</rss>