<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Layerscape中的主题 VR500 PMIC SW1 Current Insufficient For LS1028A Applications</title>
    <link>https://community.nxp.com/t5/Layerscape/VR500-PMIC-SW1-Current-Insufficient-For-LS1028A-Applications/m-p/1044062#M5876</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am in the process of implementing the power scheme to our custom LS1028A application. I saw from the LS1028A Reference Design Board that NXP utilizes and recommends the VR500 PMIC, specifically the&amp;nbsp;MC34VR500V9ES, for the LS1028A application.&amp;nbsp;In the VR500 datasheet, the SW1 output is described to supply the LS1028A's VDD core (1.0V/0.9V) with a max current of 4.5 Amps.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;According to the LS1028A Design Checklist "Table 7. Typical use case power at 65 C", every LS1028A configuration exceeds the current available from the VR500 SW1 output.&amp;nbsp;I find it unusual that the PMIC recommended for this processor is not capable of providing sufficient VDD&amp;nbsp;current under load.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is this the right PMIC for the LS1028A, or is there another PMIC available that is capable of providing sufficient power without having to use another separate switching power supply?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 01 Jun 2020 22:22:16 GMT</pubDate>
    <dc:creator>jimmymm</dc:creator>
    <dc:date>2020-06-01T22:22:16Z</dc:date>
    <item>
      <title>VR500 PMIC SW1 Current Insufficient For LS1028A Applications</title>
      <link>https://community.nxp.com/t5/Layerscape/VR500-PMIC-SW1-Current-Insufficient-For-LS1028A-Applications/m-p/1044062#M5876</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am in the process of implementing the power scheme to our custom LS1028A application. I saw from the LS1028A Reference Design Board that NXP utilizes and recommends the VR500 PMIC, specifically the&amp;nbsp;MC34VR500V9ES, for the LS1028A application.&amp;nbsp;In the VR500 datasheet, the SW1 output is described to supply the LS1028A's VDD core (1.0V/0.9V) with a max current of 4.5 Amps.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;According to the LS1028A Design Checklist "Table 7. Typical use case power at 65 C", every LS1028A configuration exceeds the current available from the VR500 SW1 output.&amp;nbsp;I find it unusual that the PMIC recommended for this processor is not capable of providing sufficient VDD&amp;nbsp;current under load.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is this the right PMIC for the LS1028A, or is there another PMIC available that is capable of providing sufficient power without having to use another separate switching power supply?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 01 Jun 2020 22:22:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/VR500-PMIC-SW1-Current-Insufficient-For-LS1028A-Applications/m-p/1044062#M5876</guid>
      <dc:creator>jimmymm</dc:creator>
      <dc:date>2020-06-01T22:22:16Z</dc:date>
    </item>
    <item>
      <title>Re: VR500 PMIC SW1 Current Insufficient For LS1028A Applications</title>
      <link>https://community.nxp.com/t5/Layerscape/VR500-PMIC-SW1-Current-Insufficient-For-LS1028A-Applications/m-p/1044063#M5877</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It is reasonable to refer to the QorIQ LS1028A Reference Design Board Reference Manual,&amp;nbsp;2.2 Power supplies where it is shown that &lt;STRONG&gt;VDD is provided by LTC7151S&lt;/STRONG&gt;:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/108829i48C4D7A398C3EF98/image-size/large?v=v2&amp;amp;px=999" title="UM.jpg" alt="UM.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;and the RDB schematics:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/108830i2410F27141B41BD1/image-size/large?v=v2&amp;amp;px=999" title="SCH.jpg" alt="SCH.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 02 Jun 2020 04:57:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/VR500-PMIC-SW1-Current-Insufficient-For-LS1028A-Applications/m-p/1044063#M5877</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2020-06-02T04:57:36Z</dc:date>
    </item>
  </channel>
</rss>