<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LayerscapeのトピックRe: LS1021a CPLD Reset</title>
    <link>https://community.nxp.com/t5/Layerscape/LS1021a-CPLD-Reset/m-p/1036833#M5807</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;(2) Can you explain a little bit more about the CKE? I do have an active high CKE enable pin from my atmega328 which use to drive the D1_MCKE0 pin low on the LS1021A, if I do have this pin my question is do I need to follow a certain logic for the reset. For example do I need to wait for assertion event of PORESET_B to trigger the DDR reset. what is the DDR control signal assertion logic suppose to be ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 26 Nov 2019 13:31:48 GMT</pubDate>
    <dc:creator>jiye</dc:creator>
    <dc:date>2019-11-26T13:31:48Z</dc:date>
    <item>
      <title>LS1021a CPLD Reset</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1021a-CPLD-Reset/m-p/1036831#M5805</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can anyone explain this below:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/94115i9DEF25F503FD42CA/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;(1)Does this mean that every time when there is a hreset_b_18 event let's say 1, then all variable relates to this signal will get reset to 1 as well? such as pcie interface or DDR?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;(2) If my standalone ls1021a board does not have hreset_b_18 signal anymore how am I able to reset such as pcie or DDR?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 25 Nov 2019 22:43:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1021a-CPLD-Reset/m-p/1036831#M5805</guid>
      <dc:creator>jiye</dc:creator>
      <dc:date>2019-11-25T22:43:33Z</dc:date>
    </item>
    <item>
      <title>Re: LS1021a CPLD Reset</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1021a-CPLD-Reset/m-p/1036832#M5806</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;1) Yes, the HRESET_B timing makes it convenient to use&amp;nbsp;this signal as reset for DDR SDRAM and PCIe.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2) Mostly HRESET_B is used because of DDR SDRAM - refer to the&amp;nbsp;AN5097 - Hardware and Layout Design Considerations for DDR4 SDRAM,&amp;nbsp;Appendix B DRAM reset signal considerations. If CKE is not used in the design it is possible to use PORESET_B as global reset.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Nov 2019 04:44:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1021a-CPLD-Reset/m-p/1036832#M5806</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2019-11-26T04:44:33Z</dc:date>
    </item>
    <item>
      <title>Re: LS1021a CPLD Reset</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1021a-CPLD-Reset/m-p/1036833#M5807</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;(2) Can you explain a little bit more about the CKE? I do have an active high CKE enable pin from my atmega328 which use to drive the D1_MCKE0 pin low on the LS1021A, if I do have this pin my question is do I need to follow a certain logic for the reset. For example do I need to wait for assertion event of PORESET_B to trigger the DDR reset. what is the DDR control signal assertion logic suppose to be ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Nov 2019 13:31:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1021a-CPLD-Reset/m-p/1036833#M5807</guid>
      <dc:creator>jiye</dc:creator>
      <dc:date>2019-11-26T13:31:48Z</dc:date>
    </item>
    <item>
      <title>Re: LS1021a CPLD Reset</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1021a-CPLD-Reset/m-p/1036834#M5808</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please refer to the&amp;nbsp;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;AN5097.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Nov 2019 14:26:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1021a-CPLD-Reset/m-p/1036834#M5808</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2019-11-26T14:26:17Z</dc:date>
    </item>
  </channel>
</rss>