<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: ls1046a using emmc as boot source in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/ls1046a-using-emmc-as-boot-source/m-p/1033295#M5760</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please provide the processor connection schematics as searchable PDF for inspection.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 15 Feb 2020 10:42:59 GMT</pubDate>
    <dc:creator>ufedor</dc:creator>
    <dc:date>2020-02-15T10:42:59Z</dc:date>
    <item>
      <title>ls1046a using emmc as boot source</title>
      <link>https://community.nxp.com/t5/Layerscape/ls1046a-using-emmc-as-boot-source/m-p/1033294#M5759</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi&lt;/P&gt;&lt;P&gt;In&amp;nbsp; my coustom board,I use emmc/sd as boot source.but i don't use&amp;nbsp;SDHC_CD_B pin.it always floating.my board is refer to ls1046ardb board.&lt;/P&gt;&lt;P&gt;Now&amp;nbsp;I can boot from sd card ,but i can't boot from emmc.&lt;/P&gt;&lt;P&gt;why I can boot from sd? the SDHC_CD_B pin is&amp;nbsp;&lt;SPAN&gt;floating&amp;nbsp; And Why I can't boot from emmc,Is it because PBL has special regulations for this pin?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;in spec,when use sdhc as boot source, SDHC_CD_B pin be&amp;nbsp;serve as the SDHC_CD_B pin for the eSDHC controller. This happens automatically when the microSD card is selected as the boot source for the board.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 15 Feb 2020 08:04:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/ls1046a-using-emmc-as-boot-source/m-p/1033294#M5759</guid>
      <dc:creator>shijj</dc:creator>
      <dc:date>2020-02-15T08:04:45Z</dc:date>
    </item>
    <item>
      <title>Re: ls1046a using emmc as boot source</title>
      <link>https://community.nxp.com/t5/Layerscape/ls1046a-using-emmc-as-boot-source/m-p/1033295#M5760</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please provide the processor connection schematics as searchable PDF for inspection.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 15 Feb 2020 10:42:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/ls1046a-using-emmc-as-boot-source/m-p/1033295#M5760</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2020-02-15T10:42:59Z</dc:date>
    </item>
  </channel>
</rss>