<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LayerscapeのトピックeSDHC of LS1021a eMMC</title>
    <link>https://community.nxp.com/t5/Layerscape/eSDHC-of-LS1021a-eMMC/m-p/1031981#M5721</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;if my only boot source of&amp;nbsp; ls1021a stand alone chip is eMMC do I need to specify the boot mode in the RCW source file again?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/94692iEE20328B3150DA2F/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Also from the ls1021ARM reference manual&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Section 4.4.1&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;The device samples the RCW source POR configuration inputs (cfg_rcw_src[0:n])&lt;BR /&gt;on deassertion of PORESET_B to determine the RCW source. Note that the POR&lt;BR /&gt;configuration inputs are sampled only on a PORESET_B.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How can I sample POR configuration inputs on my standalone application is this done automatically after deassertion of PORESET_B?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 24 Nov 2019 17:44:49 GMT</pubDate>
    <dc:creator>jiye</dc:creator>
    <dc:date>2019-11-24T17:44:49Z</dc:date>
    <item>
      <title>eSDHC of LS1021a eMMC</title>
      <link>https://community.nxp.com/t5/Layerscape/eSDHC-of-LS1021a-eMMC/m-p/1031981#M5721</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;if my only boot source of&amp;nbsp; ls1021a stand alone chip is eMMC do I need to specify the boot mode in the RCW source file again?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/94692iEE20328B3150DA2F/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Also from the ls1021ARM reference manual&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Section 4.4.1&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;The device samples the RCW source POR configuration inputs (cfg_rcw_src[0:n])&lt;BR /&gt;on deassertion of PORESET_B to determine the RCW source. Note that the POR&lt;BR /&gt;configuration inputs are sampled only on a PORESET_B.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How can I sample POR configuration inputs on my standalone application is this done automatically after deassertion of PORESET_B?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 24 Nov 2019 17:44:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/eSDHC-of-LS1021a-eMMC/m-p/1031981#M5721</guid>
      <dc:creator>jiye</dc:creator>
      <dc:date>2019-11-24T17:44:49Z</dc:date>
    </item>
    <item>
      <title>Re: eSDHC of LS1021a eMMC</title>
      <link>https://community.nxp.com/t5/Layerscape/eSDHC-of-LS1021a-eMMC/m-p/1031982#M5722</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;The &lt;/SPAN&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;cfg_rcw_src&lt;/SPAN&gt;&lt;SPAN style="font-size: 10.0pt;"&gt; signals are used for RCW source. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; color: black;"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; color: black;"&gt;The LS1021a SDHC is RCW source fir 0_0100_0000 setting of the &lt;/SPAN&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;cfg_rcw_src. See the Table 4-9 of the LS1021a Reference Manual.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;The LS1021a RCW provides configuration for SDHC pin assigning of the LS1021a.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;See the SDHC_BASE and SDHC_EXT fields in the LS1021a RCW.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;The &lt;/SPAN&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;PBI_SRC&lt;/SPAN&gt;&lt;SPAN style="font-size: 10.0pt;"&gt; RCW bits are used for setting SD/MMC as PBL initialization source.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Pavel Chubakov&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 25 Nov 2019 05:24:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/eSDHC-of-LS1021a-eMMC/m-p/1031982#M5722</guid>
      <dc:creator>Pavel</dc:creator>
      <dc:date>2019-11-25T05:24:27Z</dc:date>
    </item>
  </channel>
</rss>