<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Layerscape中的主题 Re: Can max payload size in Device_Capabilities_Register be re-set?</title>
    <link>https://community.nxp.com/t5/Layerscape/Can-max-payload-size-in-Device-Capabilities-Register-be-re-set/m-p/1031115#M5716</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt;"&gt;It is impossible set to other value larger than 256bytes in the LS1046 PCI Express Device Capabilities Register. &lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 14 Mar 2020 06:26:47 GMT</pubDate>
    <dc:creator>r8070z</dc:creator>
    <dc:date>2020-03-14T06:26:47Z</dc:date>
    <item>
      <title>Can max payload size in Device_Capabilities_Register be re-set?</title>
      <link>https://community.nxp.com/t5/Layerscape/Can-max-payload-size-in-Device-Capabilities-Register-be-re-set/m-p/1031114#M5715</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi folks,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In PCIE specification, the max payload size can be one of these:&lt;/P&gt;&lt;TABLE border="0" cellpadding="0" cellspacing="0" width="100%"&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD valign="top"&gt;&lt;TABLE border="1" cellpadding="4" cellspacing="0" rules="all" width="100%"&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD class="" valign="top"&gt;&lt;UL&gt;&lt;LI&gt;&lt;P class=""&gt;000b = 128 bytes max payload size&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P class=""&gt;001b = 256 bytes max payload size&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P class=""&gt;010b = 512 bytes max payload size&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P class=""&gt;011b = 1KB max payload size&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P class=""&gt;100b = 2KB max payload size&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P class=""&gt;101b = 4KB max payload size&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P class=""&gt;110b = Reserved&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P class=""&gt;111b = Reserved&lt;/P&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;P&gt;The max payload size field in LS1046A is 001, which is 256bytes.&lt;/P&gt;&lt;P&gt;In my scenario, two LS1046A boards are across connected for data transfer.&amp;nbsp; One LS1046A acts as RC, the other acts as EP. In order to improve the throughput, can the field be set to other value larger than 256bytes, take example, 101b for 4K bytes?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 14 Mar 2020 03:26:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Can-max-payload-size-in-Device-Capabilities-Register-be-re-set/m-p/1031114#M5715</guid>
      <dc:creator>zy_mooncity</dc:creator>
      <dc:date>2020-03-14T03:26:37Z</dc:date>
    </item>
    <item>
      <title>Re: Can max payload size in Device_Capabilities_Register be re-set?</title>
      <link>https://community.nxp.com/t5/Layerscape/Can-max-payload-size-in-Device-Capabilities-Register-be-re-set/m-p/1031115#M5716</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt;"&gt;It is impossible set to other value larger than 256bytes in the LS1046 PCI Express Device Capabilities Register. &lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 14 Mar 2020 06:26:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Can-max-payload-size-in-Device-Capabilities-Register-be-re-set/m-p/1031115#M5716</guid>
      <dc:creator>r8070z</dc:creator>
      <dc:date>2020-03-14T06:26:47Z</dc:date>
    </item>
    <item>
      <title>Re: Can max payload size in Device_Capabilities_Register be re-set?</title>
      <link>https://community.nxp.com/t5/Layerscape/Can-max-payload-size-in-Device-Capabilities-Register-be-re-set/m-p/1031116#M5717</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for the answer.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I just assume some read-only fields can be modified temporarily by operating DBI Read-only Write Enable Register.&lt;/P&gt;&lt;P&gt;So it's a design restriction for LS1046A PCI controller, and only 256Bytes capability is provided, right?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 Mar 2020 02:51:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Can-max-payload-size-in-Device-Capabilities-Register-be-re-set/m-p/1031116#M5717</guid>
      <dc:creator>zy_mooncity</dc:creator>
      <dc:date>2020-03-18T02:51:21Z</dc:date>
    </item>
    <item>
      <title>Re: Can max payload size in Device_Capabilities_Register be re-set?</title>
      <link>https://community.nxp.com/t5/Layerscape/Can-max-payload-size-in-Device-Capabilities-Register-be-re-set/m-p/1031117#M5718</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, it is right.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 Mar 2020 10:53:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Can-max-payload-size-in-Device-Capabilities-Register-be-re-set/m-p/1031117#M5718</guid>
      <dc:creator>r8070z</dc:creator>
      <dc:date>2020-03-18T10:53:28Z</dc:date>
    </item>
  </channel>
</rss>