<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: TWR-LS1021A USB STANDALONE MODE in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/TWR-LS1021A-USB-STANDALONE-MODE/m-p/359333#M56</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;USB 3.0 controller is connected to USB 3.0 hub on the TWR board, because of this reason the only host mode is available on this board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;USB 2.0 controller is available via elevator board and can be used in both modes.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 20 Jan 2015 14:41:10 GMT</pubDate>
    <dc:creator>alexander_yakov</dc:creator>
    <dc:date>2015-01-20T14:41:10Z</dc:date>
    <item>
      <title>TWR-LS1021A USB STANDALONE MODE</title>
      <link>https://community.nxp.com/t5/Layerscape/TWR-LS1021A-USB-STANDALONE-MODE/m-p/359332#M55</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I heard that LS1021A has usb controller can be configured as host or device.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But default setting of TWR-1021A is not device mode, I think.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How can I operate it as a stand-alone USB device?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 Jan 2015 09:00:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/TWR-LS1021A-USB-STANDALONE-MODE/m-p/359332#M55</guid>
      <dc:creator>JHY</dc:creator>
      <dc:date>2015-01-20T09:00:24Z</dc:date>
    </item>
    <item>
      <title>Re: TWR-LS1021A USB STANDALONE MODE</title>
      <link>https://community.nxp.com/t5/Layerscape/TWR-LS1021A-USB-STANDALONE-MODE/m-p/359333#M56</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;USB 3.0 controller is connected to USB 3.0 hub on the TWR board, because of this reason the only host mode is available on this board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;USB 2.0 controller is available via elevator board and can be used in both modes.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 Jan 2015 14:41:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/TWR-LS1021A-USB-STANDALONE-MODE/m-p/359333#M56</guid>
      <dc:creator>alexander_yakov</dc:creator>
      <dc:date>2015-01-20T14:41:10Z</dc:date>
    </item>
  </channel>
</rss>