<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LayerscapeのトピックLS1046A IFC speed</title>
    <link>https://community.nxp.com/t5/Layerscape/LS1046A-IFC-speed/m-p/1020245#M5497</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I have a very dumb question: We are designing a new board (core speed 1.8GHz) and need to connect the SoC to an FPGA via PCIe as well as via IFC (IFC for latency reasons for certain data transfers). As&amp;nbsp;I understand it with the fastest possible platform clock frequency (700MHz) the fastest possible IFC clock speed is 87.5MHz (IFC_CCR divider = 4). If I choose the max. possible IFC frequency of 100MHz the max. possible platform clock frequency would be 400MHz only &lt;SPAN&gt;(IFC_CCR divider = 2)&lt;/SPAN&gt;. Can this really be true?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 26 Mar 2020 08:10:35 GMT</pubDate>
    <dc:creator>Quitsch</dc:creator>
    <dc:date>2020-03-26T08:10:35Z</dc:date>
    <item>
      <title>LS1046A IFC speed</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1046A-IFC-speed/m-p/1020245#M5497</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I have a very dumb question: We are designing a new board (core speed 1.8GHz) and need to connect the SoC to an FPGA via PCIe as well as via IFC (IFC for latency reasons for certain data transfers). As&amp;nbsp;I understand it with the fastest possible platform clock frequency (700MHz) the fastest possible IFC clock speed is 87.5MHz (IFC_CCR divider = 4). If I choose the max. possible IFC frequency of 100MHz the max. possible platform clock frequency would be 400MHz only &lt;SPAN&gt;(IFC_CCR divider = 2)&lt;/SPAN&gt;. Can this really be true?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 Mar 2020 08:10:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1046A-IFC-speed/m-p/1020245#M5497</guid>
      <dc:creator>Quitsch</dc:creator>
      <dc:date>2020-03-26T08:10:35Z</dc:date>
    </item>
    <item>
      <title>Re: LS1046A IFC speed</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1046A-IFC-speed/m-p/1020246#M5498</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN class=""&gt;&amp;nbsp;Yes, your calculations are correct.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Regards,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Bulat&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 31 Mar 2020 12:04:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1046A-IFC-speed/m-p/1020246#M5498</guid>
      <dc:creator>Bulat</dc:creator>
      <dc:date>2020-03-31T12:04:00Z</dc:date>
    </item>
  </channel>
</rss>