<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LayerscapeのトピックLS1021A Device mode (g_ether)</title>
    <link>https://community.nxp.com/t5/Layerscape/LS1021A-Device-mode-g-ether/m-p/1014729#M5459</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a stand alone ls1021a device and my schematic is like this below:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/97674i0BE165980A36733D/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My PC can't detect my ls1021a device over USB3.0 I want to configure it as OTG g_ether device.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I want to ask couple things here:&lt;/P&gt;&lt;P&gt;(1) for device mode is the USB1_ID should be floating or pull up&lt;/P&gt;&lt;P&gt;(2) do I need to add pull down resistors at USB1_D_M and USB1_D_P&lt;/P&gt;&lt;P&gt;(3) what else do I have to fulfill?&lt;/P&gt;&lt;P&gt;(4)&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/97763i974B769BD7E84B56/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is USB g_ether OTG is a A device or B device in the picture above?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 11 Feb 2020 22:49:13 GMT</pubDate>
    <dc:creator>jiye</dc:creator>
    <dc:date>2020-02-11T22:49:13Z</dc:date>
    <item>
      <title>LS1021A Device mode (g_ether)</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1021A-Device-mode-g-ether/m-p/1014729#M5459</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a stand alone ls1021a device and my schematic is like this below:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/97674i0BE165980A36733D/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My PC can't detect my ls1021a device over USB3.0 I want to configure it as OTG g_ether device.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I want to ask couple things here:&lt;/P&gt;&lt;P&gt;(1) for device mode is the USB1_ID should be floating or pull up&lt;/P&gt;&lt;P&gt;(2) do I need to add pull down resistors at USB1_D_M and USB1_D_P&lt;/P&gt;&lt;P&gt;(3) what else do I have to fulfill?&lt;/P&gt;&lt;P&gt;(4)&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/97763i974B769BD7E84B56/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is USB g_ether OTG is a A device or B device in the picture above?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Feb 2020 22:49:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1021A-Device-mode-g-ether/m-p/1014729#M5459</guid>
      <dc:creator>jiye</dc:creator>
      <dc:date>2020-02-11T22:49:13Z</dc:date>
    </item>
    <item>
      <title>Re: LS1021A Device mode (g_ether)</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1021A-Device-mode-g-ether/m-p/1014730#M5460</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; color: black;"&gt;(1) USB1_ID should be floating for device mode. See the following Application Note:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;A href="https://www.maximintegrated.com/en/design/technical-documents/tutorials/1/1822.html"&gt;https://www.maximintegrated.com/en/design/technical-documents/tutorials/1/1822.html&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;(2) External resistors are not needed for the LS1021a USB1. &lt;/SPAN&gt;&lt;SPAN style="font-size: 10.0pt; color: black;"&gt;&amp;nbsp;The LS1021a USB1 includes USB PHY. This PHY uses internal resistors.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; color: black;"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; color: black;"&gt;(3) Use as example for USB using the TWR-LS1021a board schematic:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; color: black;"&gt;&lt;A href="https://www.nxp.com/webapp/Download?colCode=TWR-LS1021A-PB-DF&amp;amp;location=null"&gt;https://www.nxp.com/webapp/Download?colCode=TWR-LS1021A-PB-DF&amp;amp;location=null&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Pavel Chubakov&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Feb 2020 04:35:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1021A-Device-mode-g-ether/m-p/1014730#M5460</guid>
      <dc:creator>Pavel</dc:creator>
      <dc:date>2020-02-12T04:35:27Z</dc:date>
    </item>
  </channel>
</rss>