<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LayerscapeのトピックRe: LS1021a Standalone CPU Temperature Overheated</title>
    <link>https://community.nxp.com/t5/Layerscape/LS1021a-Standalone-CPU-Temperature-Overheated/m-p/994514#M5177</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You wrote:&lt;/P&gt;&lt;P&gt;&amp;gt; body of the whole board gets extremely hot&lt;/P&gt;&lt;P&gt;Which exactly components are hot?&lt;/P&gt;&lt;P&gt;Is the LS1021A operational?&lt;/P&gt;&lt;P&gt;Have you measured the LS1021A supply voltages? - What are they?&lt;/P&gt;&lt;P&gt;Which heatsink is used for the LS1021A? - Have performed thermal behaviour modelling for it?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2) You wrote:&lt;/P&gt;&lt;P&gt;&amp;gt; I am using the same image as the EVA does&lt;/P&gt;&lt;P&gt;What do you mean?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 07 Mar 2020 03:24:42 GMT</pubDate>
    <dc:creator>ufedor</dc:creator>
    <dc:date>2020-03-07T03:24:42Z</dc:date>
    <item>
      <title>LS1021a Standalone CPU Temperature Overheated</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1021a-Standalone-CPU-Temperature-Overheated/m-p/994509#M5172</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a standalone ls1021 board and when I apply the power into the board, from the USB port the USB port isn't getting hot but the body of the whole board gets extremely hot&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After 20 mins the boards get&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/54995i0D8A8C763ECD195B/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does any one know how to trouble shoot the temperature like check RCW lanes, shutdown all unused lanes or peripherals of the CPU, recompiling the kernel etc,,,,,,,,,,,,,,,?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using lsdk1906 and kernel 4.19 Ubuntu&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 05 Mar 2020 14:36:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1021a-Standalone-CPU-Temperature-Overheated/m-p/994509#M5172</guid>
      <dc:creator>jiye</dc:creator>
      <dc:date>2020-03-05T14:36:17Z</dc:date>
    </item>
    <item>
      <title>Re: LS1021a Standalone CPU Temperature Overheated</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1021a-Standalone-CPU-Temperature-Overheated/m-p/994510#M5173</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;How to interpret provided screenshot?&lt;/P&gt;&lt;P&gt;What is the temperature measurement point?&lt;/P&gt;&lt;P&gt;Was the temperature measurement circuit properly calibrated?&lt;/P&gt;&lt;P&gt;What does it mean "LS1021a Standalone" - which heatsink is attached to the processor?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 06 Mar 2020 03:08:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1021a-Standalone-CPU-Temperature-Overheated/m-p/994510#M5173</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2020-03-06T03:08:43Z</dc:date>
    </item>
    <item>
      <title>Re: LS1021a Standalone CPU Temperature Overheated</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1021a-Standalone-CPU-Temperature-Overheated/m-p/994511#M5174</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;(1) I just installed&amp;nbsp; lm-sensors into my board and perform command sensors it tells me the temperature whatever shows in the screen shot I provided&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;(2) I dont know where is the measurement point depends on the userspace ? as I performed that command from the userspace I really have no clue what it's based on.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;(3) I attached the heatsink to the processor and the whole board "standalone" (contains ls1021a, eMMC, PCIe, USB3.0, DDR3L,PMIC .etc) still really hot. But the power port which I powered on the board from USB3.0 male connector it's not hot at all.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;(4) What do you mean by circuit properly calibrated? do you know what I need to do to achieve this ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 06 Mar 2020 13:52:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1021a-Standalone-CPU-Temperature-Overheated/m-p/994511#M5174</guid>
      <dc:creator>jiye</dc:creator>
      <dc:date>2020-03-06T13:52:10Z</dc:date>
    </item>
    <item>
      <title>Re: LS1021a Standalone CPU Temperature Overheated</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1021a-Standalone-CPU-Temperature-Overheated/m-p/994512#M5175</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It is still not clear what exactly you are measuring and how this measurement is connected to the NXP product.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 06 Mar 2020 18:11:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1021a-Standalone-CPU-Temperature-Overheated/m-p/994512#M5175</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2020-03-06T18:11:21Z</dc:date>
    </item>
    <item>
      <title>Re: LS1021a Standalone CPU Temperature Overheated</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1021a-Standalone-CPU-Temperature-Overheated/m-p/994513#M5176</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;(1) Now I put a temperature probe insert into the heat sink which tells me 95 degree, is that more clear to you? what kind standard of measurements did you suggest? &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;(2)You still did not answer this question "temperature measurement circuit properly calibrated?", what do you mean by calibrated? I am using the same image as the EVA does, why do I need to calibrate?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 06 Mar 2020 19:36:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1021a-Standalone-CPU-Temperature-Overheated/m-p/994513#M5176</guid>
      <dc:creator>jiye</dc:creator>
      <dc:date>2020-03-06T19:36:07Z</dc:date>
    </item>
    <item>
      <title>Re: LS1021a Standalone CPU Temperature Overheated</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1021a-Standalone-CPU-Temperature-Overheated/m-p/994514#M5177</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You wrote:&lt;/P&gt;&lt;P&gt;&amp;gt; body of the whole board gets extremely hot&lt;/P&gt;&lt;P&gt;Which exactly components are hot?&lt;/P&gt;&lt;P&gt;Is the LS1021A operational?&lt;/P&gt;&lt;P&gt;Have you measured the LS1021A supply voltages? - What are they?&lt;/P&gt;&lt;P&gt;Which heatsink is used for the LS1021A? - Have performed thermal behaviour modelling for it?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2) You wrote:&lt;/P&gt;&lt;P&gt;&amp;gt; I am using the same image as the EVA does&lt;/P&gt;&lt;P&gt;What do you mean?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 07 Mar 2020 03:24:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1021a-Standalone-CPU-Temperature-Overheated/m-p/994514#M5177</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2020-03-07T03:24:42Z</dc:date>
    </item>
  </channel>
</rss>