<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Port pin status during RESET in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/Port-pin-status-during-RESET/m-p/984929#M5021</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;What is the port pin status of ball E13&amp;nbsp;"IFC_PAR1/GPIO2_14/QSPI_DIO_B1/FTM6_CH1", while LS1021A is set into RESET state?&lt;/P&gt;&lt;P&gt;Datasheet (Rev. 7, 06/2019) doesn't&amp;nbsp;provide any notes for this pin. Is there any internal weak pull resistor applied or is the pin in high-z mode?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 13 Nov 2019 07:44:10 GMT</pubDate>
    <dc:creator>FK</dc:creator>
    <dc:date>2019-11-13T07:44:10Z</dc:date>
    <item>
      <title>Port pin status during RESET</title>
      <link>https://community.nxp.com/t5/Layerscape/Port-pin-status-during-RESET/m-p/984929#M5021</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;What is the port pin status of ball E13&amp;nbsp;"IFC_PAR1/GPIO2_14/QSPI_DIO_B1/FTM6_CH1", while LS1021A is set into RESET state?&lt;/P&gt;&lt;P&gt;Datasheet (Rev. 7, 06/2019) doesn't&amp;nbsp;provide any notes for this pin. Is there any internal weak pull resistor applied or is the pin in high-z mode?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 Nov 2019 07:44:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Port-pin-status-during-RESET/m-p/984929#M5021</guid>
      <dc:creator>FK</dc:creator>
      <dc:date>2019-11-13T07:44:10Z</dc:date>
    </item>
    <item>
      <title>Re: Port pin status during RESET</title>
      <link>https://community.nxp.com/t5/Layerscape/Port-pin-status-during-RESET/m-p/984930#M5022</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The pin is tri-stated&amp;nbsp;when PORESET_B is asserted.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 Nov 2019 17:51:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Port-pin-status-during-RESET/m-p/984930#M5022</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2019-11-13T17:51:43Z</dc:date>
    </item>
  </channel>
</rss>