<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LayerscapeのトピックRe: Cannot use SRKH blowing command to secureboot.</title>
    <link>https://community.nxp.com/t5/Layerscape/Cannot-use-SRKH-blowing-command-to-secureboot/m-p/959803#M4771</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;Two remarks to this:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. The most recent LSDK does support LS1046A-FRWY. This package is &lt;BR /&gt;&amp;nbsp;&amp;nbsp; newer than the one you are working with, consider moving to the LSDK.&lt;BR /&gt;&amp;nbsp;&amp;nbsp; LSDK Fuse provisioning feature is described&lt;A href="https://nxp.sdlproducts.com/LiveContent/content/en-US/LSDKUG_Rev19.06/GUID-CD4E74FF-1D8D-4B01-8A47-277117292E21"&gt; here&lt;/A&gt;.&lt;BR /&gt;&amp;nbsp; &amp;nbsp;&lt;BR /&gt;2. You can use either Code Warrior or Fuse provisioning firmware, both&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; are legal ways to blow fuses, but the firmware does not display any prompt.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; It blows fuses as specified in the Fuse file which is generated by CST and&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; must be available at the firmware build time. Refer to the documentation&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; at the link above.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Hope this helps,&lt;/P&gt;&lt;P&gt;Platon&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 04 Sep 2019 16:09:09 GMT</pubDate>
    <dc:creator>bpe</dc:creator>
    <dc:date>2019-09-04T16:09:09Z</dc:date>
    <item>
      <title>Cannot use SRKH blowing command to secureboot.</title>
      <link>https://community.nxp.com/t5/Layerscape/Cannot-use-SRKH-blowing-command-to-secureboot/m-p/959801#M4769</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm trying secure boot in develop mode on LS1046A-FRWY with its manual FRWY-LS1046ABSPUG v0.1, but it fails.&lt;BR /&gt;I used following steps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. Edit build_lsdk.cfg&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;51c51&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;lt; CONFIG_APP_OPTEE=n&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;---&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;gt; CONFIG_APP_OPTEE=y&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;58c58&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;lt; CONFIG_FUSE_PROVISIONING=n&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;---&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;gt; CONFIG_FUSE_PROVISIONING=y&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2. build image&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;$ source setenv&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;$ flex-builder -m ls1046afrwy -a arm64 -b -s&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;3. deploy the image to SD card&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;$ source setenv&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;$ flex-installer -f firmware_ls1046afrwy_uboot_sdboot.img -d /dev/sde&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;4. blow OTPMK(described in 3.3.3.1 in&amp;nbsp; FRWY-LS1046ABSPUG v0.1)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;5. Boot the image&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;- Change switch setting to SD boot&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;- Insert SD to the board&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;- boot the board&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;At this point, I have expected a prompt for SRK blowing as described in 3.3.3.2, but nothing is displayed.&lt;BR /&gt;Please give me some advice.&lt;BR /&gt;thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 Aug 2019 11:10:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Cannot-use-SRKH-blowing-command-to-secureboot/m-p/959801#M4769</guid>
      <dc:creator>pomepome11</dc:creator>
      <dc:date>2019-08-22T11:10:02Z</dc:date>
    </item>
    <item>
      <title>Re: Cannot use SRKH blowing command to secureboot.</title>
      <link>https://community.nxp.com/t5/Layerscape/Cannot-use-SRKH-blowing-command-to-secureboot/m-p/959802#M4770</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I realized I should use code warrior.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 26 Aug 2019 09:26:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Cannot-use-SRKH-blowing-command-to-secureboot/m-p/959802#M4770</guid>
      <dc:creator>pomepome11</dc:creator>
      <dc:date>2019-08-26T09:26:51Z</dc:date>
    </item>
    <item>
      <title>Re: Cannot use SRKH blowing command to secureboot.</title>
      <link>https://community.nxp.com/t5/Layerscape/Cannot-use-SRKH-blowing-command-to-secureboot/m-p/959803#M4771</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;Two remarks to this:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. The most recent LSDK does support LS1046A-FRWY. This package is &lt;BR /&gt;&amp;nbsp;&amp;nbsp; newer than the one you are working with, consider moving to the LSDK.&lt;BR /&gt;&amp;nbsp;&amp;nbsp; LSDK Fuse provisioning feature is described&lt;A href="https://nxp.sdlproducts.com/LiveContent/content/en-US/LSDKUG_Rev19.06/GUID-CD4E74FF-1D8D-4B01-8A47-277117292E21"&gt; here&lt;/A&gt;.&lt;BR /&gt;&amp;nbsp; &amp;nbsp;&lt;BR /&gt;2. You can use either Code Warrior or Fuse provisioning firmware, both&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; are legal ways to blow fuses, but the firmware does not display any prompt.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; It blows fuses as specified in the Fuse file which is generated by CST and&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; must be available at the firmware build time. Refer to the documentation&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; at the link above.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Hope this helps,&lt;/P&gt;&lt;P&gt;Platon&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 Sep 2019 16:09:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Cannot-use-SRKH-blowing-command-to-secureboot/m-p/959803#M4771</guid>
      <dc:creator>bpe</dc:creator>
      <dc:date>2019-09-04T16:09:09Z</dc:date>
    </item>
    <item>
      <title>Re: Cannot use SRKH blowing command to secureboot.</title>
      <link>https://community.nxp.com/t5/Layerscape/Cannot-use-SRKH-blowing-command-to-secureboot/m-p/959804#M4772</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for reply.&lt;/P&gt;&lt;P&gt;From my understanding, POVDD should be enabled before blowing fuses.&lt;BR /&gt;On LS1046A-RDB, this is done by jumper setting before board booting.&lt;BR /&gt;But on FRWY, POVDD is enabled by uboot and is not enabled at the point of starting firmware so fuse cannot be blown.&lt;/P&gt;&lt;P&gt;Can provisioning firmware really be used on FRWY board ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Sep 2019 03:48:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Cannot-use-SRKH-blowing-command-to-secureboot/m-p/959804#M4772</guid>
      <dc:creator>pomepome11</dc:creator>
      <dc:date>2019-09-09T03:48:14Z</dc:date>
    </item>
  </channel>
</rss>