<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LS2088A can't find device file using ls-main command in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/LS2088A-can-t-find-device-file-using-ls-main-command/m-p/929283#M4460</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN class=""&gt;Please make sure MC, DPL and DPC firmware images are deployed at the following offset addresses on Flash. Please refer to the attached u-boot log, please make sure fsl-mc is set up successfully.&lt;BR /&gt;DPAA2 MC 0x00A00000&lt;BR /&gt;DPAA2 DPL 0x00D00000&lt;BR /&gt;DPAA2 DPC 0x00E00000&lt;BR /&gt;You could get these firmware images with the following method.&lt;BR /&gt;Please execute the following command and get MC firmware image in build/firmware/qoriq-mc-binary/ls2088a/mc_10.10.0_ls2088a_20180814.itb.&lt;BR /&gt;$ flex-builder -c qoriq-mc-binary -m ls2088ardb&lt;BR /&gt;You could execute the following command and get DPL and DPC firmware image in build/firmware/mc-utils/config/ls2088a/RDB/dpl-eth.0x2A_0x41.dtb(dpc.0x2A_0x41.dtb).&lt;BR /&gt;$ flex-builder -c mc-utils -m ls2088ardb&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;In addition, please run "fsl_mc lazyapply dpl 0x580d00000" to deploy DPL before booting up Linux Kernel, I assume that you have deployed dpl image at 0x580d00000.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;root@TinyDistro:~# ls-addni dpmac.1&lt;BR /&gt;[&amp;nbsp;&amp;nbsp; 35.256512] iommu: Adding device dpbp.1 to group 1&lt;BR /&gt;[&amp;nbsp;&amp;nbsp; 35.372387] iommu: Adding device dpmcp.28 to group 1&lt;BR /&gt;[&amp;nbsp;&amp;nbsp; 35.491812] iommu: Adding device dpcon.1 to group 1&lt;BR /&gt;[&amp;nbsp;&amp;nbsp; 35.611740] iommu: Adding device dpcon.2 to group 1&lt;BR /&gt;[&amp;nbsp;&amp;nbsp; 35.733597] iommu: Adding device dpcon.3 to group 1&lt;BR /&gt;[&amp;nbsp;&amp;nbsp; 35.857659] iommu: Adding device dpcon.4 to group 1&lt;BR /&gt;[&amp;nbsp;&amp;nbsp; 35.984507] iommu: Adding device dpcon.5 to group 1&lt;BR /&gt;[&amp;nbsp;&amp;nbsp; 36.113581] iommu: Adding device dpcon.6 to group 1&lt;BR /&gt;[&amp;nbsp;&amp;nbsp; 36.243637] iommu: Adding device dpcon.7 to group 1&lt;BR /&gt;[&amp;nbsp;&amp;nbsp; 36.375477] iommu: Adding device dpcon.8 to group 1&lt;BR /&gt;[&amp;nbsp;&amp;nbsp; 36.529385] NOHZ: local_softirq_pending 80&lt;BR /&gt;[&amp;nbsp;&amp;nbsp; 36.533484] NOHZ: local_softirq_pending 80&lt;BR /&gt;[&amp;nbsp;&amp;nbsp; 36.537575] NOHZ: local_softirq_pending 282&lt;BR /&gt;[&amp;nbsp;&amp;nbsp; 36.541752] NOHZ: local_softirq_pending 282&lt;BR /&gt;[&amp;nbsp;&amp;nbsp; 36.545929] NOHZ: local_softirq_pending 282&lt;BR /&gt;[&amp;nbsp;&amp;nbsp; 36.550106] NOHZ: local_softirq_pending 282&lt;BR /&gt;[&amp;nbsp;&amp;nbsp; 36.564178] iommu: Adding device dpni.1 to group 1&lt;BR /&gt;[&amp;nbsp;&amp;nbsp; 36.617191] fsl_dpaa2_eth dpni.1: Key masks not supported. Steering is disabled&lt;BR /&gt;[&amp;nbsp;&amp;nbsp; 36.660687] fsl_dpaa2_eth dpni.1: Probed interface eth2&lt;BR /&gt;Created interface: eth2 (object:dpni.1, endpoint: dpmac.1)&lt;BR /&gt;root@TinyDistro:~# ifconfig eth2 100.10.1.159&lt;BR /&gt;[&amp;nbsp;&amp;nbsp; 62.653488] fsl_dpaa2_eth dpni.1 eth2: Link Event: state up&lt;BR /&gt;root@TinyDistro:~# ping 100.10.1.1&lt;BR /&gt;PING 100.10.1.1 (100.10.1.1): 56 data bytes&lt;BR /&gt;64 bytes from 100.10.1.1: seq=0 ttl=64 time=0.334 ms&lt;BR /&gt;64 bytes from 100.10.1.1: seq=1 ttl=64 time=0.150 ms&lt;BR /&gt;64 bytes from 100.10.1.1: seq=2 ttl=64 time=0.163 ms&lt;BR /&gt;64 bytes from 100.10.1.1: seq=3 ttl=64 time=0.137 ms&lt;BR /&gt;64 bytes from 100.10.1.1: seq=4 ttl=64 time=0.136 ms&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 19 Jul 2019 07:31:52 GMT</pubDate>
    <dc:creator>yipingwang</dc:creator>
    <dc:date>2019-07-19T07:31:52Z</dc:date>
    <item>
      <title>LS2088A can't find device file using ls-main command</title>
      <link>https://community.nxp.com/t5/Layerscape/LS2088A-can-t-find-device-file-using-ls-main-command/m-p/929282#M4459</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I want to add DAPP2 10GbE port in to system in order to run some sample that provide in LSDK19.06. But I found that using ls-main, ls-listni, ls-listmac are not working and all of them pop out a error message&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;root@localhost:~# ls-listmac&lt;BR /&gt;error: Did not find a device file&lt;BR /&gt;Restool wrapper scripts only support the latest major MC version&lt;BR /&gt;that currently is MC10.x. Use with caution.&lt;BR /&gt;error: Did not find a device file.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;OS:using LSDK 19.06 default setting. command: flex-installer -i auto -m ls2088ardb -d /dev/sdb&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm new boy in arm-based system, please help if OS is&amp;nbsp;build in wrong&amp;nbsp;way or other issue.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Jul 2019 01:38:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS2088A-can-t-find-device-file-using-ls-main-command/m-p/929282#M4459</guid>
      <dc:creator>hengjianzhang</dc:creator>
      <dc:date>2019-07-17T01:38:02Z</dc:date>
    </item>
    <item>
      <title>Re: LS2088A can't find device file using ls-main command</title>
      <link>https://community.nxp.com/t5/Layerscape/LS2088A-can-t-find-device-file-using-ls-main-command/m-p/929283#M4460</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN class=""&gt;Please make sure MC, DPL and DPC firmware images are deployed at the following offset addresses on Flash. Please refer to the attached u-boot log, please make sure fsl-mc is set up successfully.&lt;BR /&gt;DPAA2 MC 0x00A00000&lt;BR /&gt;DPAA2 DPL 0x00D00000&lt;BR /&gt;DPAA2 DPC 0x00E00000&lt;BR /&gt;You could get these firmware images with the following method.&lt;BR /&gt;Please execute the following command and get MC firmware image in build/firmware/qoriq-mc-binary/ls2088a/mc_10.10.0_ls2088a_20180814.itb.&lt;BR /&gt;$ flex-builder -c qoriq-mc-binary -m ls2088ardb&lt;BR /&gt;You could execute the following command and get DPL and DPC firmware image in build/firmware/mc-utils/config/ls2088a/RDB/dpl-eth.0x2A_0x41.dtb(dpc.0x2A_0x41.dtb).&lt;BR /&gt;$ flex-builder -c mc-utils -m ls2088ardb&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;In addition, please run "fsl_mc lazyapply dpl 0x580d00000" to deploy DPL before booting up Linux Kernel, I assume that you have deployed dpl image at 0x580d00000.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;root@TinyDistro:~# ls-addni dpmac.1&lt;BR /&gt;[&amp;nbsp;&amp;nbsp; 35.256512] iommu: Adding device dpbp.1 to group 1&lt;BR /&gt;[&amp;nbsp;&amp;nbsp; 35.372387] iommu: Adding device dpmcp.28 to group 1&lt;BR /&gt;[&amp;nbsp;&amp;nbsp; 35.491812] iommu: Adding device dpcon.1 to group 1&lt;BR /&gt;[&amp;nbsp;&amp;nbsp; 35.611740] iommu: Adding device dpcon.2 to group 1&lt;BR /&gt;[&amp;nbsp;&amp;nbsp; 35.733597] iommu: Adding device dpcon.3 to group 1&lt;BR /&gt;[&amp;nbsp;&amp;nbsp; 35.857659] iommu: Adding device dpcon.4 to group 1&lt;BR /&gt;[&amp;nbsp;&amp;nbsp; 35.984507] iommu: Adding device dpcon.5 to group 1&lt;BR /&gt;[&amp;nbsp;&amp;nbsp; 36.113581] iommu: Adding device dpcon.6 to group 1&lt;BR /&gt;[&amp;nbsp;&amp;nbsp; 36.243637] iommu: Adding device dpcon.7 to group 1&lt;BR /&gt;[&amp;nbsp;&amp;nbsp; 36.375477] iommu: Adding device dpcon.8 to group 1&lt;BR /&gt;[&amp;nbsp;&amp;nbsp; 36.529385] NOHZ: local_softirq_pending 80&lt;BR /&gt;[&amp;nbsp;&amp;nbsp; 36.533484] NOHZ: local_softirq_pending 80&lt;BR /&gt;[&amp;nbsp;&amp;nbsp; 36.537575] NOHZ: local_softirq_pending 282&lt;BR /&gt;[&amp;nbsp;&amp;nbsp; 36.541752] NOHZ: local_softirq_pending 282&lt;BR /&gt;[&amp;nbsp;&amp;nbsp; 36.545929] NOHZ: local_softirq_pending 282&lt;BR /&gt;[&amp;nbsp;&amp;nbsp; 36.550106] NOHZ: local_softirq_pending 282&lt;BR /&gt;[&amp;nbsp;&amp;nbsp; 36.564178] iommu: Adding device dpni.1 to group 1&lt;BR /&gt;[&amp;nbsp;&amp;nbsp; 36.617191] fsl_dpaa2_eth dpni.1: Key masks not supported. Steering is disabled&lt;BR /&gt;[&amp;nbsp;&amp;nbsp; 36.660687] fsl_dpaa2_eth dpni.1: Probed interface eth2&lt;BR /&gt;Created interface: eth2 (object:dpni.1, endpoint: dpmac.1)&lt;BR /&gt;root@TinyDistro:~# ifconfig eth2 100.10.1.159&lt;BR /&gt;[&amp;nbsp;&amp;nbsp; 62.653488] fsl_dpaa2_eth dpni.1 eth2: Link Event: state up&lt;BR /&gt;root@TinyDistro:~# ping 100.10.1.1&lt;BR /&gt;PING 100.10.1.1 (100.10.1.1): 56 data bytes&lt;BR /&gt;64 bytes from 100.10.1.1: seq=0 ttl=64 time=0.334 ms&lt;BR /&gt;64 bytes from 100.10.1.1: seq=1 ttl=64 time=0.150 ms&lt;BR /&gt;64 bytes from 100.10.1.1: seq=2 ttl=64 time=0.163 ms&lt;BR /&gt;64 bytes from 100.10.1.1: seq=3 ttl=64 time=0.137 ms&lt;BR /&gt;64 bytes from 100.10.1.1: seq=4 ttl=64 time=0.136 ms&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 19 Jul 2019 07:31:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS2088A-can-t-find-device-file-using-ls-main-command/m-p/929283#M4460</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2019-07-19T07:31:52Z</dc:date>
    </item>
  </channel>
</rss>