<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LSDK Prebuilt Images with DHCP in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/LSDK-Prebuilt-Images-with-DHCP/m-p/915425#M4361</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I've similar issue with a LS1012ARDB board ... but a bit different. Let me give a try here but will keep seeking community for correct thread. Using latest LSDK 19.09 and also able to build&amp;nbsp; &lt;SPAN class=""&gt;firmware_ls1012ardb_uboot_qspiboot.img&lt;/SPAN&gt;&amp;nbsp; I can flash and use. Note I flash it on &lt;STRONG&gt;bank 2&lt;/STRONG&gt; and not bank 1 of embedded QSPI flash device - maybe this is my problem and I shall put it on bank 1.&lt;/P&gt;&lt;P&gt;Problem I've is I simply don't see and cannot mount the eth0 device depsite in u-boot phase it seems to be up and running already. So I can boot and log into tiny Linux as root and there, in order to flash boot partition and userland I need first to bring up eth0 by doing " &lt;SPAN class=""&gt;ifconfig eth0 hw ether 00:80:48:BA:d1:30&lt;/SPAN&gt;". Doing that simply tells me there is no such device, I only can see "lo" and "sit0@NONE" devices, ping localhost works making me believe stack is up and alive. Any idea? Thx Christophe&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 12 Feb 2020 14:31:14 GMT</pubDate>
    <dc:creator>christophe_schm</dc:creator>
    <dc:date>2020-02-12T14:31:14Z</dc:date>
    <item>
      <title>LSDK Prebuilt Images with DHCP</title>
      <link>https://community.nxp.com/t5/Layerscape/LSDK-Prebuilt-Images-with-DHCP/m-p/915424#M4360</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Platon, just burned the lastest LSDK rootfs and boot partition to the SD card this morning with flex-installer, following the online documentation. &amp;nbsp;Since it boots, I would guess that whatever FW was burned into the QSPI is irrelevant, so I cannot understand why the eth0/eth1 (pfe_eth devices) on the FRWY-LS1012A board do not get the DHCP address. &amp;nbsp;I confirmed with WireShark that the board does NOT send any DHCP request, which would explain the DHCP failure.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Nothing turns on for the LSDK DHCP failure, so I am wondering how I could have screwed up such seemingly simple steps as writing the precompiled binary to the SD card. &amp;nbsp;It seems Ubuntu 18.04 went to netplan for the interface configuration, and going back to the ifupdown legacy system is not working.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Should I assume that the FRWY-LS1012A board is tested before the LSDK release, or is my board not supported any more?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 13 Oct 2019 02:00:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LSDK-Prebuilt-Images-with-DHCP/m-p/915424#M4360</guid>
      <dc:creator>henry10210</dc:creator>
      <dc:date>2019-10-13T02:00:30Z</dc:date>
    </item>
    <item>
      <title>Re: LSDK Prebuilt Images with DHCP</title>
      <link>https://community.nxp.com/t5/Layerscape/LSDK-Prebuilt-Images-with-DHCP/m-p/915425#M4361</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I've similar issue with a LS1012ARDB board ... but a bit different. Let me give a try here but will keep seeking community for correct thread. Using latest LSDK 19.09 and also able to build&amp;nbsp; &lt;SPAN class=""&gt;firmware_ls1012ardb_uboot_qspiboot.img&lt;/SPAN&gt;&amp;nbsp; I can flash and use. Note I flash it on &lt;STRONG&gt;bank 2&lt;/STRONG&gt; and not bank 1 of embedded QSPI flash device - maybe this is my problem and I shall put it on bank 1.&lt;/P&gt;&lt;P&gt;Problem I've is I simply don't see and cannot mount the eth0 device depsite in u-boot phase it seems to be up and running already. So I can boot and log into tiny Linux as root and there, in order to flash boot partition and userland I need first to bring up eth0 by doing " &lt;SPAN class=""&gt;ifconfig eth0 hw ether 00:80:48:BA:d1:30&lt;/SPAN&gt;". Doing that simply tells me there is no such device, I only can see "lo" and "sit0@NONE" devices, ping localhost works making me believe stack is up and alive. Any idea? Thx Christophe&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Feb 2020 14:31:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LSDK-Prebuilt-Images-with-DHCP/m-p/915425#M4361</guid>
      <dc:creator>christophe_schm</dc:creator>
      <dc:date>2020-02-12T14:31:14Z</dc:date>
    </item>
    <item>
      <title>Re: LSDK Prebuilt Images with DHCP</title>
      <link>https://community.nxp.com/t5/Layerscape/LSDK-Prebuilt-Images-with-DHCP/m-p/915426#M4362</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;For those with same problem as me and hitting this post, please go to this other post that seems more appropriate:&amp;nbsp;&lt;A href="https://community.nxp.com/message/1067146"&gt;https://community.nxp.com/message/1067146&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Feb 2020 14:50:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LSDK-Prebuilt-Images-with-DHCP/m-p/915426#M4362</guid>
      <dc:creator>christophe_schm</dc:creator>
      <dc:date>2020-02-12T14:50:03Z</dc:date>
    </item>
  </channel>
</rss>