<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LS1024A Power Requirements &amp; Nand Flash max size interfacable in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/LS1024A-Power-Requirements-Nand-Flash-max-size-interfacable/m-p/914533#M4357</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN style="font-size: 10pt;"&gt;LS1024A power consumption is provided in the AN4959, QorIQ LS1024A Family Thermal Application Considerations.&lt;BR clear="none" /&gt; There is no"NAND controller"as such within LS1024A. There is an expansion bus which is used to connect to the NAND device. The IO bus on NAND devices is 8 bits wide. Higher address bits than this are used for the NAND control signals. The bus signals are controlled by software to apply the command cycle, address cycle(s) and data cycle(s) to the NAND device. There is no hardware limitation because software can apply whatever signals it wants.&lt;BR clear="none" /&gt; The software release for this device includes NAND drivers that handle accesses to NAND.&lt;/SPAN&gt; &amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 18 Jul 2019 02:50:01 GMT</pubDate>
    <dc:creator>ufedor</dc:creator>
    <dc:date>2019-07-18T02:50:01Z</dc:date>
    <item>
      <title>LS1024A Power Requirements &amp; Nand Flash max size interfacable</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1024A-Power-Requirements-Nand-Flash-max-size-interfacable/m-p/914532#M4356</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="color: #222222; background-color: #ffffff;"&gt;Dear all,&lt;/SPAN&gt;&lt;BR data-jive-statusinputadd="true" data-jive-truncation-flag="true" style="color: #222222;" /&gt;&lt;BR data-jive-statusinputadd="true" data-jive-truncation-flag="true" style="color: #222222;" /&gt;&lt;SPAN style="color: #222222; background-color: #ffffff;"&gt;I'm a newbie to processor's world.&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN style="color: #222222; background-color: #ffffff;"&gt;Kindly help me understanding the below stuff:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #222222; background-color: #ffffff;"&gt;I&lt;/SPAN&gt;&lt;SPAN style="color: #222222; background-color: #ffffff;"&gt;&amp;nbsp;want to use LS1024A for its Crypto, USB 3.0 &amp;amp; Nand flash interfacing support.&amp;nbsp;&lt;/SPAN&gt;&lt;BR data-jive-statusinputadd="true" data-jive-truncation-flag="true" style="color: #222222;" /&gt;&lt;BR data-jive-statusinputadd="true" data-jive-truncation-flag="true" style="color: #222222;" /&gt;&lt;SPAN style="color: #222222; background-color: #ffffff;"&gt;* Unlike other Processor/MCU's,.... LS1024A's Electrical characteristics were not given. (Since I want to make a device which will be USB bus powered (5v,500-1A) can use USB Y cable ) &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #222222; background-color: #ffffff;"&gt;How can I know my estimated power consumption (when using above mentioned Crypto,USB 3.0 &amp;amp; Nand)/ do some power management (switch off one A9 core..etc) to make power consumption &amp;lt; 1A.&amp;nbsp;&amp;nbsp;&lt;/SPAN&gt;&lt;BR data-jive-statusinputadd="true" data-jive-truncation-flag="true" style="color: #222222;" /&gt;&lt;BR data-jive-statusinputadd="true" data-jive-truncation-flag="true" style="color: #222222;" /&gt;&lt;SPAN style="color: #222222; background-color: #ffffff;"&gt;* Is there any limit to the size of the flash devices that can be interfaced using Nand flash controller or EBI of LS1024A ?&amp;nbsp;&lt;/SPAN&gt;&lt;BR data-jive-statusinputadd="true" data-jive-truncation-flag="true" style="color: #222222;" /&gt;&lt;SPAN style="color: #222222; background-color: #ffffff;"&gt;(PS: I want to interface a 128GB (Giga Byte) Nand flash IC )&lt;/SPAN&gt;&lt;BR data-jive-statusinputadd="true" data-jive-truncation-flag="true" style="color: #222222;" /&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #222222; background-color: #ffffff;"&gt;Thanks in advance. &lt;/SPAN&gt;&lt;BR data-jive-statusinputadd="true" data-jive-truncation-flag="true" style="color: #222222;" /&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #222222; background-color: #ffffff;"&gt;&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/PavelChubakov"&gt;PavelChubakov&lt;/A&gt;‌ &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/ufedor"&gt;ufedor&lt;/A&gt;‌ &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/yipingwang"&gt;yipingwang&lt;/A&gt;‌ &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/alexander.yakovlev"&gt;alexander.yakovlev&lt;/A&gt;‌ &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/r8070z"&gt;r8070z&lt;/A&gt;‌ &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/ebiz_ws_prod"&gt;ebiz_ws_prod&lt;/A&gt;‌&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 13 Jul 2019 17:14:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1024A-Power-Requirements-Nand-Flash-max-size-interfacable/m-p/914532#M4356</guid>
      <dc:creator>tilakmarupilla</dc:creator>
      <dc:date>2019-07-13T17:14:10Z</dc:date>
    </item>
    <item>
      <title>Re: LS1024A Power Requirements &amp; Nand Flash max size interfacable</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1024A-Power-Requirements-Nand-Flash-max-size-interfacable/m-p/914533#M4357</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN style="font-size: 10pt;"&gt;LS1024A power consumption is provided in the AN4959, QorIQ LS1024A Family Thermal Application Considerations.&lt;BR clear="none" /&gt; There is no"NAND controller"as such within LS1024A. There is an expansion bus which is used to connect to the NAND device. The IO bus on NAND devices is 8 bits wide. Higher address bits than this are used for the NAND control signals. The bus signals are controlled by software to apply the command cycle, address cycle(s) and data cycle(s) to the NAND device. There is no hardware limitation because software can apply whatever signals it wants.&lt;BR clear="none" /&gt; The software release for this device includes NAND drivers that handle accesses to NAND.&lt;/SPAN&gt; &amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 18 Jul 2019 02:50:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1024A-Power-Requirements-Nand-Flash-max-size-interfacable/m-p/914533#M4357</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2019-07-18T02:50:01Z</dc:date>
    </item>
  </channel>
</rss>