<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Booting from SDHC memory card failed in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/Booting-from-SDHC-memory-card-failed/m-p/901491#M4228</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you, I have the same question. It's worked!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 28 Jun 2019 07:09:57 GMT</pubDate>
    <dc:creator>wangxiaozhuang</dc:creator>
    <dc:date>2019-06-28T07:09:57Z</dc:date>
    <item>
      <title>Booting from SDHC memory card failed</title>
      <link>https://community.nxp.com/t5/Layerscape/Booting-from-SDHC-memory-card-failed/m-p/901487#M4224</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm using the LS1028ARDB board for evaluation and failed to boot Linux with kernel 4.14.47 built with default settings and flexbuild_ls1028a_bsp0.3.&lt;/P&gt;&lt;P&gt;The SD-card I'm using were included and shipped with the evaluation board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Booting went good until SDHC tuning is executed, this tuning fails.&amp;nbsp;From this point on the kernel log is full of different errors pointing to read problems from SD-card.&lt;/P&gt;&lt;P&gt;The question is why the tuning fails and is there also a problem with default fallback clock like read in kernel messages?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I also tried a different card not SDHC which is working without problems.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here is a kernel log snippet from the point of first error:&lt;/P&gt;&lt;P&gt;&lt;CODE&gt;[ 4.372852] mmc0: Tuning failed, falling back to fixed sampling clock&lt;BR /&gt;[ 4.381853] mmcblk0: error -84 transferring data, sector 2277376, nr 8, cmd response 0x900, card status 0xc00&lt;BR /&gt;[ 4.400299] mmc0: Tuning failed, falling back to fixed sampling clock&lt;BR /&gt;[ 4.503983] mmcblk0: error -84 transferring data, sector 2277377, nr 7, cmd response 0x900, card status 0xc00&lt;BR /&gt;[ 4.522273] mmc0: Tuning failed, falling back to fixed sampling clock&lt;BR /&gt;[ 4.529051] print_req_error: I/O error, dev mmcblk0, sector 2277378&lt;BR /&gt;[ 4.535346] Buffer I/O error on dev mmcblk0p3, logical block 0, lost sync page write&lt;BR /&gt;[ 4.543626] EXT4-fs (mmcblk0p3): mounted filesystem with ordered data mode. Opts: (null)&lt;BR /&gt;[ 4.551776] VFS: Mounted root (ext4 filesystem) on device 179:3.&lt;BR /&gt;[ 4.560984] devtmpfs: mounted&lt;/CODE&gt;&lt;/P&gt;&lt;P&gt;&lt;CODE&gt;...&lt;/CODE&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 20 May 2019 12:46:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Booting-from-SDHC-memory-card-failed/m-p/901487#M4224</guid>
      <dc:creator>sevi</dc:creator>
      <dc:date>2019-05-20T12:46:50Z</dc:date>
    </item>
    <item>
      <title>Re: Booting from SDHC memory card failed</title>
      <link>https://community.nxp.com/t5/Layerscape/Booting-from-SDHC-memory-card-failed/m-p/901488#M4225</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please refer to the Getting Started with LS1028ARDB:&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/document/guide/getting-started-with-ls1028ardb:NGS-LS1028ARDB" title="https://www.nxp.com/document/guide/getting-started-with-ls1028ardb:NGS-LS1028ARDB"&gt;Getting Started with LS1028ARDB | NXP&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;and report the results of the firmware upgrade.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 May 2019 04:19:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Booting-from-SDHC-memory-card-failed/m-p/901488#M4225</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2019-05-21T04:19:23Z</dc:date>
    </item>
    <item>
      <title>Re: Booting from SDHC memory card failed</title>
      <link>https://community.nxp.com/t5/Layerscape/Booting-from-SDHC-memory-card-failed/m-p/901489#M4226</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you for the quick replay.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've tried the Getting Started procedure without any problems.&lt;/P&gt;&lt;P&gt;But if i go on building the boot system for the SD card with the LSDK flex-builder and flex-installer like it's described in LS1028ABSPUG.pdf, the booting process fails with the error described above.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 May 2019 05:16:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Booting-from-SDHC-memory-card-failed/m-p/901489#M4226</guid>
      <dc:creator>sevi</dc:creator>
      <dc:date>2019-05-21T05:16:57Z</dc:date>
    </item>
    <item>
      <title>Re: Booting from SDHC memory card failed</title>
      <link>https://community.nxp.com/t5/Layerscape/Booting-from-SDHC-memory-card-failed/m-p/901490#M4227</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please apply the following patch:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;--- a/ls1028ardb/R_SQPP_85bb/rcw_1300_sd.rcw&lt;/P&gt;&lt;P&gt;+++ b/ls1028ardb/R_SQPP_85bb/rcw_1300_sd.rcw&lt;/P&gt;&lt;P&gt;@@ -16,7 +16,7 @@ MEM_PLL_RAT=16&lt;/P&gt;&lt;P&gt;CGA_PLL1_RAT=13&lt;/P&gt;&lt;P&gt;CGA_PLL2_RAT=12&lt;/P&gt;&lt;P&gt;HWA_CGA_M1_CLK_SEL=7&lt;/P&gt;&lt;P&gt;-HWA_CGA_M2_CLK_SEL=7&lt;/P&gt;&lt;P&gt;+HWA_CGA_M2_CLK_SEL=1&lt;/P&gt;&lt;P&gt;HWA_CGA_M3_CLK_SEL=2&lt;/P&gt;&lt;P&gt;HWA_CGA_M4_CLK_SEL=3&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Jun 2019 14:15:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Booting-from-SDHC-memory-card-failed/m-p/901490#M4227</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2019-06-11T14:15:16Z</dc:date>
    </item>
    <item>
      <title>Re: Booting from SDHC memory card failed</title>
      <link>https://community.nxp.com/t5/Layerscape/Booting-from-SDHC-memory-card-failed/m-p/901491#M4228</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you, I have the same question. It's worked!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 28 Jun 2019 07:09:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Booting-from-SDHC-memory-card-failed/m-p/901491#M4228</guid>
      <dc:creator>wangxiaozhuang</dc:creator>
      <dc:date>2019-06-28T07:09:57Z</dc:date>
    </item>
  </channel>
</rss>