<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LayerscapeのトピックRe: LS1046A &amp; LS1046A-RDB Available Memory</title>
    <link>https://community.nxp.com/t5/Layerscape/LS1046A-LS1046A-RDB-Available-Memory/m-p/895472#M4184</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Maximum supported LS1046A DDR controller 64-bit bank size is 16 GB.&lt;/P&gt;&lt;P&gt;The DDR controller supports 4 banks.&lt;/P&gt;&lt;P&gt;Refer to the QorIQ LS1046A Reference Manual, Table 15-9. Supported SDRAM Device Configurations, DDR4.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 16 Apr 2019 01:41:19 GMT</pubDate>
    <dc:creator>ufedor</dc:creator>
    <dc:date>2019-04-16T01:41:19Z</dc:date>
    <item>
      <title>LS1046A &amp; LS1046A-RDB Available Memory</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1046A-LS1046A-RDB-Available-Memory/m-p/895471#M4183</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm currently working with the LS1046A-RDB reference board design kit provided by eInfoChips.&amp;nbsp; &amp;nbsp;The application notes on the system defines that the available memory for the single physical bank is 8-GB.&amp;nbsp; For the reference kit, is this the maximum available memory or can I swap the memory module with a larger DDR4?&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When designing my own board off the LS1046A QorIQ Layerscape, what's the maximum physical bank count and memory capacity per bank that I can put into my design?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 15 Apr 2019 16:32:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1046A-LS1046A-RDB-Available-Memory/m-p/895471#M4183</guid>
      <dc:creator>ahanson</dc:creator>
      <dc:date>2019-04-15T16:32:15Z</dc:date>
    </item>
    <item>
      <title>Re: LS1046A &amp; LS1046A-RDB Available Memory</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1046A-LS1046A-RDB-Available-Memory/m-p/895472#M4184</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Maximum supported LS1046A DDR controller 64-bit bank size is 16 GB.&lt;/P&gt;&lt;P&gt;The DDR controller supports 4 banks.&lt;/P&gt;&lt;P&gt;Refer to the QorIQ LS1046A Reference Manual, Table 15-9. Supported SDRAM Device Configurations, DDR4.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 Apr 2019 01:41:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1046A-LS1046A-RDB-Available-Memory/m-p/895472#M4184</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2019-04-16T01:41:19Z</dc:date>
    </item>
  </channel>
</rss>