<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LayerscapeのトピックRe: Corrupted QSPI flash LS1046ARDB</title>
    <link>https://community.nxp.com/t5/Layerscape/Corrupted-QSPI-flash-LS1046ARDB/m-p/895259#M4162</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You wrote:&lt;/P&gt;&lt;P&gt;&amp;gt;&amp;nbsp;with the debugger, we can flash uboot_ls1046ardb_qspi.bin at 0x40100000 and dump it, but &lt;SPAN style="font-size: 12.0pt;"&gt;we are unable&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12.0pt;"&gt;&amp;gt; to flash rcw_1800_qspiboot.bin at 0x40000000~0x40008000 we can’t even erase this flash block&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Do you see a change in Flash Programmer behaviour when SW2[5] is altered?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 15 Apr 2019 10:05:43 GMT</pubDate>
    <dc:creator>ufedor</dc:creator>
    <dc:date>2019-04-15T10:05:43Z</dc:date>
    <item>
      <title>Corrupted QSPI flash LS1046ARDB</title>
      <link>https://community.nxp.com/t5/Layerscape/Corrupted-QSPI-flash-LS1046ARDB/m-p/895258#M4161</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;First, we tried to flash uboot into ls1046ardb qspi using a debugger. After a bad manipulation, Uboot was unable to load and prompt in serial neither on bank0 nor bank4. In order to recover uboot in bank0 &amp;amp; bank4 we booted from an SD card and flashed uboot on bank0 and bank4 with “sf ...” commands.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;With the command “cpld reset altbank” we can load uboot flashed in qspi bank4 (after a boot from SD card). But with SW3[5] = 1 ,in order to boot on bank4 after a simple reset, nothing happens.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Bank0 is totally inaccessible. After a reset without SD card, nothing happens, the board seems to be stuck in reset mode. Moreover, with the debugger, we can flash uboot_ls1046ardb_qspi.bin at 0x40100000 and dump it, but we are unable to flash rcw_1800_qspiboot.bin at 0x40000000~0x40008000 we can’t even erase this flash block, values are always 0.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you in advance for your assistance.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 15 Apr 2019 08:03:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Corrupted-QSPI-flash-LS1046ARDB/m-p/895258#M4161</guid>
      <dc:creator>clement_barriba</dc:creator>
      <dc:date>2019-04-15T08:03:18Z</dc:date>
    </item>
    <item>
      <title>Re: Corrupted QSPI flash LS1046ARDB</title>
      <link>https://community.nxp.com/t5/Layerscape/Corrupted-QSPI-flash-LS1046ARDB/m-p/895259#M4162</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You wrote:&lt;/P&gt;&lt;P&gt;&amp;gt;&amp;nbsp;with the debugger, we can flash uboot_ls1046ardb_qspi.bin at 0x40100000 and dump it, but &lt;SPAN style="font-size: 12.0pt;"&gt;we are unable&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12.0pt;"&gt;&amp;gt; to flash rcw_1800_qspiboot.bin at 0x40000000~0x40008000 we can’t even erase this flash block&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Do you see a change in Flash Programmer behaviour when SW2[5] is altered?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 15 Apr 2019 10:05:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Corrupted-QSPI-flash-LS1046ARDB/m-p/895259#M4162</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2019-04-15T10:05:43Z</dc:date>
    </item>
    <item>
      <title>Re: Corrupted QSPI flash LS1046ARDB</title>
      <link>https://community.nxp.com/t5/Layerscape/Corrupted-QSPI-flash-LS1046ARDB/m-p/895260#M4163</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Do you mean SW3[5] ? I have not seen differences in Flash Programmer behaviour between SW3[5]=1 and SW3[5]=0.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 15 Apr 2019 12:51:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Corrupted-QSPI-flash-LS1046ARDB/m-p/895260#M4163</guid>
      <dc:creator>clement_barriba</dc:creator>
      <dc:date>2019-04-15T12:51:43Z</dc:date>
    </item>
    <item>
      <title>Re: Corrupted QSPI flash LS1046ARDB</title>
      <link>https://community.nxp.com/t5/Layerscape/Corrupted-QSPI-flash-LS1046ARDB/m-p/895261#M4164</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;What is the RCW source when the CodeWarrior Flash Programmer is used?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please after booting from SD card use U-Boot to program complete firmware image into SPI DEV#0 by executing "sf probe 0:0" command instead of "sf probe 0:1".&lt;/P&gt;&lt;P&gt;The firmware image could be downloaded from:&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://lsdk.github.io/components.html" title="https://lsdk.github.io/components.html"&gt;LSDK Open Source&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;COMPONENTS -&amp;gt; LSDK IMAGES&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 15 Apr 2019 13:22:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Corrupted-QSPI-flash-LS1046ARDB/m-p/895261#M4164</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2019-04-15T13:22:07Z</dc:date>
    </item>
    <item>
      <title>Re: Corrupted QSPI flash LS1046ARDB</title>
      <link>https://community.nxp.com/t5/Layerscape/Corrupted-QSPI-flash-LS1046ARDB/m-p/895262#M4165</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We are using RCW and firmware image from bootpartition_arm64_lts_4.14 (it works perfectly on bank4). Our debugger is Lauterbach power debug pro. We already tried to load the firmware image with the command "sf probe 0:0". After a memory dump with the command "md" we see that the flash is correctly programmed except the RCW at the address range 0x40000000 to 0x40007fff that is empty (filled with 0). &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 15 Apr 2019 14:15:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Corrupted-QSPI-flash-LS1046ARDB/m-p/895262#M4165</guid>
      <dc:creator>clement_barriba</dc:creator>
      <dc:date>2019-04-15T14:15:14Z</dc:date>
    </item>
    <item>
      <title>Re: Corrupted QSPI flash LS1046ARDB</title>
      <link>https://community.nxp.com/t5/Layerscape/Corrupted-QSPI-flash-LS1046ARDB/m-p/895263#M4166</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please discuss the debugger SPI Flash programming issue with Lauterbach.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 15 Apr 2019 14:35:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Corrupted-QSPI-flash-LS1046ARDB/m-p/895263#M4166</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2019-04-15T14:35:31Z</dc:date>
    </item>
    <item>
      <title>Re: Corrupted QSPI flash LS1046ARDB</title>
      <link>https://community.nxp.com/t5/Layerscape/Corrupted-QSPI-flash-LS1046ARDB/m-p/895264#M4167</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;This issue is present in the flash file "snor_ls1000.bin" for LS1xxx from March-2019 - September-2019.&lt;/P&gt;&lt;P&gt;It is recommended to use the Lauterbach DVD release 2019.02 which doesn't contain this issue.&lt;/P&gt;&lt;P&gt;As an alternative, please contact Lauterbach (&lt;A href="mailto:support@lauterbach.com"&gt;support@lauterbach.com&lt;/A&gt;) for an update.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you don't want to do a full update of your software, please look for the file "snor_ls1000.bin" in your TRACE32 installation and replace it by a newer version. You can either use the binary from the Lauterbach DVD release 2019.02 or request it from the support.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 01 Oct 2019 14:14:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Corrupted-QSPI-flash-LS1046ARDB/m-p/895264#M4167</guid>
      <dc:creator>benedikt_schroe</dc:creator>
      <dc:date>2019-10-01T14:14:52Z</dc:date>
    </item>
  </channel>
</rss>