<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Layerscape中的主题 Discrepancy Between LS1043A Datasheet and Design Guide</title>
    <link>https://community.nxp.com/t5/Layerscape/Discrepancy-Between-LS1043A-Datasheet-and-Design-Guide/m-p/888669#M4127</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a question pertaining to the LS1043A and LS10xxA family. The datasheet of this device lists +/-30mV as the recommended value for the rail on VDD. The design guide for supply filtering, however, lists the requirements as +50mV/-30mV. This is a significant difference at this tight of a spec so I was posting for clarification on which of these is correct, and whether the datasheet is referring solely to DC variation and does not include transients or not.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Abhinav.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 21 Jan 2019 23:02:46 GMT</pubDate>
    <dc:creator>abhinav</dc:creator>
    <dc:date>2019-01-21T23:02:46Z</dc:date>
    <item>
      <title>Discrepancy Between LS1043A Datasheet and Design Guide</title>
      <link>https://community.nxp.com/t5/Layerscape/Discrepancy-Between-LS1043A-Datasheet-and-Design-Guide/m-p/888669#M4127</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a question pertaining to the LS1043A and LS10xxA family. The datasheet of this device lists +/-30mV as the recommended value for the rail on VDD. The design guide for supply filtering, however, lists the requirements as +50mV/-30mV. This is a significant difference at this tight of a spec so I was posting for clarification on which of these is correct, and whether the datasheet is referring solely to DC variation and does not include transients or not.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Abhinav.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 21 Jan 2019 23:02:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Discrepancy-Between-LS1043A-Datasheet-and-Design-Guide/m-p/888669#M4127</guid>
      <dc:creator>abhinav</dc:creator>
      <dc:date>2019-01-21T23:02:46Z</dc:date>
    </item>
    <item>
      <title>Re: Discrepancy Between LS1043A Datasheet and Design Guide</title>
      <link>https://community.nxp.com/t5/Layerscape/Discrepancy-Between-LS1043A-Datasheet-and-Design-Guide/m-p/888670#M4128</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;For positive transient response, it must be below Vdd + 50 mV (although it may exceed Vdd + 30 mV)&lt;BR /&gt;For negative transient response, it must be within Vdd - 30 mV.&lt;/P&gt;&lt;P&gt;The +50mv -30mv is total deviation due to thermal, di/dt of transients, base regulation and ripple from the regulator.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Andrei&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 01 Feb 2019 09:44:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Discrepancy-Between-LS1043A-Datasheet-and-Design-Guide/m-p/888670#M4128</guid>
      <dc:creator>andrei_skok</dc:creator>
      <dc:date>2019-02-01T09:44:54Z</dc:date>
    </item>
  </channel>
</rss>