<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LayerscapeのトピックRe: LS2088A - QUERY ON RTC</title>
    <link>https://community.nxp.com/t5/Layerscape/LS2088A-QUERY-ON-RTC/m-p/886823#M4120</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;TA_BB_RTC has been de-featured. Since there were customers that have already designed with the pin name, it was decided to keep the pin name.&lt;BR /&gt;Note 15 is correct. New designs should disregard the reference board on this and be implemented in accordance with the processor's Data Sheet.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 25 Feb 2019 07:11:22 GMT</pubDate>
    <dc:creator>ufedor</dc:creator>
    <dc:date>2019-02-25T07:11:22Z</dc:date>
    <item>
      <title>LS2088A - QUERY ON RTC</title>
      <link>https://community.nxp.com/t5/Layerscape/LS2088A-QUERY-ON-RTC/m-p/886822#M4119</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am working in LS2088A based project. I have doubt in RTC. There exist a pin TA_BB_RTC&amp;nbsp; - pin K19. In datasheet, it is referred as reverved and given a note to connect it ground. But, Is this anything regarding the optional RTC clock? Should we give the provision of optional Oscillator?&lt;/P&gt;&lt;P&gt;If not, why is the name TA_BB_RTC. Please clarify.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 25 Feb 2019 06:20:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS2088A-QUERY-ON-RTC/m-p/886822#M4119</guid>
      <dc:creator>preethi_rajagop</dc:creator>
      <dc:date>2019-02-25T06:20:00Z</dc:date>
    </item>
    <item>
      <title>Re: LS2088A - QUERY ON RTC</title>
      <link>https://community.nxp.com/t5/Layerscape/LS2088A-QUERY-ON-RTC/m-p/886823#M4120</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;TA_BB_RTC has been de-featured. Since there were customers that have already designed with the pin name, it was decided to keep the pin name.&lt;BR /&gt;Note 15 is correct. New designs should disregard the reference board on this and be implemented in accordance with the processor's Data Sheet.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 25 Feb 2019 07:11:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS2088A-QUERY-ON-RTC/m-p/886823#M4120</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2019-02-25T07:11:22Z</dc:date>
    </item>
  </channel>
</rss>