<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic LS2088A TA_BB_VDD and TA_BB_RTC in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/LS2088A-TA-BB-VDD-and-TA-BB-RTC/m-p/882221#M4076</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I are working LS2088 based project. I have a query regarding the power consumption of TA_BB_VDD pin which is given as 1.5mW in the application note. I just want to know whether this is the peak power dissipation or the continuous power dissipation on the TA_BB_VDD.&lt;/P&gt;&lt;P&gt;Regarding the TA_BB_RTC, can it be connected to the TA_BB_VDD if the thrust programming is not done i.e for normal operation?&lt;/P&gt;&lt;P&gt;I want a rechargable battery for generating TA_BB_VDD and the lifespan of the fully charged rechargable battery should be 7 days. So kindly let me know any reference calculation is available for the battery capacity estimation.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 21 Feb 2019 14:02:02 GMT</pubDate>
    <dc:creator>sekuru_saimukhe</dc:creator>
    <dc:date>2019-02-21T14:02:02Z</dc:date>
    <item>
      <title>LS2088A TA_BB_VDD and TA_BB_RTC</title>
      <link>https://community.nxp.com/t5/Layerscape/LS2088A-TA-BB-VDD-and-TA-BB-RTC/m-p/882221#M4076</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I are working LS2088 based project. I have a query regarding the power consumption of TA_BB_VDD pin which is given as 1.5mW in the application note. I just want to know whether this is the peak power dissipation or the continuous power dissipation on the TA_BB_VDD.&lt;/P&gt;&lt;P&gt;Regarding the TA_BB_RTC, can it be connected to the TA_BB_VDD if the thrust programming is not done i.e for normal operation?&lt;/P&gt;&lt;P&gt;I want a rechargable battery for generating TA_BB_VDD and the lifespan of the fully charged rechargable battery should be 7 days. So kindly let me know any reference calculation is available for the battery capacity estimation.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Feb 2019 14:02:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS2088A-TA-BB-VDD-and-TA-BB-RTC/m-p/882221#M4076</guid>
      <dc:creator>sekuru_saimukhe</dc:creator>
      <dc:date>2019-02-21T14:02:02Z</dc:date>
    </item>
    <item>
      <title>Re: LS2088A TA_BB_VDD and TA_BB_RTC</title>
      <link>https://community.nxp.com/t5/Layerscape/LS2088A-TA-BB-VDD-and-TA-BB-RTC/m-p/882222#M4077</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;This 1.5mW number&amp;nbsp; is absolute maximum rating, actual power consumption depends on temperature and may vary from batch to batch. You should use this 1.5mW number for your battery capacity calculations.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; TA_BB_RTC should be tied to ground according to LS2088 device datasheet, Table 1, Note 15.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Alexander,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 24 Feb 2019 13:02:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS2088A-TA-BB-VDD-and-TA-BB-RTC/m-p/882222#M4077</guid>
      <dc:creator>alexander_yakov</dc:creator>
      <dc:date>2019-02-24T13:02:57Z</dc:date>
    </item>
  </channel>
</rss>