<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: [LS1043ARDB] full duplex mode for dspi? in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/LS1043ARDB-full-duplex-mode-for-dspi/m-p/863504#M3961</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;SPI controller is full-duplex by design - "serial data in" and "serial data out" lines are separate, so you can transmit and receive simultaneously.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Alexander&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 09 Jan 2019 17:40:34 GMT</pubDate>
    <dc:creator>alexander_yakov</dc:creator>
    <dc:date>2019-01-09T17:40:34Z</dc:date>
    <item>
      <title>[LS1043ARDB] full duplex mode for dspi?</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1043ARDB-full-duplex-mode-for-dspi/m-p/863503#M3960</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Is the ls1043ardb dspi full duplex mode or half duplex?&lt;/P&gt;&lt;P&gt;and is possible to set dspi full/half duplex mode?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Jan 2019 15:05:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1043ARDB-full-duplex-mode-for-dspi/m-p/863503#M3960</guid>
      <dc:creator>randy_wang</dc:creator>
      <dc:date>2019-01-09T15:05:48Z</dc:date>
    </item>
    <item>
      <title>Re: [LS1043ARDB] full duplex mode for dspi?</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1043ARDB-full-duplex-mode-for-dspi/m-p/863504#M3961</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;SPI controller is full-duplex by design - "serial data in" and "serial data out" lines are separate, so you can transmit and receive simultaneously.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Alexander&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Jan 2019 17:40:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1043ARDB-full-duplex-mode-for-dspi/m-p/863504#M3961</guid>
      <dc:creator>alexander_yakov</dc:creator>
      <dc:date>2019-01-09T17:40:34Z</dc:date>
    </item>
  </channel>
</rss>