<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LS1043A CSn bus timing issue in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/LS1043A-CSn-bus-timing-issue/m-p/858805#M3929</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Found the issue.&amp;nbsp; In 28-bit addressing mode the RB0 input is used for the RB signal for all other CSn besides CS1.&amp;nbsp; With heavy write accesses to both NOR flash (CS0) and FPGA (CS3), the FPGA accesses were terminating early due to RY/BY# signal from NOR flash.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;CPLD design is largely copied from RDB design.&amp;nbsp; The logic for the RB0 signal has been updated to be qualified with CS0.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the help&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 08 Jan 2019 16:19:39 GMT</pubDate>
    <dc:creator>garybeck</dc:creator>
    <dc:date>2019-01-08T16:19:39Z</dc:date>
    <item>
      <title>LS1043A CSn bus timing issue</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1043A-CSn-bus-timing-issue/m-p/858803#M3927</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We have a custom LS1043A board with the following peripherals mapped&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;CS0 - NOR Flash (256MB)&lt;/P&gt;&lt;P&gt;CS1 - NOR Flash (256MB)&lt;/P&gt;&lt;P&gt;CS2 - 8 bit GPCM (64KB)&lt;/P&gt;&lt;P&gt;CS3 - 16 bit GPCM (64KB)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Seeing some strange&amp;nbsp;bus timing on CS2 and CS3 when CS0 write cycles are heavily utilized.&amp;nbsp; Seems as though the write cycle timing from the CS0 region is being applied to the write cycles for the CS2&amp;amp;3 regions for a short period of time.&amp;nbsp; The bus timing does revert back to&amp;nbsp;the programmed values&amp;nbsp;once the CS0 accesses cease.&amp;nbsp; The bus timing for CS0 is the same as the RDB.&amp;nbsp; The bus timing for CS2&amp;amp;3 are much longer (x10) due to design constraints.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Has anyone seen varying bus timing on the LS1043A IFC interface?&amp;nbsp; Is there any errata?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 07 Jan 2019 22:20:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1043A-CSn-bus-timing-issue/m-p/858803#M3927</guid>
      <dc:creator>garybeck</dc:creator>
      <dc:date>2019-01-07T22:20:35Z</dc:date>
    </item>
    <item>
      <title>Re: LS1043A CSn bus timing issue</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1043A-CSn-bus-timing-issue/m-p/858804#M3928</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please note that RB signal function for GPCM is External Termination of Access.&lt;/P&gt;&lt;P&gt;Ensure that RB signal corresponding to the CS2&amp;amp;3 is not floating.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 08 Jan 2019 02:59:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1043A-CSn-bus-timing-issue/m-p/858804#M3928</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2019-01-08T02:59:08Z</dc:date>
    </item>
    <item>
      <title>Re: LS1043A CSn bus timing issue</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1043A-CSn-bus-timing-issue/m-p/858805#M3929</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Found the issue.&amp;nbsp; In 28-bit addressing mode the RB0 input is used for the RB signal for all other CSn besides CS1.&amp;nbsp; With heavy write accesses to both NOR flash (CS0) and FPGA (CS3), the FPGA accesses were terminating early due to RY/BY# signal from NOR flash.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;CPLD design is largely copied from RDB design.&amp;nbsp; The logic for the RB0 signal has been updated to be qualified with CS0.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the help&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 08 Jan 2019 16:19:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1043A-CSn-bus-timing-issue/m-p/858805#M3929</guid>
      <dc:creator>garybeck</dc:creator>
      <dc:date>2019-01-08T16:19:39Z</dc:date>
    </item>
  </channel>
</rss>