<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Layerscape中的主题 Uboot does not boot on LS1021ATSN board</title>
    <link>https://community.nxp.com/t5/Layerscape/Uboot-does-not-boot-on-LS1021ATSN-board/m-p/857687#M3904</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;summary: we&amp;nbsp;wrote invalid data under the Uboot of the LS1021ATSN board, causing Uboot to fail to boot.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Detailed&amp;nbsp;description：&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Our LS1021ATSN is the board that the SD card boot. After I loaded the sdcard.img in the card, I debug it via USB. Enter the following command under Uboot: mmc write 0x81000000 8 0x500, then I can't enter Uboot. Finally, I formatted the SD card to re-copy the sdcard.img or not enter.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/76957iF083387334EE4DA9/image-size/large?v=v2&amp;amp;px=999" title="TIM图片20190124112826.png" alt="TIM图片20190124112826.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 24 Jan 2019 03:32:31 GMT</pubDate>
    <dc:creator>lyt1994125</dc:creator>
    <dc:date>2019-01-24T03:32:31Z</dc:date>
    <item>
      <title>Uboot does not boot on LS1021ATSN board</title>
      <link>https://community.nxp.com/t5/Layerscape/Uboot-does-not-boot-on-LS1021ATSN-board/m-p/857687#M3904</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;summary: we&amp;nbsp;wrote invalid data under the Uboot of the LS1021ATSN board, causing Uboot to fail to boot.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Detailed&amp;nbsp;description：&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Our LS1021ATSN is the board that the SD card boot. After I loaded the sdcard.img in the card, I debug it via USB. Enter the following command under Uboot: mmc write 0x81000000 8 0x500, then I can't enter Uboot. Finally, I formatted the SD card to re-copy the sdcard.img or not enter.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/76957iF083387334EE4DA9/image-size/large?v=v2&amp;amp;px=999" title="TIM图片20190124112826.png" alt="TIM图片20190124112826.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 24 Jan 2019 03:32:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Uboot-does-not-boot-on-LS1021ATSN-board/m-p/857687#M3904</guid>
      <dc:creator>lyt1994125</dc:creator>
      <dc:date>2019-01-24T03:32:31Z</dc:date>
    </item>
    <item>
      <title>Re: Uboot does not boot on LS1021ATSN board</title>
      <link>https://community.nxp.com/t5/Layerscape/Uboot-does-not-boot-on-LS1021ATSN-board/m-p/857688#M3905</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please build u-boot images with the following commands.&lt;/P&gt;&lt;P&gt;$ cd openil&lt;BR /&gt;$ make nxp_ls1021atsn_defconfig&lt;BR /&gt;$ make&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please check the switch setting&lt;/P&gt;&lt;P&gt;LS1021ATSN SD card SW2 = 0b’111111&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 07 Apr 2019 12:36:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Uboot-does-not-boot-on-LS1021ATSN-board/m-p/857688#M3905</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2019-04-07T12:36:28Z</dc:date>
    </item>
    <item>
      <title>Re: Uboot does not boot on LS1021ATSN board</title>
      <link>https://community.nxp.com/t5/Layerscape/Uboot-does-not-boot-on-LS1021ATSN-board/m-p/1439037#M10337</link>
      <description>&lt;P&gt;Hi ,&lt;/P&gt;&lt;P&gt;I want to ask how to check the switch setting&amp;nbsp;&lt;/P&gt;&lt;P&gt;Ls1021ATSN SD sdcard SW2=0b’111111&lt;/P&gt;&lt;P&gt;I check &amp;nbsp;the Openil user guide but didn’t mention it.&lt;/P&gt;&lt;P&gt;I will be grateful if you can help me&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 05 Apr 2022 16:21:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Uboot-does-not-boot-on-LS1021ATSN-board/m-p/1439037#M10337</guid>
      <dc:creator>Liing</dc:creator>
      <dc:date>2022-04-05T16:21:32Z</dc:date>
    </item>
  </channel>
</rss>