<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LayerscapeのトピックRe: can nand controller ECC has the ability to correct bit-flip in OOB area?</title>
    <link>https://community.nxp.com/t5/Layerscape/can-nand-controller-ECC-has-the-ability-to-correct-bit-flip-in/m-p/856446#M3898</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;So both main region data and the corresponding ECC bytes stored in OOB are ecc-protected,&amp;nbsp;that's good for me.&lt;/P&gt;&lt;P&gt;thank you so much for your explanation.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 11 Feb 2019 03:18:43 GMT</pubDate>
    <dc:creator>luckyluo</dc:creator>
    <dc:date>2019-02-11T03:18:43Z</dc:date>
    <item>
      <title>can nand controller ECC has the ability to correct bit-flip in OOB area?</title>
      <link>https://community.nxp.com/t5/Layerscape/can-nand-controller-ECC-has-the-ability-to-correct-bit-flip-in/m-p/856444#M3896</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear NXP,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using LS1088A in my product, I am sure that the nand controller ECC can fix the bit-flip in data area, but can nand controller ECC has the ability to correct bit-flip in OOB area? e.g if there is one bit-flip in OOB ecc position, this means the ecc content in OOB is wrong in one bit, so what will ECC do? can it detect this bit-flip and fix it?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks a lot&lt;/P&gt;&lt;P&gt;Lucky Luo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 24 Jan 2019 08:22:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/can-nand-controller-ECC-has-the-ability-to-correct-bit-flip-in/m-p/856444#M3896</guid>
      <dc:creator>luckyluo</dc:creator>
      <dc:date>2019-01-24T08:22:41Z</dc:date>
    </item>
    <item>
      <title>Re: can nand controller ECC has the ability to correct bit-flip in OOB area?</title>
      <link>https://community.nxp.com/t5/Layerscape/can-nand-controller-ECC-has-the-ability-to-correct-bit-flip-in/m-p/856445#M3897</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;A _jive_internal="true" class="" data-content-finding="Community" data-userid="312163" data-username="luckyluo" href="https://community.nxp.com/people/luckyluo"&gt;Lucky Luo&lt;/A&gt; ,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The IFC computes the ECC only for the main region data (as the ECC is not computed for the spare region).&lt;/P&gt;&lt;P&gt;The decoder detects and corrects 4/8 bits of error on the main region data and the corresponding ECC bytes stored.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 01 Feb 2019 08:31:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/can-nand-controller-ECC-has-the-ability-to-correct-bit-flip-in/m-p/856445#M3897</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2019-02-01T08:31:03Z</dc:date>
    </item>
    <item>
      <title>Re: can nand controller ECC has the ability to correct bit-flip in OOB area?</title>
      <link>https://community.nxp.com/t5/Layerscape/can-nand-controller-ECC-has-the-ability-to-correct-bit-flip-in/m-p/856446#M3898</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;So both main region data and the corresponding ECC bytes stored in OOB are ecc-protected,&amp;nbsp;that's good for me.&lt;/P&gt;&lt;P&gt;thank you so much for your explanation.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 11 Feb 2019 03:18:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/can-nand-controller-ECC-has-the-ability-to-correct-bit-flip-in/m-p/856446#M3898</guid>
      <dc:creator>luckyluo</dc:creator>
      <dc:date>2019-02-11T03:18:43Z</dc:date>
    </item>
  </channel>
</rss>