<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LayerscapeのトピックProblem using LS1046A as USB 2.0 Host</title>
    <link>https://community.nxp.com/t5/Layerscape/Problem-using-LS1046A-as-USB-2-0-Host/m-p/854903#M3890</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello!&lt;/P&gt;&lt;P&gt;We have a custom LS1046A board at which we have only connected D M/P wires from the second USB controller.&lt;/P&gt;&lt;P&gt;We do not get any USB device to register in U-Boot. Do you have any hints on what do change in U-Boot/DTB/Linux to get it working?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have seen a suggestion to set Global hardware parameters register 3 (GHWPARAMS3) DWC_USB3_SS_PHY_INTERFACE to zero to "put" it in USB 2.0 mode. But this is a read only register and it is set to 1 (PIPE3/USB 3.0).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Robert&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 26 Mar 2019 13:52:43 GMT</pubDate>
    <dc:creator>Robbo76</dc:creator>
    <dc:date>2019-03-26T13:52:43Z</dc:date>
    <item>
      <title>Problem using LS1046A as USB 2.0 Host</title>
      <link>https://community.nxp.com/t5/Layerscape/Problem-using-LS1046A-as-USB-2-0-Host/m-p/854903#M3890</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello!&lt;/P&gt;&lt;P&gt;We have a custom LS1046A board at which we have only connected D M/P wires from the second USB controller.&lt;/P&gt;&lt;P&gt;We do not get any USB device to register in U-Boot. Do you have any hints on what do change in U-Boot/DTB/Linux to get it working?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have seen a suggestion to set Global hardware parameters register 3 (GHWPARAMS3) DWC_USB3_SS_PHY_INTERFACE to zero to "put" it in USB 2.0 mode. But this is a read only register and it is set to 1 (PIPE3/USB 3.0).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Robert&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Mar 2019 13:52:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Problem-using-LS1046A-as-USB-2-0-Host/m-p/854903#M3890</guid>
      <dc:creator>Robbo76</dc:creator>
      <dc:date>2019-03-26T13:52:43Z</dc:date>
    </item>
    <item>
      <title>Re: Problem using LS1046A as USB 2.0 Host</title>
      <link>https://community.nxp.com/t5/Layerscape/Problem-using-LS1046A-as-USB-2-0-Host/m-p/854904#M3891</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;Your connection is similar to connection between super-speed host and super-speed device using USB 2.0 cable.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;We have tested this configuration. There is correct connection. There is message from u-boot that USB 2.0 device is connected.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;See information about &lt;/SPAN&gt;&lt;SPAN style="font-size: 10.0pt; color: #242729; background: white;"&gt;super speed enumeration&lt;/SPAN&gt; on the following page:&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;&lt;A href="https://electronics.stackexchange.com/questions/297031/usb-3-x-ss-enumeration"&gt;https://electronics.stackexchange.com/questions/297031/usb-3-x-ss-enumeration&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Pavel Chubakov&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Mar 2019 05:12:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Problem-using-LS1046A-as-USB-2-0-Host/m-p/854904#M3891</guid>
      <dc:creator>Pavel</dc:creator>
      <dc:date>2019-03-28T05:12:34Z</dc:date>
    </item>
  </channel>
</rss>