<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Layerscape中的主题 Recovering bricked FRWY-LS1012A</title>
    <link>https://community.nxp.com/t5/Layerscape/Recovering-bricked-FRWY-LS1012A/m-p/843786#M3825</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I recently purchased an FRWY-LS1012A, and connected it with a MAC only through USB debug/UART port. It works for a couple of times, I can see MBED pop up as a storage, and can connect through&amp;nbsp;serial. However, I bricked it after I did reset a couple of times. Now even if I hold reset and connect, nothing will show up.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After I tried a couple of times, I found only if I connect both usb&amp;nbsp;ports (USB3.0 and USB debug/UART port) the board can show up&amp;nbsp;as a bootloader folder (with reset pressed), so I can copy the bootloader firmware into it. But the still the board can't&amp;nbsp;boot up successfully, the green led keep blinking but no device being recognized&amp;nbsp;by MAC OS or windows.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What can I do then?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BTW, why doesn't NXP ship the board with a working firmware?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 16 Nov 2018 00:46:08 GMT</pubDate>
    <dc:creator>zcchai</dc:creator>
    <dc:date>2018-11-16T00:46:08Z</dc:date>
    <item>
      <title>Recovering bricked FRWY-LS1012A</title>
      <link>https://community.nxp.com/t5/Layerscape/Recovering-bricked-FRWY-LS1012A/m-p/843786#M3825</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I recently purchased an FRWY-LS1012A, and connected it with a MAC only through USB debug/UART port. It works for a couple of times, I can see MBED pop up as a storage, and can connect through&amp;nbsp;serial. However, I bricked it after I did reset a couple of times. Now even if I hold reset and connect, nothing will show up.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After I tried a couple of times, I found only if I connect both usb&amp;nbsp;ports (USB3.0 and USB debug/UART port) the board can show up&amp;nbsp;as a bootloader folder (with reset pressed), so I can copy the bootloader firmware into it. But the still the board can't&amp;nbsp;boot up successfully, the green led keep blinking but no device being recognized&amp;nbsp;by MAC OS or windows.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What can I do then?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BTW, why doesn't NXP ship the board with a working firmware?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 16 Nov 2018 00:46:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Recovering-bricked-FRWY-LS1012A/m-p/843786#M3825</guid>
      <dc:creator>zcchai</dc:creator>
      <dc:date>2018-11-16T00:46:08Z</dc:date>
    </item>
    <item>
      <title>Re: Recovering bricked FRWY-LS1012A</title>
      <link>https://community.nxp.com/t5/Layerscape/Recovering-bricked-FRWY-LS1012A/m-p/843787#M3826</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;The FRMY-LS1012a uses &lt;/SPAN&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;MK20DX128 processors for CMSIS-DAP interface. If there is no connection to CMSIS-DAP t&lt;/SPAN&gt;&lt;SPAN style="font-size: 10.0pt; background: white;"&gt;est connection to CMSIS-DAP using Windows. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; background: white;"&gt;Is there "mbed Serial Port" and "mbed" device if your board is connected to PC?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;Download and install the latest serial driver for Windows:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Fos.mbed.com%2Fhandbook%2FWindows-serial-configuration%231-download-the-mbed-windows-serial-port" rel="nofollow" target="_blank"&gt;https://os.mbed.com/handbook/Windows-serial-configuration#1-download-the-mbed-windows-serial-port&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;The &lt;/SPAN&gt;&lt;SPAN style="font-size: 10.0pt; color: black;"&gt;FRWY-LS1012A contains preinstalled u-boot and Linux.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Pavel Chubakov&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 Nov 2018 04:35:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Recovering-bricked-FRWY-LS1012A/m-p/843787#M3826</guid>
      <dc:creator>Pavel</dc:creator>
      <dc:date>2018-11-20T04:35:02Z</dc:date>
    </item>
    <item>
      <title>Re: Recovering bricked FRWY-LS1012A</title>
      <link>https://community.nxp.com/t5/Layerscape/Recovering-bricked-FRWY-LS1012A/m-p/843788#M3827</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Pavel,&lt;/P&gt;&lt;P&gt;No, there is no “mbed Serial Port” or “mbed” if I connect power and UART USB only, but it will show up if I connect both two USB ports. It is weird, I am wondering if there is some defects in my board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How can I boot into Linux? There is no SD attached, so I can only see U-boot interface when if connect it through UART USB.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Zhenchuan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 Nov 2018 18:19:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Recovering-bricked-FRWY-LS1012A/m-p/843788#M3827</guid>
      <dc:creator>zcchai</dc:creator>
      <dc:date>2018-11-20T18:19:33Z</dc:date>
    </item>
  </channel>
</rss>