<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Layerscape中的主题 Re: LS1043ARDB QE Firmware load error</title>
    <link>https://community.nxp.com/t5/Layerscape/LS1043ARDB-QE-Firmware-load-error/m-p/830327#M3744</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks you for the reply but that does not answer my question. I am already familiar with the file and with the memory layout. Why do I get the 'not a microcode' error with the default binaries for 18.09? Are you suggesting I should use the memory layout to debug the errors in flex-builder?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also - 18.09 is unusable for me as it will not build due to bad repo links as explained in this thread to which no one has yet offered a work around.&amp;nbsp;&lt;A _jive_internal="true" class="link-titled" href="https://community.nxp.com/thread/479101?commentID=1065151#comment" title="https://community.nxp.com/message/1065151?commentID=1065151#comment-1065151"&gt;https://community.nxp.com/message/1065151?commentID=1065151#comment-1065151&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 10 Oct 2018 12:17:46 GMT</pubDate>
    <dc:creator>danlenz</dc:creator>
    <dc:date>2018-10-10T12:17:46Z</dc:date>
    <item>
      <title>LS1043ARDB QE Firmware load error</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1043ARDB-QE-Firmware-load-error/m-p/830325#M3742</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;When booting from SD on the LS1043ARDB I see what I believe is a failure to load the QE firmware.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When booting from NOR I see uboot report:&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;Firmware 'Microcode version 0.0.1 for LS1021a r1.0' for 1021 V1.0&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;QE: uploading microcode 'Microcode for LS1021a r1.0' version 0.0.1&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When booting from SD however I do not see a line for QE uploading microcode&amp;nbsp;- instead I see:&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;MMC read: dev # 0, block # 18952, count 128 ...&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;Not a microcode&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there perhaps a bug in flex-builder which is placing the firmware at the wrong location on the SD?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here is the full log using the default binaries for LSDK 18.09:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;U-Boot SPL 2018.03-g1e96fd8f46 (Sep 20 2018 - 02:08:53 +0800)&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Initialzing DDR using fixed setting&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Configuring DDR for 1600 MT/s data rate&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Trying to boot from MMC1&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;&lt;EM&gt;U-Boot 2018.03-g1e96fd8f46 (Sep 20 2018 - 02:08:53 +0800)&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;SoC: unknown (0x87920411)&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Clock Configuration:&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt; CPU0(A53):1600 MHz CPU1(A53):1600 MHz CPU2(A53):1600 MHz &lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt; CPU3(A53):1600 MHz &lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt; Bus: 400 MHz DDR: 1600 MT/s FMAN: 500 MHz&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Reset Configuration Word (RCW):&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt; 00000000: 08100010 0a000000 00000000 00000000&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt; 00000010: 14550002 80004012 60040000 c1002000&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt; 00000020: 00000000 00000000 00000000 00038800&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt; 00000030: 00000000 00001100 00000096 00000001&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Model: LS1043A RDB Board&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Board: LS1043ARDB, boot from SD&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;CPLD: V1.5&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;PCBA: V3.0&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;SERDES Reference Clocks:&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;SD1_CLK1 = 156.25MHZ, SD1_CLK2 = 100.00MHZ&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;I2C: ready&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;DRAM: 1.9 GiB (DDR4, 32-bit, CL=11, ECC off)&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Using SERDES1 Protocol: 5205 (0x1455)&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;SEC0: RNG instantiated&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;FSL_SDHC: 0&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;PPA Firmware: Version LSDK-18.09&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;MMC read: dev # 0, block # 18952, count 128 ...&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Not a microcode&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Flash: 128 MiB&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;NAND: 512 MiB&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;MMC: Loading Environment from MMC... *** Warning - bad CRC, using default environment&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Failed (-5)&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;EEPROM: NXID v1&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;In: serial&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Out: serial&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Err: serial&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;SCSI: PCIe0: pcie@3400000 disabled&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;PCIe1: pcie@3500000 Root Complex: no link&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;PCIe2: pcie@3600000 Root Complex: no link&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Error: SCSI Controller(s) 1B4B:9170 not found&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Net: &lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;MMC read: dev # 0, block # 18432, count 128 ...&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Fman1: Uploading microcode version 106.4.18&lt;/EM&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 07 Oct 2018 23:02:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1043ARDB-QE-Firmware-load-error/m-p/830325#M3742</guid>
      <dc:creator>danlenz</dc:creator>
      <dc:date>2018-10-07T23:02:59Z</dc:date>
    </item>
    <item>
      <title>Re: LS1043ARDB QE Firmware load error</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1043ARDB-QE-Firmware-load-error/m-p/830326#M3743</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; color: black;"&gt;Look at attached files. These files are available in LSDK 18.09:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; color: black;"&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Fwww.nxp.com%2Fproducts%2Fprocessors-and-microcontrollers%2Farm-based-processors-and-mcus%2Fqoriq-layerscape-arm-processors%2Flayerscape-software-development-kit-v18.09%3ALAYERSCAPE-SDK" rel="nofollow" target="_blank"&gt;https://www.nxp.com/products/processors-and-microcontrollers/arm-based-processors-and-mcus/qoriq-layerscape-arm-processors/layerscape-software-development-kit-v18.09:LAYERSCAPE-SDK&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Pavel Chubakov&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 Oct 2018 04:48:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1043ARDB-QE-Firmware-load-error/m-p/830326#M3743</guid>
      <dc:creator>Pavel</dc:creator>
      <dc:date>2018-10-10T04:48:56Z</dc:date>
    </item>
    <item>
      <title>Re: LS1043ARDB QE Firmware load error</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1043ARDB-QE-Firmware-load-error/m-p/830327#M3744</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks you for the reply but that does not answer my question. I am already familiar with the file and with the memory layout. Why do I get the 'not a microcode' error with the default binaries for 18.09? Are you suggesting I should use the memory layout to debug the errors in flex-builder?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also - 18.09 is unusable for me as it will not build due to bad repo links as explained in this thread to which no one has yet offered a work around.&amp;nbsp;&lt;A _jive_internal="true" class="link-titled" href="https://community.nxp.com/thread/479101?commentID=1065151#comment" title="https://community.nxp.com/message/1065151?commentID=1065151#comment-1065151"&gt;https://community.nxp.com/message/1065151?commentID=1065151#comment-1065151&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 Oct 2018 12:17:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1043ARDB-QE-Firmware-load-error/m-p/830327#M3744</guid>
      <dc:creator>danlenz</dc:creator>
      <dc:date>2018-10-10T12:17:46Z</dc:date>
    </item>
  </channel>
</rss>