<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Configuring SERDES1 for SGMII on LS1046 in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/Configuring-SERDES1-for-SGMII-on-LS1046/m-p/829094#M3741</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Sorry ls1046ardb, the only working RCW&amp;nbsp; is 0x1133. I did manage to get a 0x3333 to work on the board, which did allow 1G optical operation from the&amp;nbsp; SFP.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 22 Aug 2018 13:01:03 GMT</pubDate>
    <dc:creator>kzambrano</dc:creator>
    <dc:date>2018-08-22T13:01:03Z</dc:date>
    <item>
      <title>Configuring SERDES1 for SGMII on LS1046</title>
      <link>https://community.nxp.com/t5/Layerscape/Configuring-SERDES1-for-SGMII-on-LS1046/m-p/829090#M3737</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp; I am&amp;nbsp;evaluating the LS1046ARDB capabilities, and per the documentation I can configure the RCW with 0x3333 to have SGMII on MAC 9 and 10.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;I have used Code Warrior to import the PBL, file produced by the LEDE distribution, and modified it using a QorIQ Project with Processor Expert. When burned into the alternate bank, UBOOT resets and comes up on the default bank. I believe this is due to a reset from the PLL failing to lock (per spec).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;Is this configuration possible, and if&amp;nbsp; so, what&amp;nbsp; is the recipe? I have tried various combinations of REF_CLK_SEL, which either resets or comes up w/o any working MAC or non-working DTSEC9 and DTSEC10.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; Has anyone tried to use a different protocol besides the default 0x1133?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;kz&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Jul 2018 14:08:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Configuring-SERDES1-for-SGMII-on-LS1046/m-p/829090#M3737</guid>
      <dc:creator>kzambrano</dc:creator>
      <dc:date>2018-07-19T14:08:35Z</dc:date>
    </item>
    <item>
      <title>Re: Configuring SERDES1 for SGMII on LS1046</title>
      <link>https://community.nxp.com/t5/Layerscape/Configuring-SERDES1-for-SGMII-on-LS1046/m-p/829091#M3738</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It is possible that modified RCW is incorrect.&lt;/P&gt;&lt;P&gt;Please consider creating a Technical Case to investigate the issue in detail:&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" class="jivelink10" href="https://community.nxp.com/thread/381898" title="https://community.nxp.com/thread/381898"&gt;https://community.nxp.com/thread/381898&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Jul 2018 06:49:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Configuring-SERDES1-for-SGMII-on-LS1046/m-p/829091#M3738</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2018-07-20T06:49:07Z</dc:date>
    </item>
    <item>
      <title>Re: Configuring SERDES1 for SGMII on LS1046</title>
      <link>https://community.nxp.com/t5/Layerscape/Configuring-SERDES1-for-SGMII-on-LS1046/m-p/829092#M3739</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;&amp;nbsp; Did that and found out that the ls1024ardb does not support any other protocol except 0x1333 (2xRGMII, 2xXGFI...).&amp;nbsp; The retimer in front of the SFP+ prevents anything but 10G. Not sure about the PHY connected XFI port, it should be capable of using SGMII, but I have not been successful in getting any output with UBOOT. The goal is to obtain 1G SGMII, but I see that the diagram for the reference board has labeled XFI/2.5G SGMII. Didn't get the memo for that either, is there a limitation there also?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 24 Jul 2018 15:15:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Configuring-SERDES1-for-SGMII-on-LS1046/m-p/829092#M3739</guid>
      <dc:creator>kzambrano</dc:creator>
      <dc:date>2018-07-24T15:15:58Z</dc:date>
    </item>
    <item>
      <title>Re: Configuring SERDES1 for SGMII on LS1046</title>
      <link>https://community.nxp.com/t5/Layerscape/Configuring-SERDES1-for-SGMII-on-LS1046/m-p/829093#M3740</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;gt; found out that the ls1024ardb&lt;/P&gt;&lt;P&gt;Excuse me, which exactly board is in question?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Jul 2018 06:05:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Configuring-SERDES1-for-SGMII-on-LS1046/m-p/829093#M3740</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2018-07-25T06:05:29Z</dc:date>
    </item>
    <item>
      <title>Re: Configuring SERDES1 for SGMII on LS1046</title>
      <link>https://community.nxp.com/t5/Layerscape/Configuring-SERDES1-for-SGMII-on-LS1046/m-p/829094#M3741</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Sorry ls1046ardb, the only working RCW&amp;nbsp; is 0x1133. I did manage to get a 0x3333 to work on the board, which did allow 1G optical operation from the&amp;nbsp; SFP.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Aug 2018 13:01:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Configuring-SERDES1-for-SGMII-on-LS1046/m-p/829094#M3741</guid>
      <dc:creator>kzambrano</dc:creator>
      <dc:date>2018-08-22T13:01:03Z</dc:date>
    </item>
  </channel>
</rss>