<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LayerscapeのトピックRe: LS2088A PCIe and NFA</title>
    <link>https://community.nxp.com/t5/Layerscape/LS2088A-PCIe-and-NFA/m-p/826595#M3721</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;A _jive_internal="true" data-content-finding="Community" data-userid="328912" data-username="mmcminn@uniondynamic.com" href="https://community.nxp.com/people/mmcminn@uniondynamic.com"&gt;Michael McMinn&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;QDMA can go across PCIe to access data, the PCIe EP can use QDMA to access data/buffers across PCIe to RC.&lt;/P&gt;&lt;P&gt;NFA engine(PME) belongs to DPAA, which is primarily for Ethernet because it has portal interface to QBMAN. The PME de-queues data from its QMAN hardware portal based on FQ configuration. QBMAN can be used to improve performance for data that are come in through the PCI bus.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;PME supports ~10 Gbps data scanning.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 06 Nov 2018 07:57:02 GMT</pubDate>
    <dc:creator>yipingwang</dc:creator>
    <dc:date>2018-11-06T07:57:02Z</dc:date>
    <item>
      <title>LS2088A PCIe and NFA</title>
      <link>https://community.nxp.com/t5/Layerscape/LS2088A-PCIe-and-NFA/m-p/826594#M3720</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is there a high speed data path between the PCIe bus and the NFA engine in the LS2088A and is it able to run at the rated 10Gb/s speed.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 23 Oct 2018 18:34:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS2088A-PCIe-and-NFA/m-p/826594#M3720</guid>
      <dc:creator>mmcminn</dc:creator>
      <dc:date>2018-10-23T18:34:50Z</dc:date>
    </item>
    <item>
      <title>Re: LS2088A PCIe and NFA</title>
      <link>https://community.nxp.com/t5/Layerscape/LS2088A-PCIe-and-NFA/m-p/826595#M3721</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;A _jive_internal="true" data-content-finding="Community" data-userid="328912" data-username="mmcminn@uniondynamic.com" href="https://community.nxp.com/people/mmcminn@uniondynamic.com"&gt;Michael McMinn&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;QDMA can go across PCIe to access data, the PCIe EP can use QDMA to access data/buffers across PCIe to RC.&lt;/P&gt;&lt;P&gt;NFA engine(PME) belongs to DPAA, which is primarily for Ethernet because it has portal interface to QBMAN. The PME de-queues data from its QMAN hardware portal based on FQ configuration. QBMAN can be used to improve performance for data that are come in through the PCI bus.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;PME supports ~10 Gbps data scanning.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 06 Nov 2018 07:57:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS2088A-PCIe-and-NFA/m-p/826595#M3721</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2018-11-06T07:57:02Z</dc:date>
    </item>
  </channel>
</rss>