<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LayerscapeのトピックRe: A Question About The Kernel Configuration For The Linux Build Distributed With Clonezilla</title>
    <link>https://community.nxp.com/t5/Layerscape/A-Question-About-The-Kernel-Configuration-For-The-Linux-Build/m-p/433745#M366</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Pavel,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for attaching the .config that the SDK defaults to.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Unfortunately, this is not the file we have been interested in finding.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In an attempt to clarify our question:&lt;/P&gt;&lt;P&gt;The LS1021A-TWR board was shipped to us in August 2014 with a thumb drive. On that thumb drive, there was an .iso with the Clonezilla disk cloning utility and the necessary files for the Access Point demo Linux image. This demo is different from the image on our TWR board's default NOR flash (which just shows two Tux logos). The Access Point demo has three slide shows which are advanced with mouse clicks and it has a menu for configuring wireless connectivity. Since the thumb drive only contains the rootfs, DTB, and uImage for this demo, we are asking where we might find the files (.config, .dtsi, .dts, etc... but specifically the .config) that were used to build the demo kernel.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you need us to further clarify or provide you with any more information, we would be happy to.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Patrick&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 08 Jun 2015 14:19:49 GMT</pubDate>
    <dc:creator>patrickmorrow</dc:creator>
    <dc:date>2015-06-08T14:19:49Z</dc:date>
    <item>
      <title>A Question About The Kernel Configuration For The Linux Build Distributed With Clonezilla</title>
      <link>https://community.nxp.com/t5/Layerscape/A-Question-About-The-Kernel-Configuration-For-The-Linux-Build/m-p/433743#M364</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We have built a custom board around an LS1021A chip.&amp;nbsp; We've managed to create everything one would need (u-boot, device trees, linux kernels, etc.) in order to run Linux on our system.&amp;nbsp; After running Linux for several minutes, we encounter either kernel panics or faults that bring everything to a standstill.&amp;nbsp; We've managed to cobble together an SD card complete with a u-boot that was compiled explicitly for our custom board, and Linux files (uImage, dtb and rootfs) for the LS1021A-TWR that we got from the Clonezilla distribution built on Linux 3.12.0.&amp;nbsp; This setup runs indefinitely.&amp;nbsp; Nothing seems to cause panics or faults or anything else.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We were wondering if we could somehow get the Kernel Configuration file for the Clonezilla build and compare it to our configuration file.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We're fairly certain it has to do with some kind of faulty driver that is not included on Clonezilla, but we are having a hard time tracking it down. Using SDK1.7 with Service Pack 1.5 to build Linux with the default kernel configuration and default dts files also produces kernel panics. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Patrick&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 05 Jun 2015 20:24:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/A-Question-About-The-Kernel-Configuration-For-The-Linux-Build/m-p/433743#M364</guid>
      <dc:creator>patrickmorrow</dc:creator>
      <dc:date>2015-06-05T20:24:36Z</dc:date>
    </item>
    <item>
      <title>Re: A Question About The Kernel Configuration For The Linux Build Distributed With Clonezilla</title>
      <link>https://community.nxp.com/t5/Layerscape/A-Question-About-The-Kernel-Configuration-For-The-Linux-Build/m-p/433744#M365</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN lang="EN-US" style="font-family: 'Times New Roman';"&gt;Freescale offers Linux SDK 1.7:&lt;/SPAN&gt;&lt;/P&gt;&lt;PRE class="jive-pre"&gt;&lt;SPAN lang="EN-US" style="font-family: 'Times New Roman';"&gt;&lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=SDKLINUX&amp;amp;fsrch=1" rel="nofollow noopener noreferrer" target="_blank"&gt;http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=SDKLINUX&amp;amp;fsrch=1&lt;/A&gt;&lt;/SPAN&gt;&lt;/PRE&gt;&lt;PRE class="jive-pre"&gt; &lt;/PRE&gt;&lt;PRE class="jive-pre"&gt;&lt;SPAN lang="EN-US" style="font-family: 'Times New Roman';"&gt;This SDK supports the TWR-LS1021A board. Board from the factory contains configuration from the SDK. &lt;/SPAN&gt;&lt;/PRE&gt;&lt;PRE class="jive-pre"&gt; &lt;/PRE&gt;&lt;PRE class="jive-pre"&gt;&lt;SPAN lang="EN-US" style="font-family: 'Times New Roman';"&gt;Attached file contains .config file from this SDK.&lt;/SPAN&gt;&lt;/PRE&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Pavel&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 08 Jun 2015 12:17:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/A-Question-About-The-Kernel-Configuration-For-The-Linux-Build/m-p/433744#M365</guid>
      <dc:creator>Pavel</dc:creator>
      <dc:date>2015-06-08T12:17:00Z</dc:date>
    </item>
    <item>
      <title>Re: A Question About The Kernel Configuration For The Linux Build Distributed With Clonezilla</title>
      <link>https://community.nxp.com/t5/Layerscape/A-Question-About-The-Kernel-Configuration-For-The-Linux-Build/m-p/433745#M366</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Pavel,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for attaching the .config that the SDK defaults to.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Unfortunately, this is not the file we have been interested in finding.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In an attempt to clarify our question:&lt;/P&gt;&lt;P&gt;The LS1021A-TWR board was shipped to us in August 2014 with a thumb drive. On that thumb drive, there was an .iso with the Clonezilla disk cloning utility and the necessary files for the Access Point demo Linux image. This demo is different from the image on our TWR board's default NOR flash (which just shows two Tux logos). The Access Point demo has three slide shows which are advanced with mouse clicks and it has a menu for configuring wireless connectivity. Since the thumb drive only contains the rootfs, DTB, and uImage for this demo, we are asking where we might find the files (.config, .dtsi, .dts, etc... but specifically the .config) that were used to build the demo kernel.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you need us to further clarify or provide you with any more information, we would be happy to.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Patrick&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 08 Jun 2015 14:19:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/A-Question-About-The-Kernel-Configuration-For-The-Linux-Build/m-p/433745#M366</guid>
      <dc:creator>patrickmorrow</dc:creator>
      <dc:date>2015-06-08T14:19:49Z</dc:date>
    </item>
    <item>
      <title>Re: A Question About The Kernel Configuration For The Linux Build Distributed With Clonezilla</title>
      <link>https://community.nxp.com/t5/Layerscape/A-Question-About-The-Kernel-Configuration-For-The-Linux-Build/m-p/433746#M367</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN lang="EN-US" style="font-family: 'Times New Roman';"&gt;Install SDK 1.7 and Service Pack for this SDK:&lt;/SPAN&gt;&lt;/P&gt;&lt;PRE class="jive-pre"&gt;&lt;SPAN lang="EN-US" style="font-family: 'Times New Roman';"&gt;&lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=LS1021A&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab" rel="nofollow noopener noreferrer" target="_blank"&gt;http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=LS1021A&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab&lt;/A&gt;&lt;/SPAN&gt;&lt;/PRE&gt;&lt;PRE class="jive-pre"&gt; &lt;/PRE&gt;&lt;PRE class="jive-pre"&gt;&lt;SPAN lang="EN-US" style="font-family: 'Times New Roman';"&gt;See the .config file. This file contains tumb configuration parameters.&lt;/SPAN&gt;&lt;/PRE&gt;&lt;PRE class="jive-pre"&gt;&lt;SPAN lang="EN-US" style="font-family: 'Times New Roman';"&gt;These parameters can be enabled using kernel menu.&lt;/SPAN&gt;&lt;/PRE&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Pavel&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 Jun 2015 06:05:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/A-Question-About-The-Kernel-Configuration-For-The-Linux-Build/m-p/433746#M367</guid>
      <dc:creator>Pavel</dc:creator>
      <dc:date>2015-06-09T06:05:43Z</dc:date>
    </item>
    <item>
      <title>Re: A Question About The Kernel Configuration For The Linux Build Distributed With Clonezilla</title>
      <link>https://community.nxp.com/t5/Layerscape/A-Question-About-The-Kernel-Configuration-For-The-Linux-Build/m-p/433747#M368</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Pavel,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;&lt;SPAN lang="EN-US" style="font-family: 'Times New Roman';"&gt;Install SDK 1.7 and Service Pack for this SDK:&lt;/SPAN&gt;&lt;/P&gt;&lt;PRE class="jive-pre"&gt;&lt;SPAN lang="EN-US" style="font-family: 'Times New Roman';"&gt;&lt;A class="jive-link-external-small" data-content-finding="Community" href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=LS1021A&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab" onclick="" rel="nofollow noopener noreferrer" target="_blank"&gt;http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=LS1021A&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab&lt;/A&gt;&lt;/SPAN&gt;&lt;/PRE&gt;&lt;/BLOCKQUOTE&gt;&lt;PRE class="jive-pre"&gt; &lt;/PRE&gt;&lt;PRE class="jive-pre"&gt;&lt;SPAN lang="EN-US" style="font-family: 'Times New Roman';"&gt;See the .config file. This file contains tumb configuration parameters.&lt;/SPAN&gt;&lt;/PRE&gt;&lt;PRE class="jive-pre"&gt;&lt;SPAN lang="EN-US" style="font-family: 'Times New Roman';"&gt;&lt;/SPAN&gt;&lt;/PRE&gt;&lt;P&gt;As mentioned in the original post, SDK 1.7 with Service Pack 1.5 &lt;EM&gt;&lt;STRONG&gt;IS&lt;/STRONG&gt;&lt;/EM&gt; what we are using when we encounter the problem. Issuing &lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;&lt;SPAN style="font-family: 'courier new', courier;"&gt;bitbake -c cleansstate virtual/kernel&lt;/SPAN&gt; &lt;/P&gt;&lt;P&gt;followed by &lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;&lt;SPAN style="font-family: 'courier new', courier;"&gt;bitbake -c menuconfig virtual/kernel&lt;/SPAN&gt; &lt;/P&gt;&lt;P&gt;generates the default .config but this does not appear to be the .config that was used when building the Access Point demo from the thumb drive.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If we boot from SD with a known good rootfs, the uImage.bin from the build process on SDK 1.7 SP 1.5 with the default .config you recommend, and the DTB from the same process, our kernel will panic after a several minutes.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If we use the same RCW, U-Boot, and rootfs from the above scenario but use the Access Point demo's uImage.bin and the Access Point demo's DTB, we do not encounter the same problem.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 Jun 2015 16:01:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/A-Question-About-The-Kernel-Configuration-For-The-Linux-Build/m-p/433747#M368</guid>
      <dc:creator>patrickmorrow</dc:creator>
      <dc:date>2015-06-09T16:01:51Z</dc:date>
    </item>
    <item>
      <title>Re: A Question About The Kernel Configuration For The Linux Build Distributed With Clonezilla</title>
      <link>https://community.nxp.com/t5/Layerscape/A-Question-About-The-Kernel-Configuration-For-The-Linux-Build/m-p/433748#M369</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN lang="EN-US" style="font-family: 'Times New Roman';"&gt;Try to enable thumb using the following command sequence:&lt;/SPAN&gt;&lt;/P&gt;&lt;PRE class="jive-pre"&gt;&lt;SPAN lang="EN-US" style="font-family: 'Times New Roman';"&gt;$ bitbake -c cleanall virtual/kernel&lt;/SPAN&gt;&lt;/PRE&gt;&lt;PRE class="jive-pre"&gt;&lt;SPAN lang="EN-US" style="font-family: 'Times New Roman';"&gt;$ bitbake -c patch virtual/kernel&lt;/SPAN&gt;&lt;/PRE&gt;&lt;PRE class="jive-pre"&gt;&lt;SPAN lang="EN-US" style="font-family: 'Times New Roman';"&gt;$ bitbake -c menuconfig virtual/kernel&amp;nbsp; // enable thumb&lt;/SPAN&gt;&lt;/PRE&gt;&lt;PRE class="jive-pre"&gt;&lt;SPAN lang="EN-US" style="font-family: 'Times New Roman';"&gt;$ bitbake virtual/kernel // Rebuild kernel:&lt;/SPAN&gt;&lt;/PRE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Pavel&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 Jun 2015 11:54:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/A-Question-About-The-Kernel-Configuration-For-The-Linux-Build/m-p/433748#M369</guid>
      <dc:creator>Pavel</dc:creator>
      <dc:date>2015-06-10T11:54:45Z</dc:date>
    </item>
    <item>
      <title>Re: A Question About The Kernel Configuration For The Linux Build Distributed With Clonezilla</title>
      <link>https://community.nxp.com/t5/Layerscape/A-Question-About-The-Kernel-Configuration-For-The-Linux-Build/m-p/433749#M370</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Pavel,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The &lt;SPAN style="font-family: 'courier new', courier;"&gt;CONFIG_ARM_THUMB&lt;/SPAN&gt;, &lt;SPAN style="font-family: 'courier new', courier;"&gt;CONFIG_THUMB2_KERNEL&lt;/SPAN&gt;, and &lt;SPAN style="font-family: 'courier new', courier;"&gt;CONFIG_THUMB2_AVOID_R_ARM_THM_JUMP11&lt;/SPAN&gt; kernel configuration options are all enabled by default and the default configuration produces the same problem.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the interest of being through, we ran another test in which we also enabled the only other Thumb option (&lt;SPAN style="font-family: 'courier new', courier;"&gt;CONFIG_ARM_THUMBEE&lt;/SPAN&gt;) but there was no difference.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Patrick&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 Jun 2015 20:11:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/A-Question-About-The-Kernel-Configuration-For-The-Linux-Build/m-p/433749#M370</guid>
      <dc:creator>patrickmorrow</dc:creator>
      <dc:date>2015-06-10T20:11:49Z</dc:date>
    </item>
  </channel>
</rss>