<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LayerscapeのトピックRe: IFC: GPCM - write in burst mode to async. memory</title>
    <link>https://community.nxp.com/t5/Layerscape/IFC-GPCM-write-in-burst-mode-to-async-memory/m-p/813798#M3630</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Neither WE nor CS toggles during GPCM burst. Yes, you need additional logic to get pulses on those signals. Or optionally you can disable bursts, this affects performance but does not require external logic.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Bulat&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 04 Sep 2018 13:09:56 GMT</pubDate>
    <dc:creator>Bulat</dc:creator>
    <dc:date>2018-09-04T13:09:56Z</dc:date>
    <item>
      <title>IFC: GPCM - write in burst mode to async. memory</title>
      <link>https://community.nxp.com/t5/Layerscape/IFC-GPCM-write-in-burst-mode-to-async-memory/m-p/813797#M3629</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello again.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We're evalutating options to connect a non-volatile memory (nvSRAM, MRAM, FRAM - not flash based) to the LS1046A. One option I'm looking at in more detail right now is the GPCM mode of the IFC and I ran across a question regarding burst access for writing:&lt;/P&gt;&lt;P&gt;Does TCH (chip-select hold time) play a role in burst accesses? And does the write enable signal toggle at all during the burst?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The memory devices we're looking at have an asynchronous SRAM interface, so the IFC_CLK is not used and write accesses are controlled by the chip select and write enable signals. If these don't toggle during burst accesses weÄd need to add some additional logic to insert an additional pulse into the WE or CS signal.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does anyone have experience connecting asynchronous memory (not flash based)?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Ferdinand&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Aug 2018 12:32:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/IFC-GPCM-write-in-burst-mode-to-async-memory/m-p/813797#M3629</guid>
      <dc:creator>ferdinandgrossm</dc:creator>
      <dc:date>2018-08-22T12:32:18Z</dc:date>
    </item>
    <item>
      <title>Re: IFC: GPCM - write in burst mode to async. memory</title>
      <link>https://community.nxp.com/t5/Layerscape/IFC-GPCM-write-in-burst-mode-to-async-memory/m-p/813798#M3630</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Neither WE nor CS toggles during GPCM burst. Yes, you need additional logic to get pulses on those signals. Or optionally you can disable bursts, this affects performance but does not require external logic.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Bulat&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 04 Sep 2018 13:09:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/IFC-GPCM-write-in-burst-mode-to-async-memory/m-p/813798#M3630</guid>
      <dc:creator>Bulat</dc:creator>
      <dc:date>2018-09-04T13:09:56Z</dc:date>
    </item>
    <item>
      <title>Re: IFC: GPCM - write in burst mode to async. memory</title>
      <link>https://community.nxp.com/t5/Layerscape/IFC-GPCM-write-in-burst-mode-to-async-memory/m-p/813799#M3631</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Bulat,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks for confirming!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Sep 2018 06:18:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/IFC-GPCM-write-in-burst-mode-to-async-memory/m-p/813799#M3631</guid>
      <dc:creator>ferdinandgrossm</dc:creator>
      <dc:date>2018-09-05T06:18:00Z</dc:date>
    </item>
  </channel>
</rss>